4. Building Debian Images Using Armbian
4.1. Introduction
Texas Instruments uses the Armbian build framework to generate Debian images for its platforms. Armbian describes itself to be a “base operating system”; that is, a build framework used to build Linux images optimized for Single-Board Computers.
AM62Px-SDK-Download-page provides Debian images, but users can also build these, especially if users require something custom (such as different kernel configurations or default desktop environments).
4.2. Armbian Usage
This document provides high-level information about how to build Debian images for TI platforms, using Armbian. For a full list of options available for users to configure these images at build time, see Armbian Documentation.
4.2.1. Get Armbian
For the time being, TI’s fork of Armbian/build maintains support for TI platforms. Therefore, the first step is to fetch TI’s fork:
git clone https://github.com/TexasInstruments/armbian-build.git
4.2.2. Repository Structure
The following files and directories are relevant to this high-level overview:
config/: This directory has configurations for boards, families, kernel configurations, desktop or CLI environments and so on. To find configuration files relevant to TI, see:config/boards/<TI EVM board>.confconfig/sources/families/include/k3_common.incconfig/sources/families/k3.confconfig/kernel/linux-k3-vendor.confconfig/kernel/linux-k3-vendor-rt.confconfig/kernel/linux-k3-vendor-edge.confconfig/kernel/linux-k3-edge.conf
compile.sh: This is the script that the user should run for building Armbian images.lib/: This directory stores the scripts that do most of the work in building Armbian images.extensions/: This directory has files that define extension hooks. In Armbian, extension hooks are function signatures, which the build framework calls in the process of building an image. However, the build framework does not define these inlib/. Users can define these functions and integrate custom steps in the build process. TI hasextensions/ti-debpkgs.shextension file. To customize the build process, create a new file in this directory, and define your extension hooks there. Once the file is created, be sure to add the following line to board/family config file:enable_extension <extension_name>userpatches/: This directory stores files that define build parameters, user patches and so on.
4.2.3. Building Images
Armbian supports both an interactive UI and a noninteractive build process.
Note
This build guide has been tested on an x86 host machine running Ubuntu 22.04. The Armbian compile.sh script
builds in an ARM64 docker container. Install the following packages and configure docker:
sudo apt update
sudo apt install docker.io qemu-user-static binfmt-support
sudo usermod -aG docker $USER
newgrp docker
To build interactively:
./compile.shThe build framework will then display dialog boxes. The user can use this to select the board, CLI or desktop environment, kernel configurations and so on.
To build non-interactively:
./compile.sh [command] [switch...] [command...]A full list of build switches is available at Build Switches.
Warning
If build issues arise, try adding these build switches to the end of the build command:
GIT_SKIP_SUBMODULES=yes SKIP_ARMBIAN_REPO=yesFor example, the following command builds the minimal non-RT Trixie image:
./compile.sh build BOARD=<board> BRANCH=vendor BUILD_MINIMAL=yes KERNEL_CONFIGURE=no RELEASE=trixie GIT_SKIP_SUBMODULES=yes SKIP_ARMBIAN_REPO=yes
For a list of boards and branches supported by each SoC, refer:
SoC
Board
Board Config File
Branch
AM62x
sk-am62b
config/boards/sk-am62b.confvendor, vendor-rt, vendor-edge, edge
AM62-LP
sk-am62-lp
config/boards/sk-am62-lp.confvendor, vendor-rt, vendor-edge, edge
AM62SIP
sk-am62-sip
config/boards/sk-am62-sip.confvendor, vendor-rt, vendor-edge, edge
AM62Lx
tmds62levm
config/boards/tmds62levm.confvendor, vendor-rt, vendor-edge
AM62Lx
beaglebadge
config/boards/beaglebadge.confvendor-edge
AM62Px
sk-am62p
config/boards/sk-am62p.confvendor, vendor-rt, vendor-edge, edge
AM64x
sk-am64b
config/boards/sk-am64b.confvendor, vendor-rt, vendor-edge, edge
output/images/ stores the built images. These images have a .img extension.