3.6.5. Flash via UART

This tool uses UART as the transport or interface to send the file to flash to the EVM.

The UART Flash tool is part of MCU+SDK installer and can be downloaded from AM62Px-SDK-Download-page.

Detailed instructions on using the tool can be found in MCU+SDK docs.

MCU+SDK Flash Tools Documentation.