2.3. Yocto Layer Configuration

Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:

$ ./oe-layertool-setup.sh -f <config>

The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.

Config File

Description

Supported machines/platforms

processor-sdk-scarthgap-chromium-11.01.16.13-config.txt

Processor SDK 11.01.16.13 Release

am62pxx-evm

processor-sdk-scarthgap-11.01.16.13-config.txt

Processor SDK 11.01.16.13 Release

am62pxx-evm

processor-sdk-scarthgap-selinux-11.01.16.13-config.txt

Processor SDK 11.01.16.13 Release

am62pxx-evm

The oe-layersetup configuration, as defined in processor-sdk-scarthgap-chromium-11.01.16.13-config.txt, is used for configuring the meta layers in the yocto SD card image available on AM62Px-SDK-Download-page.