4.1.14. How to check some device tree information from user-space of Linux?
You might need to check value of some dtb entry, for debugging, checking that your dtb really got updated after you modfified, etc. Though you can’t have a .dts-file-like view of the device tree which was loaded, you can check values using the entries in /proc/device-tree.
In the command prompt of Linux, you should see something similar to the following in the /proc/device-tree directory:
root@j721e-evm:~# ls /proc/device-tree/
#address-cells firmware l3-cache0
#size-cells fixedregulator-evm12v0 main_r5fss_cpsw9g_virt_mac0
__symbols__ fixedregulator-sd memory@80000000
aliases fixedregulator-vsys3v3 model
chosen fixedregulator-vsys5v0 name
compatible gpio-keys pmu
connector interconnect@100000 reserved-memory
cpus interrupt-parent serial-number
dma_buf_phys ion sound@0
dummy-panel l2-cache0 timer-cl0-cpu0
Following are some typical usages you might need:
Let’s say you don’t know the exact path of the device tree entry you are
trying to check. There is a __symbols__ directory in /proc/device-tree, which
is very helpful in such cases. It has an entry for each symbol label in the
device tree. You can find the exact path for that symbol by running cat
command on that entry. Following is an example demonstrating the use:
root@am62xx-evm:~# cat /proc/device-tree/__symbols__/main_i2c0
/bus@f0000/i2c@20000000
root@am62xx-evm:~# ls /proc/device-tree/bus@f0000/i2c@20000000/
'#address-cells' clock-names eeprom@51 phandle power-domains tps6598x@3f
'#size-cells' clocks interrupts pinctrl-0 reg
clock-frequency compatible name pinctrl-names status
You can check the value of a device tree entry using cat command if it is a string. But if the value is an integer or some numeric data, you will have to run the hexdump command instead to get output in a readable format. Following is an example demonstrating the use:
# Example for a string value
root@am62xx-evm:~# cat /proc/device-tree/bus@f0000/i2c@20000000/compatible
ti,am64-i2cti,omap4-i2c
# Example for an integer value where the first column represents input offsets
root@am62xx-evm:~# hexdump -C /proc/device-tree/bus@f0000/i2c@20000000/clock-frequency
00000000 00 06 1a 80 |....|
00000004
# The above value is in hexadecimal. You can calculate it's value in decimal by using following command
root@am62xx-evm:~# echo $((0x00061a80))
400000
One common scenario of a device tree change is tweaking the memory for remoteproc processors like R5F. You can check if it got updated correctly, by running a command similar to following for the specific processor core.
# Finding symbols for remote cores
root@am62xx-evm:~# ls /proc/device-tree/__symbols__/ | grep "r5f"; ls /proc/device-tree/__symbols__/ | grep "m4f"; ls /proc/device-tree/__symbols__/ | grep "c7x";
wkup_r5fss0
wkup_r5fss0_core0
wkup_r5fss0_core0_dma_memory_region
wkup_r5fss0_core0_memory_region
mcu_m4fss
mcu_m4fss_dma_memory_region
mcu_m4fss_memory_region
# Finding location from the symbols
root@am62xx-evm:~# cat /proc/device-tree/__symbols__/mcu_m4fss_memory_region
/reserved-memory/m4f-memory@9cc00000
root@am62xx-evm:~# cat /proc/device-tree/__symbols__/mcu_m4fss_dma_memory_region
/reserved-memory/m4f-dma-memory@9cb00000
# Checking the values
root@am62xx-evm:~# hexdump -C /proc/device-tree/reserved-memory/m4f-memory@9cc00000/reg
00000000 00 00 00 00 9c c0 00 00 00 00 00 00 00 e0 00 00 |................|
00000010
root@am62xx-evm:~# hexdump -C /proc/device-tree/reserved-memory/m4f-dma-memory@9cb00000/reg
00000000 00 00 00 00 9c b0 00 00 00 00 00 00 00 10 00 00 |................|
00000010
Warning
Before tweaking the memory for remote processors, please verify that the memory can be modified since some remote processors can be running firmware like DM firmware.