3.8.2. Rogue debug info
Rogue graphics drivers include the following tools bundled with their user mode libraries:
|
Control debug verbosity and other device info |
|
Dump diagnostic information for an application |
|
Start, Stop, Restart and configure the GPU using a powervr.ini file |
|
Try several blit operations and display them to the screen |
|
Try several different compute tasks on the core |
|
Try several processes on the core to stress the KickSync API |
|
Render a triangle to the attached display |
|
Twiddle several textures in several different pixel formats |
Future releases of ti-img-rogue-umlibs can include more tools. This is the core set expected to be available in most ti-img-rogue-umlibs releases and are the most useful for verifying GPU functionality.
The order of operation to verify fundamental GPU functionality is as follows:
Use
rgx_kicksync_testto verify the GPU can communicate with the kernel module.Use
rgx_compute_testto verify that the GPU is able to handle a proper compute load.Use
rgx_triangle_testto verify that the GPU is able to render to an output buffer.
If you are still experiencing issues after verifying fundamental functionality, try checking the output of the following:
# pvrdebug -dd
Note
When raising a ticket on e2e forums it is useful to include the output of this command if available.
This will dump all device information as reported by the kernel module. Please ensure that the debug info reports:
Comparison of UM/KM components: MATCHING
User mode and kernel mode components must move in lockstep. If they do not match this could lead to the kernel module failing to initialize or undefined behavior.