2.1. Release Notes

2.1.1. Overview

The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.

To simplify the end user experience, Processor SDK Linux AM62Px installer provides everything needed as discussed below to create the embedded system from “scratch” :

  • Platform/board-support software and configuration files for Linux

  • U-Boot and Kernel sources and configuration files

  • An ARM cross-compiling toolchain as well as other host binaries and components

  • A Yocto/OE compliant filesystem and sources for example applications

  • A variety of scripts and Makefiles to automate certain tasks

  • Other components needed to build an embedded system that don’t fit neatly into one of the above buckets

  • Reference Examples, benchmarks

This release supports High Security - Field Securable (HS-FS) devices.

2.1.2. Licensing

Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.

  • Linux Manifest: <PSDK_PATH>/manifest/software_manifest.htm

2.1.3. Release 11.00.09.04

Released on April 2025

2.1.3.1. What’s new

Processor SDK Linux AM62PX Release has following new features:

  • First 2025 LTS Reference Release Including RT combined branch model - Important Bug Fixes on top of Processor SDK 10.01.10.04 Release - Review Issue Tracker Section for the new fixes.

Key Release References:

Component version:

  • Kernel 6.12.17

  • U-Boot 2025.01

  • Toolchain GCC 13.3

  • ATF 2.12+

  • OPTEE 4.5.0

  • Graphics DDK 24.2

  • TIFS Firmware / SYSFW v11.00.07 (Click on the link for more information)

  • DM Firmware 11.00.00.06

  • Yocto scarthgap 5.0

2.1.4. Build Information

2.1.4.1. U-Boot

u-boot

Head Commit: cd91d73601810374d16a1f17505ab2e72e31f75d PENDING: mmc: am654_sdhci: Unset HIGH_SPEED_ENA for MMC_HS_52
uBoot Version: 2025.01
uBoot Description: RC Release 11.00.09
Clone: git://git.ti.com/ti-u-boot/ti-u-boot.git
Branch: ti-u-boot-2025.01
uBoot Tag: 11.00.09

2.1.4.2. TF-A

Head Commit: b11beb2b6bd30b75c4bfb0e9925c0e72f16ca53f PENDING: feat(ti): Update DDR Configurations
Branch: ti-master
Tag: (2.12 based): 11.00.09

2.1.4.3. OP-TEE

Head Commit: ef1ebdc23034a804a72da2207f1a825ce96a1464 plat-k3: Add initial support for AM62Lx SoC
Branch: master
Tag: 4.5.0+

2.1.4.4. ti-linux-firmware

Head Commit: 27003b6bff61a55dd1fff2cc777e5e07b092b1f7 ti-eth: j721e/j784s4/j7200: update firmware to version 11.00.02
Branch: ti-linux-firmware
Tag: 11.00.09

2.1.4.5. Kernel

Linux Kernel

Head Commit: c85877d40f8e70e1e201eca2ae1648781f238a37 PENDING: can: m_can: Support pinctrl wakeup state for Partial I/O
Kernel Version: v6.12.17
Kernel Description: RC Release 11.00.09
Repo: git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git
Branch: ti-linux-6.12.y
Tag: 11.00.09
use-kernel-config=defconfig
non-rt-config-fragment=kernel/configs/ti_arm64_prune.config
rt-config-fragment=config-fragment=kernel/configs/ti_arm64_prune.config kernel/configs/ti_rt.config

2.1.4.6. Yocto

meta-ti

Head Commit: 5385fb9231e8d48c30ddd965c4cc623a1f004e3e CI/CD Auto-Merger: cicd.scarthgap.202503251551
Clone: git://git.yoctoproject.org/meta-ti
Branch: scarthgap
Release Tag: 11.00.09

meta-arago

Head Commit: 4ec7ae427f9a6aeb7d0b98ac7251bfc2436dbae2 CI/CD Auto-Merger: cicd.scarthgap.202503251551
Clone: git://git.yoctoproject.org/meta-arago
Branch: scarthgap
Release Tag: 11.00.09

meta-tisdk

Head Commit: c1f4a8eaf9b0779e9dfa66d2e4de0ac4173772c4 meta-ti-foundational: seva: Make service file work with emptty
Branch: scarthgap
Release Tag: 11.00.09.04

2.1.5. Issues Tracker

Note

  • Release Specific Issues including details will be published through Software Incident Report (SIR) portal

  • Further Information can be found at SIR Portal

2.1.5.1. Errata Resolved

Record ID

Title

EXT_EP-12128

USB2 PHY locks up due to short suspend

EXT_EP-12124

BCDMA: RX Channel can lockup in certain scenarios

EXT_EP-12294

MMCHS: eMMC HS400 tDCD timing marginal to JEDEC spec

2.1.5.2. Issues Resolved

Record ID

Title

EXT_SITMPUSW-75

Update OTAP values to match the latest datasheet updates

EXT_EP-12063

Update the DDR configuration with DDR syscfg 10.03

EXT_EP-12293

Update OTAP values for HS400 to match the latest datasheet updates

EXT_EP-12111

Linux SDK v10.0: TI-added support for W25N01JW SPI NAND breaks other existing Flash support

EXT_EP-12112

Add Timer PWM documentation and other infrastructure as needed

EXT_EP-12268

alloc space exhausted error at u-boot for display cluster

EXT_EP-12284

Partial I/O not resuming from mcan

EXT_EP-12288

Graphics driver fails to suspend

EXT_EP-12289

Unable to boot kernel from eMMC

EXT_EP-12295

IO Only + DDR Resume Failure: platform 79000000.r5f: ti-sci processor set_config failed

2.1.5.3. Issues Open

Record ID

Title

None

TODO