5.1. TI LVGL Demo - User Guide

5.1.1. Overview

TI LVGL Demo is a simple app that showcases the capabilities of the LVGL - Light and Versatile Graphics Library. It includes various demo applications, such as:

  • EV Charging

  • Arm analytics

  • Smart Home

  • Smart Meter

  • Thermostat

  • Security

Note

Platform compatibility varies for different demo applications. Please see the platform compatibility table below:

Table 5.1 Demo Compatibility by Platform

Platform

EV Charging

Arm analytics

Smart Home

Smart Meter

Thermostat

Security

AM62L

AM62x

AM62P

AM335X

AM437X

AM65X

All necessary equipment and step by step instructions are provided below:

Note

Some of the features within each of these applications are not supported on all platforms. So there will be differences in feature enablement across platforms.

5.1.2. Hardware Prerequisites

  • PC (Windows or Linux, to use serial terminal console)

  • HDMI/DSI Display (to view the Demo on Display)

  • Ethernet Cable or CC33xx WiFi module (to connect EVM to internet)

  • Mouse or Touch Input from HDMI monitor (to control the TI LVGL Demo)

  • SD card (minimum 32GB)

  • Aux cable connected to earphone/speaker

  • Jumper cable (to connect potentiometer to ADC input) or some analog signal connected to ADC input. In the J11 header, pin D7 (A01) is the potentiometer out, which needs to be connected to pin D6 (A02) ADC in for channel 0. (Reference schematics can be found in AM62L schematics)

    ../../_images/ti-lvgl-demo-tmds62levm-potentiometer-connection.png

5.1.3. Launching the TI LVGL Demo

The demo will auto launch upon Linux booting on the EVM. Follow the below instructions to flash the SD card:

  1. Flash an SD card with the tisdk-default-image. User can download the tisdk-default-image wic image from AM62L-SDK-Download-page. Please follow the instructions from here to Flash an SD card.

  2. Insert the flashed SD card to the board, connect the display, mouse/touch-input, ethernet cable, aux cable, jumper wire and power on the EVM. The TI LVGL Demo will launch automatically when the device is fully booted.

Note

AM62LX Performance Issue - SDK 11.02.08.02 and 12.00.00.07.04:

For AM62LX platform in SDK releases 11.02.08.02 and 12.00.00.07.04, the default LVGL application is configured to run on Direct Rendering Manager (DRM) which has resulted in performance issues. To improve performance, the rendering mode needs to be changed from DRM to framebuffer (FB) rendering.

5.1.4. Using the TI LVGL Demo

The landing/home page of the LVGL demo looks like the following:

../../_images/ti-lvgl-demo-home-page.gif
  • In the demo, scroll through the various widgets to launch different apps.

  • The date/time panel shows the UTC timezone provided the EVM is connected to the internet.

  • Exit button on top left can be used to exit the demo. systemctl stop ti-lvgl-demo can also be used to stop the demo.

  • System button (Center button in top-right toolbar) shows FPS of the demo and CPU Utilization of the system.

  • Buttons in bottom-right toolbar enable to switch between light and dark theme.

  • The temperature panel shows a value derived from the ADC data being input on ADC channel 0 pin.

5.1.4.1. Launching the EV Charging HMI

  1. To launch the EV Charging HMI demo, click on the EV Charging widget in the apps scroll menu.

  2. Click on the Start charging button to emulate charging of EV. This will increment charge percentage at fixed time intervals.

    ../../_images/ti-lvgl-demo-ev-charging1.png ../../_images/ti-lvgl-demo-ev-charging2.png

5.1.4.2. Launching the Arm analytics

  1. Launch the Arm Analytics demo by clicking the Arm Analytics widget in the apps scroll menu.

  2. Connect the microphone and click the Play button to start audio recognition.

    ../../_images/ti-lvgl-demo-arm-analytics1.png
  3. Expose multiple audio sources to the microphone to view the output results. Click the Stop button to stop audio recognition.

    ../../_images/ti-lvgl-demo-arm-analytics2.png ../../_images/ti-lvgl-demo-arm-analytics3.png

Technical Details:

The Arm Analytics demo leverages machine learning for real-time audio recognition:

  • ML Framework: The demo uses TensorFlow Lite (LiteRT) as the deep learning runtime for efficient on-device inference on Arm Cortex-A cores

  • Pipeline Management: NNStreamer is used to manage the neural network pipeline, providing seamless integration between audio capture and ML inference through GStreamer plugins

For more information on the underlying technologies:

5.1.4.3. Launching the Smart Home HMI

To launch the Smart Home HMI demo, click on the Smart Home widget in the apps scroll menu.

Understanding the MQTT setup of Smart Home
  • All MQTT messages that are sent/received in this demo are to/from broker.hivemq.com over port 8883.

  • MQTT communication example between the demo HMI and online MQTT client can be found in the following images:

  • Please note that the broker service used for this demo is free of charge, however, other broker services can be used as well and here are the necessary changes required in ti-lvgl-demo/lv_port_linux/lvgl/demos/high_res/

    /* In mqtt_temp_pub_init() function in adc.c AND
       in mqtt_sub_init() function in mqtt_sub.c*/
    
    //Remove the following line if using unencrypted communication, else,
    //Update with path of the broker certificate in the filesystem.
    mosquitto_tls_set(mosq, "/usr/share/ti-lvgl-demo/cert/AmazonRootCA1.pem", NULL, NULL, NULL, NULL);
    
    //Replace 8883 with 1883 for unencrypted communication
    //Replace "broker.hivemq.com" with URL/IP of the broker to be used
    rc = mosquitto_connect(mosq, "broker.hivemq.com", 8883, 60);
    
  • All messages transmitted/received are SSL-encrypted MQTT messages.

  • To interact with the HMI remotely, user can use any interface (mobile-app/web-app/website) that implements transmitting/receiving MQTT messages over internet. To do this, just set broker to broker.hivemq.com on that interface and subscribe to or publish on the below mentioned topics:

    • Remote device can subscribe to topic: SmartHome/temp

    • Remote device can subscribe to topic: SmartHome/evCharge

    • Remote device can publish to topic: SmartHome/volume

    • Remote device can publish to topic: SmartHome/led

  • Note that there is no restriction on who can publish/subscribe to the above topics. That means that one device can receive data published from some other remote application as well. Concurrent usage by other users on same MQTT topic may impact your GUI. To minimize any issues, try to use unique MQTT topic names, like <unique ID>/SmartHome/<widget>. The topics can be changed at following locations in ti-lvgl-demo/lv_port_linux/lvgl/demos/high_res/:

    /* In  on_connect_vol_sub() function in mqtt_sub.c*/
    rc = mosquitto_subscribe(mosq, NULL, "SmartHome/volume", 1);
    :
    rc = mosquitto_subscribe(mosq, NULL, "SmartHome/led", 1);
    
    /* In  publish_sensor_data() function in adc.c*/
    rc = mosquitto_publish(mosq, NULL, "SmartHome/temp", strlen(payload), payload, 1, false);
    
    /* In  publish_evCharge_data() function in adc.c*/
    rc = mosquitto_publish(mosq, NULL, "SmartHome/evCharge", strlen(payload), payload, 1, false);
    

Note

By default CC33xx is configured at boot, so here are the steps that can be followed to enable it. If you are running as non-root user, run the following using sudo:

root@<machine>:~ systemctl stop ti-lvgl-demo
root@<machine>:~  cd /usr/share/cc33xx
root@<machine>:~  ./sta_start.sh
root@<machine>:~  ./sta_connect.sh -s WPA-PSK -n <SSID> -p <PASSWORD>
root@<machine>:~  udhcpc -i wlan0
root@<machine>:~  systemctl start ti-lvgl-demo

For more details on how to enable CC33xx and connect to WiFi, visit How to Enable M.2-CC33x1 in Linux

The application includes the following widgets:

Widget#1: Climate Control

Note

This feature will work on platforms that have on-chip ADC. Following is supported on AM62Lx

  • The indoor temperature in this widget displays the digital data obtained from ADC and display (data/10) on the widget.

  • The outdoor temperature below the indoor temperature shows the value of (data/10)-6.5, if it is positive, else, shows zero.

  • The indoor temperature is sent over SSL-encrypted MQTT messages under the topic SmartHome/temp

  • This demo uses channel 0 for ADC input. To change the channel being used, modify the following in

    ti-lvgl-demo/lv_port_linux/lvgl/demos/high_res/adc.c

FILE *fp = popen("cat /sys/bus/iio/devices/iio\:device0/in_voltage0_raw", "r");

Widget#2: Charging

  • The data shown in this widget is the same that is shown in the EV Charging HMI app.

  • This percentage completion data is also sent over SSL-encrypted MQTT messages under the topic SmartHome/evCharge

Widget#3: Lock

Note

Lock screen feature has only been enabled on AM62L

  • Sliding the lock to the right will lock the screen (disable all screen input)

  • To unlock, press the SW5: User Button on the TMDS62LEVM

Widget#4: Speaker

  • The play/pause button will play noise in the McASP device.

  • Custom audio filecan also be played by making necessary changes as shown below in

    ti-lvgl-demo/lv_port_linux/lvgl/demos/high_res/audio.c

    /* Copy the audio file in the SD file system */
    /* In audio_play() function in audio.c */
    
    //Modify the following as per the specification of the audio file
    rate     = 48000; //in Hz
    channels = 1;     //1: mono, 2:stereo
    seconds  = 1;     //duration of audio
    :
    :
    //Replace "/usr/share/sounds/alsa/Noise.wav" with the path of the audio file
    char *filename_wav = "/usr/share/sounds/alsa/Noise.wav";
    
  • Volume can be controlled from the vertical slider on the right-side of the widget.

  • Volume can also be set by sending values between 1 to 100 over MQTT topic SmartHome/volume from remote device over internet.

Widget#5: Main Light

  • The Light temperature slider will increase/decrease the User LED blinking frequency.

  • The left-end of slider (0 K) toggles LED every 250ms and the right-end of slider (20000 K) toggles LED every 20ms.

  • Light temperature can also be set by sending values between 0 to 20000 over MQTT topic SmartHome/led from remote device over internet.

  • In HMI, the slider Light temperature is not associated with any functionality but can be programmed be user to perform any function.

Widget#6: Sensor Controls

  • The buttons/sliders in this widget are not associated with any functionality but can be programmed by the user to perform any function.

5.1.4.4. Launching the Smart Meter HMI

To launch the Smart Meter HMI demo, click on the Smart Meter widget in the apps scroll menu.

5.1.4.5. Launching the Thermostat HMI

To launch the Thermostat HMI demo, click on the Thermostat widget in the apps scroll menu.

5.1.4.6. Launching the Security HMI

To launch the Security HMI demo, click on the Security widget in the apps scroll menu.

This widget contains a slide-show on Application Processor Security for AM6X devices.

5.1.5. Building the TI LVGL Demo from Sources

The TI LVGL Demo is enabled in tisdk-default-image yocto filesystem for AM62Lx by default.

Note, that the binary itself does not have asset images and slides built in it. The image contains the required assets within /usr/share/ti-lvgl-demo/. Place any additional assets here while making any modifications.

Yocto recipe for building this demo can be found at github: ti-lvgl-demo.bb

The source code is available at TI LVGL Demo and can be re-compiled with the following steps:

  1. First clone the appropriate git repository and its submodules using:

    $ git clone --recurse-submodules https://github.com/TexasInstruments/ti-lvgl-demo.git
    
  2. Create the docker environment and build the application:

    $ cd ti-lvgl-demo
    $ sudo ./scripts/docker_setup.sh --create-image
    $ sudo ./scripts/docker_setup.sh --build-app
    
  3. Copy the compiled binary to /usr/bin directory of the device

    $ scp lv_port_linux/bin/lvglsim root@<ip-addr-of-device>:/usr/bin/
    $ scp -r lv_port_linux/demos/high_res/assets/* root@<ip-addr-of-device>:/usr/share/ti-lvgl-demo/assets/  #make sure assets directory is there on target
    $ scp -r lv_port_linux/demos/high_res/slides/* root@<ip-addr-of-device>:/usr/share/ti-lvgl-demo/slides/  #make sure slides directory is there on target
    $ scp lv_port_linux/certs/<certificate> root@<ip-addr-of-device>:/usr/share/ti-lvgl-demo/cert/           #make sure cert directory is there on target