3.2.2.2. Crypto
3.2.2.2.1. Introduction
The Crypto API Driver is a set of Linux drivers that provide access to the hardware cryptographic accelerators available on AM62L devices. These drivers are available built-in in the kernel in the current SDK release.
Following are the Hardware accelerators supported on the following devices:
* AM62LX : Encryption - AES-ECB, AES-CBC, AES-XTS, AES-CTR
Encryption with Authentication - AES-GCM, AES-CCM
Hashing - MD5, SHA224, SHA256, SHA384, SHA512
Message Authentication - HMAC(MD5), HMAC(SHA224), HMAC(SHA256), HMAC(SHA384), HMAC(SHA512)
3.2.2.2.2. Building the Drivers
For devices with available cryptographic hardware accelerators, a Linux driver and additionally a Cryptodev kernel module (for OpenSSL) is used to access them. Other devices use the pure software implementation of these cryptographic operations.
AM62Lx SoC supports a hardware accelerator called DATA TRANSFORM AND HASHING ENGINE (DTHE) v2 for crypto operations.
The kernel configuration has already been set up in the SDK and no further configuration is needed for the drivers to be built-in to the kernel.
For reference, the configuration details are shown below. The configuration of the cryptographic drivers is done under the Hardware crypto devices sub-menu of the Cryptographic API menu in the kernel configuration.
Symbol: CRYPTO_DEV_TI_DTHEV2 [=m]
| Type : tristate
| Prompt: Support for TI security accelerator
| Location:
| -> Cryptographic API (CRYPTO [=y])
| (1) -> Hardware crypto devices (CRYPTO_HW [=y])
To check if DTHEv2 module is properly installed, run the below command from the Linux command prompt:
lsmod | grep dthev2
Output should show something similar to below:
dthev2 262144 0
Build the Cryptodev kernel module using SDK
For using OpenSSL to access the Crypto Hardware Accelerator Drivers above, the Cryptodev is required (can be built as module). The framework is not officially in the kernel and was ported to Linux under the name “cryptodev”. It is built as part of the SDK and no further configuration is needed.
3.2.2.2.3. Using Cryptographic Hardware Accelerators from OpenSSL
In order to use these drivers from OpenSSL, a special driver is available which abstracts the access to these accelerators through Cryprodev module.
Cryptodev is itself a special device driver which provides a general interface for higher level applications such as OpenSSL to access hardware accelerators.
The filesystem which comes with the SDK comes built with the Cryptodev kernel modules and the TI driver which directly accesses the hardware accelerators is built into the kernel.
The following shows the command used to query the system for the state of the cryptodev module.
root@evm:~# lsmod | grep cryptodev
cryptodev 11962 0
The following example demonstrates the OpenSSL built-in speed test to demonstrate performance. The addition of the parameter -engine devcrypto tells OpenSSL to use the Cryptodev driver if it exists.
root@evm:~# openssl speed -evp aes-128-cbc -engine devcrypto
Engine "devcrypto" set.
Doing AES-128-CBC ops for 3s on 16 size blocks: 37316 AES-128-CBC ops in 0.00s
Doing AES-128-CBC ops for 3s on 64 size blocks: 37305 AES-128-CBC ops in 0.00s
Doing AES-128-CBC ops for 3s on 256 size blocks: 37503 AES-128-CBC ops in 0.00s
Doing AES-128-CBC ops for 3s on 1024 size blocks: 37504 AES-128-CBC ops in 0.00s
Doing AES-128-CBC ops for 3s on 8192 size blocks: 18784 AES-128-CBC ops in 0.00s
Doing AES-128-CBC ops for 3s on 16384 size blocks: 18701 AES-128-CBC ops in 0.00s
version: 3.2.3
built on: Tue Sep 3 12:52:35 2024 UTC
options: bn(64,64)
compiler: aarch64-oe-linux-gcc -mbranch-protection=standard --sysroot=recipe-sysroot -O2 -pipe -g -feliminate-unused-debug-types -fcanon-prefix-map -fmacro-prefix-map= -fdebug-prefix-map= -fmacro-prefix-mapG
CPUINFO: OPENSSL_armcap=0xbd
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes 16384 bytes
AES-128-CBC infk infk infk infk infk infk
Using the Linux time -v function gives more information about CPU usage during the test.
root@evm:~# time -v openssl speed -evp aes-128-cbc -engine devcrypto
Engine "devcrypto" set.
Doing AES-128-CBC ops for 3s on 16 size blocks: 37194 AES-128-CBC ops in 0.00s
Doing AES-128-CBC ops for 3s on 64 size blocks: 37406 AES-128-CBC ops in 0.00s
Doing AES-128-CBC ops for 3s on 256 size blocks: 37455 AES-128-CBC ops in 0.00s
Doing AES-128-CBC ops for 3s on 1024 size blocks: 37503 AES-128-CBC ops in 0.00s
Doing AES-128-CBC ops for 3s on 8192 size blocks: 18744 AES-128-CBC ops in 0.01s
Doing AES-128-CBC ops for 3s on 16384 size blocks: 18727 AES-128-CBC ops in 0.01s
version: 3.2.3
built on: Tue Sep 3 12:52:35 2024 UTC
options: bn(64,64)
compiler: aarch64-oe-linux-gcc -mbranch-protection=standard --sysroot=recipe-sysroot -O2 -pipe -g -feliminate-unused-debug-types -fcanon-prefix-map -fmacro-prefix-map= -fdebug-prefix-map= -fmacro-prefix-mapG
CPUINFO: OPENSSL_armcap=0xbd
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes 16384 bytes
AES-128-CBC infk infk infk infk 15355084.80k 30682316.80k
Command being timed: "openssl speed -evp aes-128-cbc -engine devcrypto"
User time (seconds): 0.02
System time (seconds): 11.40
Percent of CPU this job got: 62%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 18.42s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 23760
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 329
Voluntary context switches: 187095
Involuntary context switches: 95
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
When the cryptodev driver is removed, OpenSSL reverts to the software implementation of the crypto algorithm. The performance using the software only implementation can be compared to the previous test.
root@evm:~# modprobe -r cryptodev
root@evm:~# time -v openssl speed -evp aes-128-cbc
Doing AES-128-CBC ops for 3s on 16 size blocks: 18675602 AES-128-CBC ops in 2.99s
Doing AES-128-CBC ops for 3s on 64 size blocks: 14189260 AES-128-CBC ops in 2.99s
Doing AES-128-CBC ops for 3s on 256 size blocks: 7121339 AES-128-CBC ops in 2.98s
Doing AES-128-CBC ops for 3s on 1024 size blocks: 2437075 AES-128-CBC ops in 2.99s
Doing AES-128-CBC ops for 3s on 8192 size blocks: 340806 AES-128-CBC ops in 2.98s
Doing AES-128-CBC ops for 3s on 16384 size blocks: 171986 AES-128-CBC ops in 2.98s
version: 3.2.3
built on: Tue Sep 3 12:52:35 2024 UTC
options: bn(64,64)
compiler: aarch64-oe-linux-gcc -mbranch-protection=standard --sysroot=recipe-sysroot -O2 -pipe -g -feliminate-unused-debug-types -fcanon-prefix-map -fmacro-prefix-map= -fdebug-prefix-map= -fmacro-prefix-mapG
CPUINFO: OPENSSL_armcap=0xbd
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes 16384 bytes
AES-128-CBC 99936.33k 303716.60k 611766.03k 834637.06k 936873.41k 945576.72k
Command being timed: "openssl speed -evp aes-128-cbc"
User time (seconds): 17.91
System time (seconds): 0.04
Percent of CPU this job got: 99%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 18.02s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 24304
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 324
Voluntary context switches: 1
Involuntary context switches: 24
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
3.2.2.2.4. Using the True Random Number Generator (TRNG) Hardware Accelerator
The pre-built kernel included within the SDK already has the OP-TEE TRNG driver enabled. You do not need any further configuration.
Verify that the optee-rng driver is loaded:
root@am62lxx-evm:~# cat /sys/class/misc/hw_random/rng_current
optee-rng
The hwrng device should now show up in the filesystem.
root@am62lxx-evm:~# ls -l /dev/hwrng
crw------- 1 root root 10, 183 Jan 1 2000 /dev/hwrng
Use cat on this device to generate random numbers.
root@am62lxx-evm:~# cat /dev/hwrng | od -x
0000000 b2bd ae08 4477 be48 4836 bf64 5d92 01c9
0000020 0cb6 7ac5 16f9 8616 a483 7dfd 6bf4 3aa5
0000040 d693 db24 d917 5ee7 feb7 34c3 34e9 e7a5
0000060 36b7 ea85 fc17 0e66 555c 0934 7a0c 4c69
0000100 523b 9f21 1546 fddb d58b e5ed 142a 6712
0000120 8d76 8f80 a6d2 30d8 d107 32bc 7f45 f997
0000140 9d5d 0d0c f1f0 64f9 a77f 408f b0c1 f5a0
0000160 39c6 f0ae 4b59 1a76 84a7 a364 8964 f557
root@am62lxx-evm:~#
Test the random number generator on the target.
root@am62lxx-evm:~# cat /dev/hwrng | rngtest -c 1000
rngtest 6.16
Copyright (c) 2004 by Henrique de Moraes Holschuh
This is free software; see the source for copying conditions. There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
rngtest: starting FIPS tests...
rngtest: bits received from input: 20000032
rngtest: FIPS 140-2 successes: 999
rngtest: FIPS 140-2 failures: 1
rngtest: FIPS 140-2(2001-10-10) Monobit: 0
rngtest: FIPS 140-2(2001-10-10) Poker: 0
rngtest: FIPS 140-2(2001-10-10) Runs: 0
rngtest: FIPS 140-2(2001-10-10) Long run: 1
rngtest: FIPS 140-2(2001-10-10) Continuous run: 0
rngtest: input channel speed: (min=72.965; avg=3848.070; max=9765625.000)Kibits/s
rngtest: FIPS tests speed: (min=10.794; avg=53.373; max=54.967)Mibits/s
rngtest: Program run time: 5710839 microseconds
root@am62lxx-evm:~#
Note that the results might be slightly different on your system, since, after all, we are dealing with a random number generator. Any appreciable number of errors typically indicates a bad random number generator.
If you’re satisfied the random number generator is working correctly,
you can use rngd (the random number generator daemon) to feed the
/dev/random entropy pool.
3.2.2.2.5. Hardware Accelerator testing
3.2.2.2.5.1. Testing using the tcrypt module
root@am62lxx-evm:~# modprobe tcrypt mode=500 sec=1
[ 1012.121422] tcrypt: testing speed of async ecb(aes) (ecb-aes-dthev2) encryption
[ 1012.128872] tcrypt: test 0 (128 bit key, 16 byte blocks): 4931 operations in 1 seconds (78896 bytes)
[ 1013.138110] tcrypt: test 1 (128 bit key, 64 byte blocks): 4940 operations in 1 seconds (316160 bytes)
[ 1014.146146] tcrypt: test 2 (128 bit key, 128 byte blocks): 4940 operations in 1 seconds (632320 bytes)
[ 1015.154298] tcrypt: test 3 (128 bit key, 256 byte blocks): 4940 operations in 1 seconds (1264640 bytes)
[ 1016.162329] tcrypt: test 4 (128 bit key, 1024 byte blocks): 4980 operations in 1 seconds (5099520 bytes)
[ 1017.170491] tcrypt: test 5 (128 bit key, 1424 byte blocks): 4940 operations in 1 seconds (7034560 bytes)
[ 1018.178486] tcrypt: test 6 (128 bit key, 4096 byte blocks): 4960 operations in 1 seconds (20316160 bytes)
[ 1019.186570] tcrypt: test 7 (192 bit key, 16 byte blocks): 4960 operations in 1 seconds (79360 bytes)
[ 1020.194482] tcrypt: test 8 (192 bit key, 64 byte blocks): 4940 operations in 1 seconds (316160 bytes)
[ 1021.202151] tcrypt: test 9 (192 bit key, 128 byte blocks): 5000 operations in 1 seconds (640000 bytes)
[ 1022.210225] tcrypt: test 10 (192 bit key, 256 byte blocks): 4940 operations in 1 seconds (1264640 bytes)
[ 1023.218410] tcrypt: test 11 (192 bit key, 1024 byte blocks): 5000 operations in 1 seconds (5120000 bytes)
[ 1024.226494] tcrypt: test 12 (192 bit key, 1424 byte blocks): 5000 operations in 1 seconds (7120000 bytes)
[ 1025.234490] tcrypt: test 13 (192 bit key, 4096 byte blocks): 4980 operations in 1 seconds (20398080 bytes)
[ 1026.242625] tcrypt: test 14 (256 bit key, 16 byte blocks): 4940 operations in 1 seconds (79040 bytes)
[ 1027.250155] tcrypt: test 15 (256 bit key, 64 byte blocks): 4960 operations in 1 seconds (317440 bytes)
[ 1028.258293] tcrypt: test 16 (256 bit key, 128 byte blocks): 4940 operations in 1 seconds (632320 bytes)
[ 1029.266342] tcrypt: test 17 (256 bit key, 256 byte blocks): 4940 operations in 1 seconds (1264640 bytes)
[ 1030.274405] tcrypt: test 18 (256 bit key, 1024 byte blocks): 4960 operations in 1 seconds (5079040 bytes)
[ 1031.282506] tcrypt: test 19 (256 bit key, 1424 byte blocks): 4980 operations in 1 seconds (7091520 bytes)
[ 1032.294641] tcrypt: test 20 (256 bit key, 4096 byte blocks): 4980 operations in 1 seconds (20398080 bytes)
[ 1033.302656] tcrypt: testing speed of async ecb(aes) (ecb-aes-dthev2) decryption
[ 1033.310809] tcrypt: test 0 (128 bit key, 16 byte blocks): 4940 operations in 1 seconds (79040 bytes)
[ 1034.318058] tcrypt: test 1 (128 bit key, 64 byte blocks): 4960 operations in 1 seconds (317440 bytes)
[ 1035.326153] tcrypt: test 2 (128 bit key, 128 byte blocks): 4940 operations in 1 seconds (632320 bytes)
[ 1036.334354] tcrypt: test 3 (128 bit key, 256 byte blocks): 4940 operations in 1 seconds (1264640 bytes)
[ 1037.342372] tcrypt: test 4 (128 bit key, 1024 byte blocks): 4920 operations in 1 seconds (5038080 bytes)
[ 1038.350475] tcrypt: test 5 (128 bit key, 1424 byte blocks): 4940 operations in 1 seconds (7034560 bytes)
[ 1039.358415] tcrypt: test 6 (128 bit key, 4096 byte blocks): 4940 operations in 1 seconds (20234240 bytes)
[ 1040.366508] tcrypt: test 7 (192 bit key, 16 byte blocks): 4940 operations in 1 seconds (79040 bytes)
[ 1041.374071] tcrypt: test 8 (192 bit key, 64 byte blocks): 4960 operations in 1 seconds (317440 bytes)
[ 1042.382158] tcrypt: test 9 (192 bit key, 128 byte blocks): 4960 operations in 1 seconds (634880 bytes)
[ 1043.390282] tcrypt: test 10 (192 bit key, 256 byte blocks): 4940 operations in 1 seconds (1264640 bytes)
[ 1044.398466] tcrypt: test 11 (192 bit key, 1024 byte blocks): 4940 operations in 1 seconds (5058560 bytes)
[ 1045.406558] tcrypt: test 12 (192 bit key, 1424 byte blocks): 4940 operations in 1 seconds (7034560 bytes)
[ 1046.414503] tcrypt: test 13 (192 bit key, 4096 byte blocks): 4940 operations in 1 seconds (20234240 bytes)
[ 1047.422793] tcrypt: test 14 (256 bit key, 16 byte blocks): 4960 operations in 1 seconds (79360 bytes)
[ 1048.430409] tcrypt: test 15 (256 bit key, 64 byte blocks): 4960 operations in 1 seconds (317440 bytes)
[ 1049.438295] tcrypt: test 16 (256 bit key, 128 byte blocks): 4940 operations in 1 seconds (632320 bytes)
[ 1050.446313] tcrypt: test 17 (256 bit key, 256 byte blocks): 4940 operations in 1 seconds (1264640 bytes)
[ 1051.454411] tcrypt: test 18 (256 bit key, 1024 byte blocks): 4960 operations in 1 seconds (5079040 bytes)
[ 1052.462508] tcrypt: test 19 (256 bit key, 1424 byte blocks): 4960 operations in 1 seconds (7063040 bytes)
[ 1053.470497] tcrypt: test 20 (256 bit key, 4096 byte blocks): 4960 operations in 1 seconds (20316160 bytes)
...