2.3. Yocto Layer Configuration

Processor SDK uses oe-layersetup configuration files to initialize the Yocto build environment. Configure your build with the following command:

$ ./oe-layertool-setup.sh -f <config>

Replace <config> with one of the following configuration files.

The oe-layersetup git repository has the following configuration files in the configs/processor-sdk directory.

Table 2.2 Yocto Layer Configuration

Config File

Description

Supported machines/platforms

processor-sdk-scarthgap-nonqt-11.02.08.02-config.txt

Used for building Yocto based filesystem

am62lxx-evm

processor-sdk-scarthgap-evse-11.02.08.03-config.txt

Used for building Yocto based filesystem with AM62L-EVSE-DEV-EVM support (for EV charging Use cases)

am62lxx-evm