2. Setting Up Robotics SDK
This section describes how to set up the Robotics SDK on the Processor SDK Linux for Edge AI.
2.1. Requirements & Dependencies
2.1.1. Supported Hardware Platforms
Platform |
EVM |
---|---|
2.1.2. Processor SDK Linux for Edge AI
The Robotics SDK requires the SD card image from Processor SDK Linux for Edge AI:
Platform |
Link to Processor SDK Linux |
---|---|
AM62A |
Processor SDK Linux for AM62A (Version 10.1.0.X) |
The SD card image contains Processor SDK Linux and libraries that are necessary for setting up the Robotics SDK environment.
2.1.3. Ubuntu PC
A Ubuntu PC is required for visualization of ROS topics published from the TI EdgeAI Starter Kit (SK) board. We have tested only with native x86_64 Ubuntu PCs and have not tested with any other Ubuntu systems: including Ubuntu virtual machines and Docker Desktop on Mac or Windows.
It is assumed that a matching ROS distro (ROS 2 Humble) is installed on the remote Ubuntu PC, either in the host Ubuntu filesystem natively or in a Docker container. In case you want to install ROS natively on the remote Ubuntu filesystem:
For ROS 2 Humble installation steps, please refer to this ROS 2 documentation.
We also provide Dockerfiles (docker/Dockerfile.x86_64.humble
) that can build and run on the remote Ubuntu PC for ROS 2 Humble, with detailed steps for setting up the Docker environment on the remote PC. For installation of Docker on the Ubuntu PC, the following links may be useful:
2.1.4. Cameras
The Robotics SDK provides camera ROS nodes for USB mono cameras (Logitech C270, C920, C922) and CSI cameras including IMX219 and IMX390. All the demo applications can be tried out with a live camera as well as with a ROSBAG file that is provided with the SDK.
For configuration of a USB mono camera, please see ros2/drivers/mono_capture/README.
For configuration of CSI cameras, please see this section of Processor SDK Linux documentation.
For GStreamer camera ROS node (USB cameras are also supported), please see ros2/drivers/gscam2/README_TI
2.2. Set Up Development Environment on the Target
Figure 1 shows the hardware setup and high-level installation steps on the target SK board and the Ubuntu PC. The target SK board and the remote Ubuntu PC are assumed to be connected on the same network through Ethernet.
2.2.1. Build SD Card
From the Ubuntu PC, download the SD card image (
tisdk-edgeai-image-<platform>-evm.wic.xz
) from Processor SDK Linux (using the links provided in Section 1.2).Flash the downloaded image to an SD card (minimum 32GB, high-performance) using the Balena Etcher tool. For detailed instructions, please refer to this section.
2.2.2. Connect Remotely to the Target
To find the target IP address assigned to the EVM, use a serial port communications program (for example,
sudo minicom -D /dev/ttyUSBx
where/dev/ttyUSBx
is the device for the UART serial port), log in withroot
account, and runifconfig
.From a terminal on the PC, open an SSH session to connect remotely to the target:
user@pc:~$ ssh root@<target_IP_address>
Tip
It is recommended to use a static IP for the SK board to make ROS network setting easy.
2.2.3. Initial Setup for the Robotics SDK
2.2.3.1. On the SK Board
You can run the installation script on the target as follows:
root@am6x-sk:~$ cd /opt/edgeai-gst-apps/scripts
root@am6x-sk:~$ source ./install_robotics_sdk.sh
This script takes care of:
Cloning the main GIT repository for Robotics SDK under
/opt/robotics_sdk
Setting up the folders for evaluating the Robotics SDK under
$HOME/j7ros_home
Downloading ROSBAG and other data files
Downloading several deep-learning models from the edge AI model zoo. You can also use the model downloader tool (please refer to this section of Edge AI documentation).
2.2.3.2. On the Remote Ubuntu PC
In a similar way, you can use a script to set up on the remote Ubuntu PC for visualization:
user@pc:~$ wget -O init_setup.sh https://raw.githubusercontent.com/TexasInstruments/edgeai-robotics-sdk/master/init_setup.sh
user@pc:~$ source ./init_setup.sh REL.10.01.00
Note
In a proxy network, in case the wget
command above does not work, you can try again with adding --proxy off
argument:
user@pc:~$ wget --proxy off -O init_setup.sh https://raw.githubusercontent.com/TexasInstruments/edgeai-robotics-sdk/master/init_setup.sh
2.2.4. Set Up Docker Environment on the Target
The Robotics SDK runs in a Docker container environment on the Processor SDK Linux. In the Robotics SDK Docker environment, ROS and necessary libraries and tools are installed.
First, following this link, please check that Docker and network work correctly on the target SK board.
The following section describes the Docker environment setup, details of building, and running apps under Docker. Please note that it will take several minutes to build the Docker image. The Docker image built can be listed with docker images
.
Note
Proxy Network: If the board running the Docker container is behind a proxy server, the default settings for downloading files and installing packages via apt-get
may not work, and proper settings for proxy should be established for building and running the SDK Docker image.