5. Examples and Demos¶
Applications available by development platform
There are a number of Example Applications provided within the Processor SDK for Linux. Below are the applications available on each platform and the User’s Guides associated with each component.
Note
The example applications below assume that you are using the default pinmux/profile configuration that the board ships with, unless otherwise noted in the individual application’s User’s Guide
Applications |
Users Guide |
Description |
||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Matrix GUI |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
Provides an overview and details of the graphical user interface (GUI) implementation of the application launcher provided in the Sitara Linux SDK |
|
Power & Clocks |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
Provides details of power management features for all supported platforms. |
|
Multimedia |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
Provides details on implementing ARM/Neon based multimedia using GStreamer pipelines and FFMPEG open source codecs. |
|||||||
Accelerated Multimedia |
X |
X |
X |
X |
X |
X |
X |
X |
Provides details on hardware accelerated (IVAHD/VPE/DSP) multimedia processing using GStreamer pipelines. |
|||||||||||
Graphics |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
Provides details on hardware accelerated 3D graphics demos. |
|||||||
OpenCL |
X |
X |
X |
X |
Provides OpenCL example descriptions. Matrix GUI provides two out of box OpenCL demos: Vector Addition and Floating Point Computation. |
|||||||||||||||
Camera |
X |
X |
X |
X |
X |
X |
X |
Provides details on how to support smart sensor camera sensor using the Media Controller Framework |
||||||||||||
Video Analytics |
Demonstrates the capability of AM57x for video analytics. It builds on Qt and utilizes various IP blocks on AM57x. |
|||||||||||||||||||
DLP 3D Scanner |
Demonstrates the capability of AM57x for DLP 3D scanning. |
|||||||||||||||||||
Simple People Tracking |
X |
X |
X |
X |
X |
X |
Demonstrates the capability of people tracking and detection with TI?s ToF (Time-of-Flight) sensor |
|||||||||||||
Barcode Reader |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
Demonstrates the capability of detecting and decoding barcodes |
||||||
USB Profiler |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
NA |
|
ARM Benchmarks |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
NA |
|
Display |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
NA |
|||||||||
WLAN and Bluetooth |
X |
X |
X |
X |
X |
Provides details on how to enable the WL1271 daughtercard which is connected to the EVM |
||||||||||||||
QT Demos |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
Provides out of box Qt5.4 demos from Matrix GUI, including Calculator, Web Browser, Deform (shows vector deformation in the shape of a lens), and Animated Tiles. |
|||||||
Web Browser |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
NA |
|||||||
System Settings |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
NA |
|
EVSE Demo |
X |
X |
X |
X |
X |
X |
X |
X |
Provides out of box demo to showcase Human Machine Interface (HMI) for Electric Vehicle Supply Equipment(EVSE) Charging Stations. |
|||||||||||
Protection Relay Demo |
X |
X |
X |
Matrix UI provides out of box demo to showcase Human Machine Interface (HMI) for Protection Relays. |
||||||||||||||||
mmWave Gesture Controlled HMI |
X |
X |
X |
X |
X |
X |
X |
X |
Gesture controlled HMI based on mmWave gesture recognition and presence detection |
Provides out of box demo to showcase gesture controlled Human Machine Interface (HMI). |
||||||||||
Predictive Maintenance (PdM) demo |
X |
X |
X |
X |
X |
X |
X |
X |
Provides out of box demo for Predictive Maintenance using Recurrent Neural Network (RNN) for anomaly detection. |
|||||||||||
Qt5 Thermostat HMI Demo |
X |
X |
X |
X |
X |
X |
X |
X |
Provides out of box Qt5-based HMI for Thermostat |
|||||||||||
TI Deep Learning |
X |
X |
X |
X |
Provides TI Deep Learning examples |
|||||||||||||||
Arm NN |
X |
X |
X |
X |
X |
X |
X |
X |
X |
Demonstrates Arm NN classification with MobileNet model |
- 5.1. Matrix User Guide
- 5.2. Sub-system Demos
- 5.3. Application Demos
- 5.3.1. Qt5 Thermostat HMI Demo
- 5.3.2. Predictive Maintenance Demo
- 5.3.3. DLP 3D Scanner
- 5.3.4. People Tracking
- 5.3.5. EVSE Demos
- 5.3.6. Protection Relay Demo
- 5.3.7. mmWave Gesture Controlled HMI
- 5.3.8. TIDL Demo
- 5.3.9. Arm NN Classification Demo