2.3. Yocto Layer Configuration
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layertool-setup.sh -f <config>
The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.
Config File |
Description |
Supported machines/platforms |
|---|---|---|
processor-sdk-scarthgap-11.02.05.02-config.txt |
Processor SDK 11.02.05.02 Release |
am335x-evm, am437x-evm, am65xx-hs-evm |
processor-sdk-scarthgap-11.02.08.02-config.txt |
Processor SDK 11.02.08.02 Release |
am64xx-evm, am62xx-evm, am62xx-lp-evm, am62xxsip-evm, am62lxx-evm, am62pxx-evm, am62dxx-evm |