3.1.2.8. UART
This section documents how to use the UART to load files to boot the board into U-Boot. After that the user is expected to know how they want to continue loading files.
3.1.2.8.1. Booting U-Boot from the console UART
In some cases we support loading SPL and U-Boot over the console UART.
You will need to use the u-boot-spl.bin and u-boot.img files to boot.
As per the TRM, the file is to be loaded via the X-MODEM
protocol at 115200 baud 8 stop bits no parity (same as using it for
console). SPL in turn expects to be sent u-boot.img at the same rate
but via Y-MODEM. An example session from the host PC, assuming console
is on ttyUSB0 and already configured would be and the lrzsz package
is installed
$ sb -kb $OUT/u-boot-spl.bin < $UART_BOOT_MAIN_UART > $UART_BOOT_MAIN_UART
$ sb -kb --ymodem $OUT/u-boot.img < $UART_BOOT_MAIN_UART > $UART_BOOT_MAIN_UART