3.2.4.10.4. Suspend/Resume

3.2.4.10.4.1. Overview

The user can deliberately force the system to low power state. There are various levels: Suspend to memory(RAM), Suspend to disk, etc. Certains parts support different levels of idle, such as DeepSleep0 or standby, which allow additional wake-up sources to be used with less wake latency at the expense of less power savings.

Source Location

The files that provide suspend/resume differ from part to part however they generally reside in arch/arm/mach-omap2/pm****.c for the higher-level code and arch/arm/mach-omap2/sleep****.S for the lower-level code.

Kernel Configuration Options

Suspend/resume can be enable or disabled within the kernel using the same method for all parts. To configure suspend/resume, enter the kernel configuration tool using:

$ make menuconfig

Select Power management options from the main menu.

...
...
Kernel Features  --->
Boot options  --->
CPU Power Management  --->
Floating point emulation  --->
Userspace binary formats  --->
Power management options  --->
[*] Networking support  --->
Device Drivers  --->
...
...

Select Suspend to RAM and standby to toggle the power management support.

[*] Suspend to RAM and standby
-*- Run-time PM core functionality
...
< > Advanced Power Management Emulation

And then build the kernel as usual.


IO Pad Configuration

In order to optimize power on the I/O supply rails, each pin can be given a “sleep” configuration in addition to it’s run-time configuration. This can be handled with the pinctrl states defined in the board device tree for each peripheral. These values are used to configure the PAD_CONF registers found in the control module of the device which allow for selection of the MUXMODE of the pin and the operation of the internal pull resistor. Typically a device defines it’s pinctrl state for normal operation:

davinci_mdio_default: davinci_mdio_default {
        pinctrl-single,pins = <
                /* MDIO */
                0x148 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0)    /* mdio_data.mdio_data */
                0x14c (PIN_OUTPUT_PULLUP | MUX_MODE0)                   /* mdio_clk.mdio_clk */
        >;
};

In order to define a sleep state for the same device, another pinctrl state can be defined:

davinci_mdio_sleep: davinci_mdio_sleep {
        pinctrl-single,pins = <
                /* MDIO reset value */
                0x148 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                0x14c (PIN_INPUT_PULLDOWN | MUX_MODE7)
        >;
};

The driver then defines the sleep state in addition to the default state:

&davinci_mdio {
        pinctrl-names = "default", "sleep";
        pinctrl-0 = <&davinci_mdio_default>;
        pinctrl-1 = <&davinci_mdio_sleep>;
        ...

Although the driver core handles selection of the default state during the initial probe of the driver, some extra work may be needed within the driver to make sure the sleep state is selected during suspend and the default state is re-selected at resume time. This is accomplished by placing calls to pinctrl_pm_select_sleep_state at the end of the suspend handler of the driver and pinctrl_pm_select_default_state at the start of the resume handler. These functions will not cause failure if the driver cannot find a sleep state so even with them added the sleep state is still default. Some drivers rely on the default configuration of the pins without any need for a default pinctrl entry to be set but if a sleep state is added a default state must be added as well in order for the resume path to be able to properly reconfigure the pins. Most TI drivers included with the 3.12 release already have this done.

The required pinctrl states will differ from board to board; configuration of each pin is dependent on the specific use of the pin and what it is connected to. Generally the most desirable configuration is to have an internal pull-down and GPIO mode set which gives minimal leakage. However, in a case where there are external pull-ups connected to the line (like for I2C lines) it makes more sense to disable the pull on the pin. The pins are supplied by several different rails which are described in the data manual for the part in use. By measuring current draw on each of these rails during suspend it may be possible to fine tune the pin configuration for maximum power savings. The AM335x EVM has pinctrl sleep states defined for its peripheral and serves as a good example.

Even pins that are not in use and not connected to anything can still leak some power so it is important to consider these pins as well when implementing the pad configuration. This can be accomplished by defining a pinctrl state for unused pins and then assigning it directly the the pinctrl node itself in the board device tree so the state is configured during boot even though there is no specific driver for these pins:

&am43xx_pinmux {
         pinctrl-names = "default";
         pinctrl-0 = <&unused_wireless>;
         ...
         unused_pins: unused_pins {
                 pinctrl-single,pins = <
                        0x80    (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_csn1.mmc1_clk */
                        ...

3.2.4.10.4.1.1. CM3 Firmware

Suspend on am335x and am437x depends on interaction between the Linux kernel and the wkup_m3, so there are several requirements when building the Linux kernel to ensure this will work. The following config options are required when building a kernel to support suspend:

# Firmware Loading from rootfs
CONFIG_FW_LOADER_USER_HELPER=y
CONFIG_FW_LOADER_USER_HELPER_FALLBACK=y

# AMx3 Power Config Options
CONFIG_MAILBOX=y
CONFIG_OMAP2PLUS_MBOX=y
CONFIG_WKUP_M3_RPROC=y
CONFIG_SOC_TI=y
CONFIG_WKUP_M3_IPC=y
CONFIG_TI_EMIF_SRAM=y
CONFIG_AMX3_PM=y

CONFIG_RTC_DRV_OMAP=y

Note that it is also possible to build all of the options under `` AMx3 Power Config Options `` as modules if desired. Finally, do not forget the steps mentioned in the CM3 Firmware section of the guide to make sure the proper firmware binary is available.

The LCPD release supports mem sleep and standby sleep. On both AM335 and AM437 mem sleep corresponds to DeepSleep0. The following wake sources are supported from DeepSleep0

  • UART
  • GPIO0
  • Touchscreen (AM335x only)

To enter DeepSleep0 enter the following at the command line:

$ echo mem > /sys/power/state

From here, the system will enter DeepSleep0. At any point, triggering one of the aforementioned wake-up sources will cause the kernel to resume and the board to exit DeepSleep0. A successful suspend/resume cycle should look like this:

$ echo mem > /sys/power/state
$ PM: Syncing filesystems ... done.
$ Freezing user space processes ... (elapsed 0.007 seconds) done.
$ Freezing remaining freezable tasks ... (elapsed 0.006 seconds) done.
$ Suspending console(s) (use no_console_suspend to debug)
$ PM: suspend of devices complete after 194.787 msecs
$ PM: late suspend of devices complete after 14.477 msecs
$ PM: noirq suspend of devices complete after 17.849 msecs
$ Disabling non-boot CPUs ...
$ PM: Successfully put all powerdomains to target state
$ PM: Wakeup source UART
$ PM: noirq resume of devices complete after 39.113 msecs
$ PM: early resume of devices complete after 10.180 msecs
$ net eth0: initializing cpsw version 1.12 (0)
$ net eth0: phy found : id is : 0x4dd074
$ PM: resume of devices complete after 368.844 msecs
$ Restarting tasks ... done
$

It is also possible to enter standby sleep with the possibility to use additional wake sources and have a faster resume time while using slightly more power. To enter standby sleep, enter the following at the command line:

$ echo standby > /sys/power/state

A successful cycle through standby sleep should look the same as DeepSleep0.

In the event that a cycle fails, the following message will be present in the log:

$ PM: Could not transition all powerdomains to target state

This is usually due to clocks that have not properly been shut off within the PER powerdomain. Make sure that all clocks within CM_PER are properly shut off and try again.

A small ARM Cortex-M3 co-processor is present on these parts that helps the SoC to get to the lowest power mode. This processor requires firmware to be loaded from the kernel at run-time for all low-power features of the SoC to be enabled. The name of the binary file containing this firmware is am335x-pm-firmware.elf for both SoCs. The git repository containing the source and pre-compiled binaries of this file can be found here: https://git.ti.com/processor-firmware/ti-amx3-cm3-pm-firmware/commits/ti-v4.1.y .

There are two options for loading the CM3 firmware. If using the CoreSDK, the firmware will be included in /lib/firmware and the root filesystem should handle loading it automatically. Placing any version of am335x-pm-firmware.elf at this location will cause it to load automatically during boot. However, due to changes in the upstream kernel it is now required that CONFIG_FW_LOADER_USER_HELPER_FALLBACK be enabled if the CONFIG_WKUP_M3_IPC is being built-in to the kernel so that the firmware can be loaded once userspace and the root filesystem becomes avaiable. It is also possible to manually load the firmware by following the instructions below:

The final option is to build the binary directly into the kernel. Note that if the firmware binary is built into the kernel it cannot be loaded using the methods above and will be automatically loaded during boot. To accomplish this, first make sure you have placed am335x-pm-firmware.elf under <KERNEL SOURCE>/firmware. Then enter the kernel configuration by typing:

$ make menuconfig

Select Device Drivers from the main menu.

...
...
Kernel Features  --->
Boot options  --->
CPU Power Management  --->
Floating point emulation  --->
Userspace binary formats  --->
Power management options  --->
[*] Networking support  --->
Device Drivers  --->
...
...

Select Generic Driver Options

Generic Driver Options
CBUS support
...
...

Configure the name of the PM firmware and the location as shown below

...
-*- Userspace firmware loading support
[*] Include in-kernel firmware blobs in the kernel binary
(am335x-pm-firmware.elf) External firmware blobs to build into the kernel binary
(firmware) Firmware blobs root directory

The CM3 firmware is needed for all idle low power modes on am335x and am437x and for cpuidle on am335x. During boot, if the CM3 firmware has been properly loaded, the following message will be displayed:

PM: CM3 Firmware Version = 0x191

3.2.4.10.4.1.1.1. CM3 Firmware Linux Kernel Interface

The kernel interface to the CM3 firmware is through the wkup_m3_rproc driver, which is used to load and boot the CM3 firmware, and the wkup_m3_ipc driver, which exposes an API to be used by the PM code to communicate with the CM3 firmware.

wkup_m3_rproc Driver

This driver is responsible for loading and booting the CM3 firmware on the wkup_m3 inside the SoC using the remoteproc framework.

Source Location:

`` drivers/remoteproc/wkup_m3_rproc.c ``

wkup_m3_ipc Driver

This driver exposes an API to be used by the PM code to provide board and SoC specific data from the kernel to the CM3 firmware, request certain power state transitions, and query the status of any previous power state transitions performed by the CM3 firmware.

Source Location:

`` drivers/soc/ti/wkup_m3_ipc.c `` - provides the wkup_m3_ipc driver responsible for communicating with the CM3 firmware.

3.2.4.10.4.1.1.2. Debugging Techniques

Debugging suspend and resume issues can be inherently difficult because by nature portions of the processor may be clock gated or powered down, making traditional methods difficult or impossible.

To aid your debugging efforts, the following resources are available:


3.2.4.10.4.1.1.3. RTC-Only and RTC+DDR Mode

RTC-Only and RTC+DDR modes are only supported on AM437x devices.

DDR3 VTT Regulator Toggling

Some boards using DDR3 have a VTT Regulator that must be shut off during suspend to further conserve power. There are two methods that can be used to toggle DDR3 VTT regulators (or any GPIO for that matter) during suspend on am335x and am437x, through the use of GPIO0 (AM335x and AM437x) or IO Isolation (AM437x only).

GPIO0 Toggling

An example of a board with this regulator is the AM335X EVM SK. On AM335x and AM437x, GPIO0 remains powered during DS0 so it is possible to use this to toggle a pin to control the VTT regulator. This is handled by the wakeup M3 processor and gets defined inside the device node within the board device tree file.

&wkup_m3_ipc {
        ti,needs-vtt-toggle;
        ti,vtt-gpio-pin = <7>;
};

ti,needs-vtt-toggle is used to indicate that the vtt regulator must be toggled and ti,vtt-gpio-pin indicates which pin within GPIO0 is connected to the VTT regulator to control it.

3.2.4.10.4.1.1.4. IO Isolation Control

Many of the pins on AM437x have the ability to configure both normal and sleep states. Because of this it is possible to use any pin with a corresponding CTRL_CONF_* register in the control module and the DS_PAD_CONFIG bits to toggle the VTT regulator enable pin. The DS state of the pin must be configured such that the pin disables the VTT regulator. The normal state of the pin must be configured such that the VTT regulator is enabled by the state alone. This is because the VTT regulator must be enabled before context is restored to the controlling GPIO.

Example:

On the AM437x GP EVM, the VTT enable line must be held low to disable VTT regulator and held high to enable, so the following pinctrl entry is used. The DS pull is enabled which uses a pull down by default and DS off mode is used which outputs a low by default. For the normal state, a pull up is specified so that the VTT enable line gets pulled high immediately after the DS states are removed upon exit from DeepSleep0.

The ti,set-io-isolation flag below in the wkup_m3_ipc node tells the CM3 firmware to place the IO’s in isolation and actually trigger the value provided in the ddr3_vtt_toggle_default pinctrl entry.

&am43xx_pinmux {
        pinctrl-names = "default";
        pinctrl-0 = <&ddr3_vtt_toggle_default>;

        ddr3_vtt_toggle_default: ddr_vtt_toggle_default {
        pinctrl-single,pins = <
                0x25C (DS0_PULL_UP_DOWN_EN | PIN_OUTPUT_PULLUP |
                       DS0_FORCE_OFF_MODE | MUX_MODE7)>;
        };
        ...
};

wkup_m3_ipc: wkup_m3_ipc@1324 {
        compatible = "ti,am4372-wkup-m3-ipc";
        ...
        ...
        '''ti,set-io-isolation;'''
        ...
};

3.2.4.10.4.1.1.5. Deep Sleep Voltage Scaling

It is possible to scale the voltages on both the MPU and CORE supply rails down to 0.95V while we are in DeepSleep once powerdomains are shut off. The i2c sequences needed to scale voltage vary from board to board and are dependent on which PMIC is in use, so we use board specific binaries that are passed to the CM3 firmware to define the sequences needed during the sleep and wake paths. The CM3 firmware is then able to write these sequences out at the proper location in the Deep Sleep path on i2c0.

The CM3 firmware at https://git.ti.com/processor-firmware/ti-amx3-cm3-pm-firmware/ti-v4.1.y/bin contains scale data binaries for these platforms:

am335x-evm-scale-data.bin

  • AM335x EVM
  • AM335x Starter kit

am335x-bone-scale-data.bin

  • AM335x Beaglebone
  • AM335x Beaglebone Black

am43x-evm-scale-data.bin

  • AM437x GP EVM
  • AM437x EPOS EVM
  • AM437x SK EVM

The name of the binary to use is specified in the wkup_m3_ipc node with the ti,scale-data-fw property of a board file like so:

/* From arch/arm/boot/dts/am437x-gp-evm.dts */
&wkup_m3_ipc {
        ...
        ti,scale-data-fw = "am43x-evm-scale-data.bin";
};

The wkup_m3_ipc driver atdrivers/soc/ti/wkup_m3_ipc.c handles loading this binary to the proper data region of the CM3 and then passing the offsets to the wake and sleep sequences through IPC register 5 to the firmware. As long as the format of the binary is proper the driver will handle this automatically.

Binary Data Format

Each binary file contains a small header with a magic number and offsets to the sleep wand wake sections and then the sleep and wake sections themsevles which consist of two bytes to specify the i2c bus speed for the operation and then blocks of bytes that specify the message. The header is 4 bytes long and is shown here:

Size (bytes) Field
2 Magic Number (0x0c57)
1 Offset to sleep data
1 Offset to wake data

Table: Scale data binary header

The offsets to the sleep and wake are counted from the first byte after the header starting at zero and point to the first of the two bytes in little-endian order that specify the bus speed in kHz. In all scale data provided by TI the i2c bus speed is specified as 0x6400, which corresponds to 100kHz. After these two bytes are the message blocks which can have a variable length. A standard message block is defined as:

Size (bytes) Field
1 Message size, counting from first byte *after* I2C Bus address below.
1 I2C Bus Address
1 First byte of message (typically I2C register address)
1 Second byte of message (typically value to write to register)
1 Nth byte of message
... ...

Table: Scale data message block

Each block is a single I2C transaction, and multiple blocks can be placed one after the other to send multiple messages, as is needed in the case of PMICs which have GO bits to actually apply the programmed voltage to the rail.


3.2.4.10.4.1.1.6. Simple Example

Single message for both sleep and wake sequence (from bin/am335x-evm-scale-data.bin).

Raw binary data using xxd:

a0274052local@uda0274052:~/git-repos/amx3-cm3$ xxd bin/am335x-evm-scale-data.bin
0000000: 0c57 0006 0034 022d 251f 0034 022d 252b  .W...4.-%..4.-%+

Explanation of values:

0c57        # Magic number
00      # Offset from first byte after header to sleep section
06      # Offset from first byte after header to wake section

0034        # Sleep sequence section, starts with two bytes to describe i2c bus in khz (100)
02 2d 25 1f # Length of message, evm i2c bus addr, then message (i2c reg 0x25, write value 0x1f)

0034        # Wake sequence section, starts with two bytes to describe i2c bus in khz (100)
02 2d 25 2b # Length of message, evm i2c bus addr, then message (i2c reg 0x25, write value 0x2b)

3.2.4.10.4.1.1.7. Advanced Example

Multiple messages on sleep and wake sequence (from bin/am43x-evm-scale-data.bin).

Raw binary data using xxd:

amx3-cm3$ xxd bin/am43x-evm-scale-data.bin
0000000: 0c57 0012 0034 0224 106b 0224 168a 0224  .W...4.$.k.$...$
0000010: 1067 0224 1a86 0034 0224 106b 0224 1699  .g.$...4.$.k.$..
0000020: 0224 1067 0224 1a86                      .$.g.$..

Explanation of values:

0C 57           # Magic number 0x0C57
00          # Offset, starting after header, to sleep sequence
12          # Offset, starting after header, to wake sequence

0034            # Sleep sequence section, starts with two bytes to describe i2c bus in khz (100)
02 24 10 6b     # msg length 0x02, to i2c addr 0x24, message is (i2c reg 0x10, write 0x6b)
02 24 16 8a     # msg length 0x02, to i2c addr 0x24, message is (i2c reg 0x16, write 0x8a)
02 24 10 67     # msg length 0x02, to i2c addr 0x24, message is (i2c reg 0x10, write 0x67)
02 24 1a 86     # msg length 0x02, to i2c addr 0x24, message is (i2c reg 0x1a, write 0x86)

0034            # Wake sequence section, starts with two bytes to describe i2c bus in khz (100)
02 24 10 6b     # msg length 0x02, to i2c addr 0x24, message is (i2c reg 0x10, write 0x6b)
02 24 16 99     # msg length 0x02, to i2c addr 0x24, message is (i2c reg 0x16, write 0x99)
02 24 10 67     # msg length 0x02, to i2c addr 0x24, message is (i2c reg 0x10, write 0x67)
02 24 1a 86     # msg length 0x02, to i2c addr 0x24, message is (i2c reg 0x1a, write 0x86)