2.3. Migration GuideΒΆ
Overview
This page covers migration information for applications built on top of the Processor SDK for Android.
Processor SDK Android 05.02.00
- This is a maintenance update release of Processor SDK Android for AM57xx with Oreo. More details about Oreo can be obtained from here.
 - See 05.02.00 Release Notes for full list of modifications.
 
Processor SDK Android 05.01.00
- This is a maintenance update release of Processor SDK Android for AM57xx with Oreo. More details about Oreo can be obtained from here
 - Multimedia with hardware acceleration is not supported
 - Video decoding up to 720p resolution
 - See 05.01.00 Release Notes for full list of modifications.
 
Processor SDK Android 05.00.00
- Linux Kernel and U-boot are updated to v4.14 and 2018.01 respectively, while the pastry continues to be Android-Oreo
 - More details about Oreo can be obtained from here
 - SD card creation now creates boot partition only with MLO, u-boot.img, and uEnv.txt. After flashing the eMMC device by Running Setup Scripts, SD card is required to boot AM57x IDKs. Keep the SD card plugged in, power cycle AM57x IDKs to use MLO and u-boot.img from the SD card and the rest from the eMMC. For AM57x GP EVM, SD card can be removed before the power cycle to boot Android with everything from the eMMC.
 - VPE is not supported
 - See 05.00.00 Release Notes for full list of modifications.
 
Processor SDK Android 04.03.00
- This is a maintenance update release of Processor SDK Android for AM57xx with Oreo. More details about Oreo can be obtained from here
 - See 04.03.00 Release Notes for full list of modifications.
 
Processor SDK Android 04.02.00
- This is the first release of the Processor SDK Android for AM57xx with Oreo. Both U-Boot and Android Kernel are the same LTS as prior Processor SDK releases, i.e. 2016.05 and 4.4 respectively.
 - More details about Oreo can be obtained from here
 - See 04.02.00 Release Notes for full list of modifications.
 
Processor SDK Android 04.01.00
- This is the final release of the Processor SDK Android for AM57xx with Marshmallow. The next release will be based on Oreo
 - See 04.01.00 Release Notes for full list of modifications.
 
Processor SDK Android 04.00.00
- This is the first release of the Processor SDK Android which supports AM57xx devices.
 - See 04.00.00 Release Notes for full list of modifications.