1.2. Building the SDK¶
1.2.1. Build PC Setup¶
Please refer to the following pages from Android documentation to setup your environment for Android build:
Getting the Repo tool
You will need the Repo tool to retrieve repositories. To install it, please refer to this webpage : https://source.android.com/setup/develop#installing-repo
Getting toolchain for u-boot builds
Links to download toolchains for building u-boot are mentioned in the SDK download page.
Install Optee-OS build dependencies
Check OPTEE OS docs to know list of dependencies needed to be installed : https://optee.readthedocs.io/en/latest/building/prerequisites.html
1.2.2. Downloading Sources¶
Create a folder for downloading all sources
mkdir ~/09_00_00 && cd $_
export YOUR_PATH=$PWD
1.2.2.1. Bootloader components¶
mkdir ${YOUR_PATH}/ti-bootloader-aosp/ && cd $_
git clone -b 08.06.00.007 git://git.ti.com/atf/arm-trusted-firmware.git
git clone -b 3.22.0-rc1 https://github.com/OP-TEE/optee_os.git
git clone -b 09.00.00.007-android git://git.ti.com/ti-u-boot/ti-u-boot.git
git clone -b 09.00.00.007 git://git.ti.com/processor-firmware/ti-linux-firmware.git
1.2.2.2. Kernel¶
Fetch the code using repo:
mkdir ${YOUR_PATH}/ti-kernel-aosp/ && cd $_
repo init -u git://git.ti.com/android/manifest.git -b android13-release -m releases/RLS_09_00_Kernel.xml
repo sync
Note
To save same disk space, pass the --depth=1 option to repo init:
repo init -u git://git.ti.com/android/manifest.git -b android13-release -m releases/RLS_09_00_Kernel.xml --depth=1
1.2.2.3. Android File System¶
Fetch the code using repo:
mkdir ${YOUR_PATH}/ti-aosp-13 && cd $_
repo init -u git://git.ti.com/android/manifest.git -b android13-release -m releases/RLS_09_00.xml
repo sync
1.2.3. Build Instructions¶
Note
The Bootloader and Kernel builds below are optional if they are used as is from TI release. Prebuilt copies of these
binaries are already part of Android file system sources in device/ti/am62x-kernel and
vendor/ti/am62x/bootloader folder.
1.2.3.1. Bootloader components¶
- Build ATF
cd ${YOUR_PATH}/ti-bootloader-aosp/arm-trusted-firmware
make E=0 CROSS_COMPILE=aarch64-none-linux-gnu- ARCH=aarch64 PLAT=k3 TARGET_BOARD=lite SPD=opteed CFLAGS+="-DK3_PM_SYSTEM_SUSPEND=1"
- Build OPTEE-OS
cd ${YOUR_PATH}/ti-bootloader-aosp/ti-optee-os
make PLATFORM=k3 CFG_ARM64_core=y CROSS_COMPILE=arm-none-linux-gnueabihf- CROSS_COMPILE64=aarch64-none-linux-gnu-
- Build tiboot3.bin
cd ${YOUR_PATH}/ti-bootloader-aosp/ti-u-boot/
make ARCH=arm am62x_evm_r5_defconfig
make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabihf- \
BINMAN_INDIRS=${YOUR_PATH}/ti-bootloader-aosp/ti-linux-firmware
- Build tispl.bin and u-boot.img
cd ${YOUR_PATH}/ti-bootloader-aosp/ti-u-boot/
make ARCH=arm am62x_evm_a53_defconfig
make ARCH=arm am62x_android_a53.config
make ARCH=arm CROSS_COMPILE=aarch64-none-linux-gnu- \
BL31=${YOUR_PATH}/ti-bootloader-aosp/arm-trusted-firmware/build/k3/lite/release/bl31.bin \
TEE=${YOUR_PATH}/ti-bootloader-aosp/optee_os/out/arm-plat-k3/core/tee-pager_v2.bin \
BINMAN_INDIRS=${YOUR_PATH}/ti-bootloader-aosp/ti-linux-firmware
- Copy the tiboot3.bin, tispl.bin and u-boot.img generated in steps 3 and 4 to
${YOUR_PATH}/ti-aosp-13/vendor/ti/am62x/bootloader. If not copied, the prebuilt bootloader binaries already present in vendor/ti/am62x/bootloader will get use by flashall.sh flashing script.
Note
To Build bootloaders for AM62X LP Board please do same step with this defconfig:
- For step 3 use
am62x_lpsk_r5_defconfig- For step 4 use
am62x_lpsk_a53_defconfigwith same fragment
1.2.3.2. Kernel¶
1.2.3.2.1. Building everything from scratch¶
cd ${YOUR_PATH}/ti-kernel-aosp/
export DIST_DIR=${YOUR_PATH}/ti-aosp-13/device/ti/am62x-kernel/kernel/6.1
tools/bazel run --lto=full //common:ti_dist -- --dist_dir=$DIST_DIR
1.2.3.2.2. Rebuilding faster¶
cd ${YOUR_PATH}/ti-kernel-aosp/
export DIST_DIR=${YOUR_PATH}/ti-aosp-13/device/ti/am62x-kernel/kernel/6.1
tools/bazel run --config=fast //common:ti_dist -- --dist_dir=$DIST_DIR
1.2.3.3. Android File System¶
cd ${YOUR_PATH}/ti-aosp-13
lunch <BUILD_TARGET>
m
Where BUILD_TARGET is listed in the table below :
| Android Build type | Build target |
|---|---|
| AM62X-SK Tablet userdebug | am62x-userdebug |
| AM62X-SK Tablet user | am62x-user |
| AM62X-SK Car userdebug | am62x_car-userdebug |
| AM62X-SK Car user | am62x_car-user |
Note
Default BUILD_TARGET to use is am62x-userdebug
Note
By default with User images AVB feature was enabled.
For userdebug images if you want to enable AVB feature you need to build with TARGET_AVB_ENABLE=true build args
cd ${YOUR_PATH}/ti-aosp-13
lunch <BUILD_TARGET>
m TARGET_AVB_ENABLE=true
After building all components, refer to instruction in next section for flashing the images to EVM