1.2. Building the SDK¶
1.2.1. Build PC Setup¶
Please refer to the following pages from Android documentation to setup your environment for Android build:
Getting the Repo tool
You will need the Repo tool to retrieve repositories. To install it, please refer to this webpage : https://source.android.com/setup/develop#installing-repo
Getting toolchain for u-boot builds
Links to download toolchains for building u-boot are mentioned in the SDK download page.
Install Optee-OS build dependencies
Check OPTEE OS docs to know list of dependencies needed to be installed : https://optee.readthedocs.io/en/latest/building/prerequisites.html
1.2.2. Downloading Sources¶
Create a folder for downloading all sources
mkdir ~/08_06_00 && cd $_
export YOUR_PATH=$PWD
1.2.2.1. Bootloader components¶
mkdir ${YOUR_PATH}/ti-bootloader-aosp/ && cd $_
git clone -b 08.06.00.007 git://git.ti.com/k3-image-gen/k3-image-gen.git
git clone -b 08.06.00.007 git://git.ti.com/atf/arm-trusted-firmware.git
git clone -b 08.06.00.007-android git://git.ti.com/optee/ti-optee-os.git
git clone -b 08.06.00.007-android git://git.ti.com/ti-u-boot/ti-u-boot.git
git clone -b 08.06.00.007 git://git.ti.com/processor-firmware/ti-linux-firmware.git
git clone -b 08.06.00.007 git://git.ti.com/security-development-tools/core-secdev-k3.git
1.2.2.2. Kernel¶
Fetch the code using repo:
mkdir ${YOUR_PATH}/ti-kernel-aosp/ && cd $_
repo init -u git://git.ti.com/android/manifest.git -b android12-core-release -m releases/RLS_08_06_Kernel.xml
repo sync
1.2.2.3. Android File System¶
Fetch the code using repo:
mkdir ${YOUR_PATH}/ti-aosp-12 && cd $_
repo init -u git://git.ti.com/android/manifest.git -b android12-core-release -m releases/RLS_08_06.xml
repo sync
To get the SDK 8.6a patch release use the below manifest
mkdir ${YOUR_PATH}/ti-aosp-12 && cd $_
repo init -u git://git.ti.com/android/manifest.git -b android12-core-release -m releases/RLS_08_06a.xml
repo sync
1.2.3. Build Instructions¶
Note
The Bootloader and Kernel builds below are optional if they are used as is from TI release. Prebuilt copies of these
binaries are already part of Android file system sources in device/ti/am62x-kernel and
vendor/ti/am62x/bootloader folder.
1.2.3.1. Bootloader components¶
- Build tiboot3.bin
export TI_SECURE_DEV_PKG="${YOUR_PATH}/core-secdev-k3"
cd ${YOUR_PATH}/ti-bootloader-aosp/ti-u-boot/
make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabihf- am62x_evm_r5_defconfig O=/tmp/r5
make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabihf- O=/tmp/r5
cd ${YOUR_PATH}/ti-bootloader-aosp/k3-image-gen
make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabihf- SOC=am62x SOC_TYPE=gp CONFIG=evm SBL=/tmp/r5/spl/u-boot-spl.bin SYSFW_PATH=${YOUR_PATH}/ti-bootloader-aosp/ti-linux-firmware/ti-sysfw/ti-fs-firmware-am62x-gp.bin
Use the tiboot3.bin generated from last command in ${YOUR_PATH}/ti-bootloader-aosp/k3-image-gen
Note
To build tiboot3 for HS-FS board change SOC_TYPE=gp by SOC_TYPE=hs-fs in make command
- Build tispl.bin and u-boot.img
In order to build tispl.bin and u-boot.img, OPTEE and ATF (arm trusted firmware) need to be built.
cd ${YOUR_PATH}/ti-bootloader-aosp/arm-trusted-firmware
make CROSS_COMPILE=aarch64-none-linux-gnu- ARCH=aarch64 PLAT=k3 TARGET_BOARD=lite SPD=opteed CFLAGS+="-DK3_PM_SYSTEM_SUSPEND=1"
cd ${YOUR_PATH}/ti-bootloader-aosp/ti-optee-os
make PLATFORM=k3 CFG_ARM64_core=y CROSS_COMPILE=arm-none-linux-gnueabihf- CROSS_COMPILE64=aarch64-none-linux-gnu-
It is now possible to generate tispl.bin and u-boot.img.
cd ${YOUR_PATH}/ti-bootloader-aosp/ti-u-boot/
make ARCH=arm CROSS_COMPILE=aarch64-none-linux-gnu- am62x_evm_a53_defconfig O=/tmp/a53
make ARCH=arm CROSS_COMPILE=aarch64-none-linux-gnu- ATF=${YOUR_PATH}/ti-bootloader-aosp/arm-trusted-firmware/build/k3/lite/release/bl31.bin TEE=${YOUR_PATH}/ti-bootloader-aosp/ti-optee-os/out/arm-plat-k3/core/tee-pager_v2.bin DM=${YOUR_PATH}/ti-bootloader-aosp/ti-linux-firmware/ti-dm/am62xx/ipc_echo_testb_mcu1_0_release_strip.xer5f O=/tmp/a53
Use tispl.bin and u-boot.img located in /tmp/a53
- Copy the tiboot3.bin, tispl.bin and u-boot.img generated in steps 1 and 2 to
${YOUR_PATH}/ti-aosp-12/vendor/ti/am62x/bootloader. If not copied, the prebuilt bootloader binaries already present in vendor/ti/am62x/bootloader will get use by flashall.sh flashing script.
1.2.3.2. Kernel¶
1.2.3.2.1. Building everything from scratch¶
cd ${YOUR_PATH}/ti-kernel-aosp/
export DIST_DIR=${YOUR_PATH}/ti-aosp/device/ti/am62x-kernel/kernel/5.10
export BUILD_CONFIG=./common/build.config.ti
build/build.sh
1.2.3.2.2. Rebuilding incrementally¶
Add the SKIP_MRPROPER=1 flag:
$ cd ${YOUR_PATH}/ti-kernel-aosp/
$ export DIST_DIR=${YOUR_PATH}/ti-aosp/device/ti/am62x-prebuilts/kernel/5.10
$ export BUILD_CONFIG=./common/build.config.ti
$ export SKIP_MRPROPER=1
$ build/build.sh
1.2.3.2.4. Building the kernel without Android project code¶
Download and extract the prebuilt binaries following : Using Prebuilt binaries and start building the kernel by running the following commands.
cd ${YOUR_PATH}/ti-kernel-aosp/ export BUILD_CONFIG=./common/build.config.ti export PREBUILT_BOOTIMG=<PATH/TO/ANDROID/PREBUILT/BINARIES/boot.img> build/build.sh
The new boot image will be located in ${YOUR_PATH}/ti-kernel-aosp/out/android13-5.10/
Please refer to : Flashing the kernel to flash the new kernel.
1.2.3.3. Android File System¶
cd ${YOUR_PATH}/ti-aosp-12
lunch <BUILD_TARGET>
m
Where BUILD_TARGET is listed in the table below :
| Android Build type | Build target |
|---|---|
| AM62X-SK Tablet userdebug | am62x-userdebug |
| AM62X-SK Tablet user | am62x-user |
| AM62X-SK Car userdebug | am62x_car-userdebug |
| AM62X-SK Car user | am62x_car-user |
| AM62X-LP-SK Tablet userdebug | am62x_lp-userdebug |
| AM62X-LP-SK Tablet user | am62x_lp-user |
| AM62X-LP-SK Car userdebug | am62x_lp_car-userdebug |
| AM62X-LP-SK Car user | am62x_lp_car-user |
Note
Default BUILD_TARGET to use is am62x-userdebug
Note
By default with User images AVB feature was enabled.
For userdebug images if you want to enable AVB feature you need to build with TARGET_AVB_ENABLE=true build args
cd ${YOUR_PATH}/ti-aosp-12
lunch <BUILD_TARGET>
m TARGET_AVB_ENABLE=true
Note
Follow this link if you want to build and test in Android Generic Kernel Image mode.
After building all components, refer to instruction in next section for flashing the images to EVM