3.1. Android Kernel
3.1.1. Downloading sources
Fetch the code using repo:
$ mkdir ${YOUR_PATH}/ti-kernel-aosp/ && cd $_
$ repo init -u https://git.ti.com/git/android/manifest.git -b android15-release -m releases/RLS_10_01_Kernel-6.6.xml
$ repo sync
Tip
To save some disk space, pass the --depth=1 option to repo init:
$ repo init -u https://git.ti.com/git/android/manifest.git -b android15-release -m releases/RLS_10_01_Kernel-6.6.xml --depth=1
3.1.2. Build Instructions
3.1.2.1. Building everything from scratch
$ cd ${YOUR_PATH}/ti-kernel-aosp/
$ export TARGET_KERNEL_USE="6.6"
$ export DIST_DIR=${YOUR_PATH}/ti-aosp-15/device/ti/am62x-kernel/kernel/${TARGET_KERNEL_USE}
$ tools/bazel run //common:ti_dist -- --dist_dir=$DIST_DIR
Android uses Kleaf, a Bazel-based build system to build the kernel. AOSP documentation can be found here and Kleaf documentation here
Attention
Kernel builds hangs when using the btrfs file system.
This is a known issue according to the kleaf documentation
Make sure to pass the --workaround_btrfs_b292212788 flag to bazel when using btrfs.
3.1.2.2. Rebuilding faster
$ cd ${YOUR_PATH}/ti-kernel-aosp/
$ export TARGET_KERNEL_USE="6.6"
$ export DIST_DIR=${YOUR_PATH}/ti-aosp-15/device/ti/am62x-kernel/kernel/${TARGET_KERNEL_USE}
$ tools/bazel run --config=fast //common:ti_dist -- --dist_dir=$DIST_DIR
3.1.2.4. Rebuild Android images
We should re-generate the Android images to include the newly build kernel. Follow the Android Build Instructions to do so.
3.1.3. Flashing instructions
In order to flash a new kernel, several images should be flashed:
$ adb reboot fastboot
< Wait for fastbootd reboot >
$ cd <PATH/TO/IMAGES>
$ fastboot flash boot boot.img
$ fastboot flash vendor_boot vendor_boot.img
$ fastboot flash vendor_dlkm vendor_dlkm.img
$ fastboot reboot
The board should boot with the new kernel.
3.1.4. Enabling new drivers
Since the kernel is based on the Generic Kernel Image, new drivers should always be added as modules.
To enable new modules:
Run
menuconfigas documented previously, Select=mfor the driver.Edit
$YOUR_PATH/ti-kernel-aosp/BUILD.bazelto add your new module. Look for the following section:_TI_MODULE_OUTS = [ # keep sorted "crypto/af_alg.ko", "crypto/algif_hash.ko",In the
_TI_MODULE_OUTSarray, add the path to your new kernel module.Rebuild the kernel as documented in Build Instructions.
If the driver module needs to be loaded early (in the ramdisk), edit
$YOUR_PATH/ti-aosp-15/device/ti/am62x/BoardConfig-common.mkand add the path to your module:BOARD_VENDOR_RAMDISK_KERNEL_MODULES += \ device/ti/am62x-kernel/kernel/$(TARGET_KERNEL_USE)/your_module.koFinally, rebuild the Android images.
3.1.5. Device tree overlays
3.1.5.1. Mapping adtbo_idx with filenames
Device tree overlays can be used to configure additional hardware peripherals.
These overlays are stored in the dtbo.img. This image is generated when
building the Android kernel as documented in Build Instructions.
As listed in Device Tree Overlay Support, we can configure an overlay to be applied
from U-Boot by setting the adtbo_idx variable.
To view how the adtbo_idx maps with the dtbo file, we can inspect the BUILD.bazel
from the kernel source code.
Looking at the kernel_images() macro, we can see:
kernel_images(
name = "ti_images",
build_dtbo = True,
build_initramfs = True,
dtbo_srcs = [
":ti/k3-am62x-sk-hdmi-audio.dtbo",
":ti/k3-am62x-sk-csi2-ov5640.dtbo",
":ti/k3-am62x-sk-csi2-tevi-ov5640.dtbo",
":ti/k3-am625-sk-microtips-mf101hie-panel.dtbo",
":ti/k3-am62x-sk-lpm-wkup-sources.dtbo",
":ti/k3-am62-lp-sk-microtips-mf101hie-panel.dtbo",
":ti/k3-am625-beagleplay-csi2-ov5640.dtbo",
":ti/k3-am625-beagleplay-csi2-tevi-ov5640.dtbo",
":ti/k3-am625-beagleplay-lincolntech-lcd185-panel.dtbo",
":ti/k3-am62p5-sk-mcan.dtbo",
":ti/k3-am62p5-sk-microtips-mf101hie-panel.dtbo",
":ti/k3-am625-sk-m2-cc3301.dtbo",
":ti/k3-am62p5-sk-m2-cc3301.dtbo",
":ti/k3-am625-sk-wl1837.dtbo",
The dtbo_srcs array order dicates the index. For example:
filename |
index |
|---|---|
|
0 |
|
1 |
3.1.5.2. Adding more .dtbo files to the dtbo.img
In this section, we will see how to add more .dtbo files to the dtbo.img.
Let’s see how to add ti/k3-am62p5-sk-dsi-rpi-7inch-panel.dtbo for example:
Edit
$YOUR_PATH/ti-kernel-aosp/BUILD.bazel. Look for the following section:kernel_build( name = "ti", outs = [ "Image", "System.map", "k3-am62-lp-sk.dtb", "k3-am62-lp-sk-microtips-mf101hie-panel.dtbo",In the
kernel_build()section, addk3-am62p5-sk-dsi-rpi-7inch-panel.dtboto theoutsarray.Still in
kernel_build(), look for themake_goalsarray and addti/k3-am62p5-sk-dsi-rpi-7inch-panel.dtbo.Now look for the following section:
kernel_images( name = "ti_images", build_dtbo = True, build_initramfs = True, dtbo_srcs = [ ":ti/k3-am62x-sk-hdmi-audio.dtbo", ":ti/k3-am62x-sk-csi2-ov5640.dtbo", ":ti/k3-am62x-sk-csi2-tevi-ov5640.dtbo",In the
kernel_images(), add:ti/k3-am62p5-sk-dsi-rpi-7inch-panel.dtboat the end of the array.Important
Make sure to add the it at the end of the array. The order in
dtbo_srcswill determine theadtbo_idxto be used.Rebuild the kernel as documented in Build Instructions.