1.2. Building the SDK¶
1.2.1. Build PC setup¶
Please refer to the following pages from Android documentation to setup your environment for Android build:
Getting the repo tool
You will need the repo tool to retrieve repositories.
To install it, please refer to this webpage : https://source.android.com/setup/develop#installing-repo
Getting toolchain for u-boot builds
Links to download toolchains for building u-boot are mentioned in the SDK download page.
Install OPTEE-OS build dependencies
Check OPTEE-OS docs to know list of dependencies needed to be installed : https://optee.readthedocs.io/en/latest/building/prerequisites.html
1.2.2. Downloading sources¶
Create a folder for downloading all sources
mkdir ~/09_01_00 && cd $_
export YOUR_PATH=$PWD
1.2.2.1. Bootloader components¶
mkdir ${YOUR_PATH}/ti-bootloader-aosp/ && cd $_
git clone -b 09.01.00.008 git://git.ti.com/atf/arm-trusted-firmware.git
git clone -b 3.22.0-rc1 https://github.com/OP-TEE/optee_os.git
git clone -b 09.01.00.008 git://git.ti.com/ti-u-boot/ti-u-boot.git
git clone -b 09.01.00.008 git://git.ti.com/processor-firmware/ti-linux-firmware.git
1.2.2.2. Kernel¶
Fetch the code using repo:
mkdir ${YOUR_PATH}/ti-kernel-aosp/ && cd $_
repo init -u git://git.ti.com/android/manifest.git -b android14-release -m releases/RLS_09_01_Kernel.xml
repo sync
Note
To save some disk space, pass the --depth=1 option to repo init:
repo init -u git://git.ti.com/android/manifest.git -b android14-release -m releases/RLS_09_01_Kernel.xml --depth=1
1.2.2.3. Android file system¶
Fetch the code using repo:
mkdir ${YOUR_PATH}/ti-aosp-14 && cd $_
repo init -u git://git.ti.com/android/manifest.git -b android14-release -m releases/RLS_09_01.xml
repo sync
1.2.3. Build Instructions¶
Note
The bootloader and kernel builds below are optional if they are used as-is from TI release.
Prebuilt copies of these binaries are already part of Android file system sources
in device/ti/am62x-kernel and vendor/ti/am62x/bootloader folder.
1.2.3.1. Bootloader components¶
Build ATF:
cd ${YOUR_PATH}/ti-bootloader-aosp/arm-trusted-firmware make E=0 CROSS_COMPILE=aarch64-none-linux-gnu- ARCH=aarch64 PLAT=k3 TARGET_BOARD=lite SPD=opteed CFLAGS+="-DK3_PM_SYSTEM_SUSPEND=1"Build OPTEE-OS:
cd ${YOUR_PATH}/ti-bootloader-aosp/optee_os make PLATFORM=k3 CFG_ARM64_core=y CROSS_COMPILE=arm-none-linux-gnueabihf- CROSS_COMPILE64=aarch64-none-linux-gnu-Build
tiboot3.bin:
cd ${YOUR_PATH}/ti-bootloader-aosp/ti-u-boot/ make ARCH=arm am62px_evm_r5_defconfig make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabihf- \ BINMAN_INDIRS=${YOUR_PATH}/ti-bootloader-aosp/ti-linux-firmware
- Build
tispl.binandu-boot.img:
cd ${YOUR_PATH}/ti-bootloader-aosp/ti-u-boot/ make ARCH=arm am62px_evm_a53_defconfig make ARCH=arm am62x_android_a53.config make ARCH=arm CROSS_COMPILE=aarch64-none-linux-gnu- \ BL31=${YOUR_PATH}/ti-bootloader-aosp/arm-trusted-firmware/build/k3/lite/release/bl31.bin \ TEE=${YOUR_PATH}/ti-bootloader-aosp/optee_os/out/arm-plat-k3/core/tee-pager_v2.bin \ BINMAN_INDIRS=${YOUR_PATH}/ti-bootloader-aosp/ti-linux-firmware
- Copy the
tiboot3.bin,tispl.binandu-boot.imggenerated in steps 3 and 4 to${YOUR_PATH}/ti-aosp-14/vendor/ti/am62x/bootloader. If not copied, the prebuilt bootloader binaries already present invendor/ti/am62x/bootloaderwill get used byflashall.shflashing script.
1.2.3.2. Kernel¶
1.2.3.2.1. Building everything from scratch¶
cd ${YOUR_PATH}/ti-kernel-aosp/
export DIST_DIR=${YOUR_PATH}/ti-aosp-14/device/ti/am62x-kernel/kernel/6.1
tools/bazel run //common:ti_dist -- --dist_dir=$DIST_DIR
1.2.3.2.2. Rebuilding faster¶
cd ${YOUR_PATH}/ti-kernel-aosp/
export DIST_DIR=${YOUR_PATH}/ti-aosp-14/device/ti/am62x-kernel/kernel/6.1
tools/bazel run --config=fast //common:ti_dist -- --dist_dir=$DIST_DIR
1.2.3.3. Android File System¶
cd ${YOUR_PATH}/ti-aosp-14
source build/envsetup.sh
lunch <BUILD_TARGET>
m
Where BUILD_TARGET is listed in the table below :
| Android Build type | Build target |
|---|---|
| AM62PX-SK Tablet userdebug | am62p-userdebug |
| AM62PX-SK Tablet user | am62p-user |
| AM62PX-SK Car userdebug | am62p_car-userdebug |
| AM62PX-SK Car user | am62p_car-user |
The recommended BUILD_TARGET to use is am62p-userdebug.
Note
By default with user images AVB feature is enabled.
For userdebug images, if you want to enable AVB feature you need to build
with TARGET_AVB_ENABLE=true build args:
cd ${YOUR_PATH}/ti-aosp-14
source build/envsetup.sh
lunch <BUILD_TARGET>
m TARGET_AVB_ENABLE=true
After building all components, refer to instruction in next section for flashing the images to EVM