This section covers the provided encoder/observer algorithms used in both sensored/sensorless field oriented control (FOC). The library source code can be found in motor_control_sdk/source/observer.
Sensored:
Sensorless:
Speed measurement:
The encoder (ENC) algorithm leverages the Enhanced Quadrature Encoder Pulse (eQEP) feature on the device for a sensored-based FOC. It calculates rotor angle based on eQEP encoder.
Enhanced Sliding Mode Observer (eSMO) estimates rotor angle to achieve a sensorless FOC.
The Hall algorithm uses an external Hall effect sensor to calculate speed and rotor angle for a sensored FOC design.
Speed measurement is a supplement algorithm that measures speed based on the rotor angle. It consists of two different implementations, speedfr (SPDFR) calculates speed from an eQEP encoder signal whereas speedcalc (SPDCALC) estimates frequency of the eSMO observer.
A benchmark on R5F core has been conducted to observe the following results when calling each functions:
| Functions | Cpu Cycles |
|---|---|
| Encoder | |
| ENC_run (w/o calibration) | 16 |
| ENC_run (w/ calibration) | 30 |
| ENC_runHall | 16 |
| Enhanced Sliding Mode Observer | |
| EMSO_run | 307 |
| Hall | |
| HALL_run | 73 |
| Sensorless speed measurement | |
| SPDCALC_run | 53 |
| Sensored speed measurement | |
| SPDFR_run | 32 |
N/A