AM263x MCU+ SDK  10.00.00

Introduction

For more details and example usage, see SOC

Functions

static void SOC_xbarSelectInputXBarInputSource (uint32_t base, uint8_t out, uint8_t group_select, uint8_t group0_muxctl, uint8_t group1_muxctl)
 Trip & Sync xbar: API to select input source of Input XBar. More...
 
static uint32_t SOC_xbarGetPWMXBarOutputSignalStatus (uint32_t base)
 Trip & Sync xbar: API to read raw output signal status of all PWM XBars. More...
 
static void SOC_xbarInvertPWMXBarOutputSignalBeforeLatch (uint32_t base, uint32_t invert_mask)
 Trip & Sync xbar: API to configure inversion of output signal status flag (latched) of PWM XBars. More...
 
static uint32_t SOC_xbarGetPWMXBarOutputSignalLatchedFlag (uint32_t base)
 Trip & Sync xbar: API to read latched output signal status of all PWM XBars. More...
 
static void SOC_xbarClearPWMXBarOutputSignalLatchedFlag (uint32_t base, uint32_t clr)
 Trip & Sync xbar: API to clear output signal status flag (latched) of PWM XBars. More...
 
static void SOC_xbarSelectPWMXBarInputSource (uint32_t base, uint8_t out, uint32_t group0_mask, uint32_t group1_mask, uint32_t group2_mask, uint32_t group3_mask, uint32_t group4_mask, uint32_t group5_mask, uint32_t group6_mask, uint32_t group7_mask, uint32_t group8_mask)
 Trip & Sync xbar: API to select input sources of PWM XBar. More...
 
static void SOC_xbarSelectMinimumDeadBandLogicXBarInputSource (uint32_t base, uint8_t out, uint32_t group0_mask, uint32_t group1_mask, uint32_t group2_mask)
 Trip & Sync xbar: API to select input sources of MDL XBar. More...
 
static void SOC_xbarSelectIllegalComboLogicXBarInputSource (uint32_t base, uint8_t out, uint32_t group0_mask, uint32_t group1_mask, uint32_t group2_mask)
 Trip & Sync xbar: API to select input sources of ICL XBar. More...
 
static void SOC_xbarSelectInterruptXBarInputSource (uint32_t base, uint8_t out, uint32_t group0_mask, uint32_t group1_mask, uint32_t group2_mask, uint32_t group3_mask, uint32_t group4_mask, uint32_t group5_mask, uint32_t group6_mask)
 Trip & Sync xbar: API to select input sources of Interrupt XBar. More...
 
static void SOC_xbarSelectDMAXBarInputSource (uint32_t base, uint8_t out, uint8_t group_select, uint8_t group0_muxctl, uint8_t group1_muxctl, uint8_t group2_muxctl, uint8_t group3_muxctl, uint8_t group4_muxctl, uint8_t group5_muxctl)
 Trip & Sync xbar: API to select input source of DMA XBar. More...
 
static uint32_t SOC_xbarGetOutputXBarOutputSignalStatus (uint32_t base)
 Trip & Sync xbar: API to read raw output signal status of all Output XBars. More...
 
static void SOC_xbarInvertOutputXBarOutputSignalBeforeLatch (uint32_t base, uint32_t invert)
 Trip & Sync xbar: API to configure inversion of output signal status flag (latched) of Output XBars. More...
 
static uint32_t SOC_xbarGetOutputXBarOutputSignalLatchedFlag (uint32_t base)
 Trip & Sync xbar: API to read latched output signal status of all Output XBars. More...
 
static void SOC_xbarClearOutputXBarOutputSignalLatchedFlag (uint32_t base, uint32_t clr)
 Trip & Sync xbar: API to clear output signal status flag (latched) of Output XBars. More...
 
static void SOC_xbarForceOutputXBarOutputSignalLatchedFlag (uint32_t base, uint32_t force)
 Trip & Sync xbar: API to force output signal status flag (latched) of Output XBars. More...
 
static void SOC_xbarSelectLatchOutputXBarOutputSignal (uint32_t base, uint32_t latchselect)
 Trip & Sync xbar: API to select output of Output XBars. More...
 
static void SOC_xbarSelectStretchedPulseOutputXBarOutputSignal (uint32_t base, uint32_t stretchselect)
 Trip & Sync xbar: API to enable pulse stretching of output of Output XBars. More...
 
static void SOC_xbarSelectStretchedPulseLengthOutputXBarOutputSignal (uint32_t base, uint32_t lengthselect)
 Trip & Sync xbar: API to configure pulse streching length of output of Output XBars. More...
 
static void SOC_xbarInvertOutputXBarOutputSignal (uint32_t base, uint32_t invertout)
 Trip & Sync xbar: API to configure inversion of output signal of Output XBars. More...
 
static void SOC_xbarSelectOutputXBarInputSource (uint32_t base, uint8_t out, uint32_t group0_mask, uint32_t group1_mask, uint32_t group2_mask, uint32_t group3_mask, uint32_t group4_mask, uint32_t group5_mask, uint32_t group6_mask, uint32_t group7_mask, uint32_t group8_mask, uint32_t group9_mask, uint32_t group10_mask)
 Trip & Sync xbar: API to select input sources of Output XBar. More...
 
static void SOC_xbarSelectPWMSyncOutXBarInput (uint32_t base, uint8_t out, uint32_t input)
 Trip & Sync xbar: API to select input sources of PWM Syncout XBar. More...
 
static void SOC_xbarSelectEdmaTrigXbarInputSource (uint32_t base, uint8_t out, uint8_t mux_control)
 SoC level xbars: API to select input source of EDMA Trigger XBar. More...
 
static void SOC_xbarSelectGpioIntrXbarInputSource (uint32_t base, uint8_t out, uint8_t mux_control)
 SoC level xbars: API to select input source of GPIO Interrupt XBar. More...
 
static void SOC_xbarSelectIcssmIntrXbarInputSource (uint32_t base, uint8_t out, uint8_t mux_control)
 SoC level xbars: API to select input source of ICSSM Interrupt XBar. More...
 
static void SOC_xbarSelectTimesyncXbar0InputSource (uint32_t base, uint8_t out, uint8_t mux_control)
 SoC level xbars: API to select input source of TimeSync XBar0. More...
 
static void SOC_xbarSelectTimesyncXbar1InputSource (uint32_t base, uint8_t out, uint8_t mux_control)
 SoC level xbars: API to select input source of TimeSync XBar1. More...
 

Macros

#define CSL_CONTROLSS_INPUTXBAR_STEP   (CSL_CONTROLSS_INPUTXBAR_INPUTXBAR1_GSEL - CSL_CONTROLSS_INPUTXBAR_INPUTXBAR0_GSEL)
 
#define CSL_CONTROLSS_PWMXBAR_STEP   (CSL_CONTROLSS_PWMXBAR_PWMXBAR1_G0 - CSL_CONTROLSS_PWMXBAR_PWMXBAR0_G0)
 
#define CSL_CONTROLSS_MDLXBAR_STEP   (CSL_CONTROLSS_MDLXBAR_MDLXBAR1_G0 - CSL_CONTROLSS_MDLXBAR_MDLXBAR0_G0)
 
#define CSL_CONTROLSS_ICLXBAR_STEP   (CSL_CONTROLSS_ICLXBAR_ICLXBAR1_G0 - CSL_CONTROLSS_ICLXBAR_ICLXBAR0_G0)
 
#define CSL_CONTROLSS_INTXBAR_STEP   (CSL_CONTROLSS_INTXBAR_INTXBAR1_G0 - CSL_CONTROLSS_INTXBAR_INTXBAR0_G0)
 
#define CSL_CONTROLSS_DMAXBAR_STEP   (CSL_CONTROLSS_DMAXBAR_DMAXBAR1_GSEL - CSL_CONTROLSS_DMAXBAR_DMAXBAR0_GSEL)
 
#define CSL_CONTROLSS_OUTPUTXBAR_STEP   (CSL_CONTROLSS_OUTPUTXBAR_OUTPUTXBAR1_G0 - CSL_CONTROLSS_OUTPUTXBAR_OUTPUTXBAR0_G0)
 
#define CSL_CONTROLSS_PWMSYNCOUTXBAR_STEP   (CSL_CONTROLSS_PWMSYNCOUTXBAR_PWMSYNCOUTXBAR1_G0 - CSL_CONTROLSS_PWMSYNCOUTXBAR_PWMSYNCOUTXBAR0_G0)
 

Macro Definition Documentation

◆ CSL_CONTROLSS_INPUTXBAR_STEP

#define CSL_CONTROLSS_INPUTXBAR_STEP   (CSL_CONTROLSS_INPUTXBAR_INPUTXBAR1_GSEL - CSL_CONTROLSS_INPUTXBAR_INPUTXBAR0_GSEL)

◆ CSL_CONTROLSS_PWMXBAR_STEP

#define CSL_CONTROLSS_PWMXBAR_STEP   (CSL_CONTROLSS_PWMXBAR_PWMXBAR1_G0 - CSL_CONTROLSS_PWMXBAR_PWMXBAR0_G0)

◆ CSL_CONTROLSS_MDLXBAR_STEP

#define CSL_CONTROLSS_MDLXBAR_STEP   (CSL_CONTROLSS_MDLXBAR_MDLXBAR1_G0 - CSL_CONTROLSS_MDLXBAR_MDLXBAR0_G0)

◆ CSL_CONTROLSS_ICLXBAR_STEP

#define CSL_CONTROLSS_ICLXBAR_STEP   (CSL_CONTROLSS_ICLXBAR_ICLXBAR1_G0 - CSL_CONTROLSS_ICLXBAR_ICLXBAR0_G0)

◆ CSL_CONTROLSS_INTXBAR_STEP

#define CSL_CONTROLSS_INTXBAR_STEP   (CSL_CONTROLSS_INTXBAR_INTXBAR1_G0 - CSL_CONTROLSS_INTXBAR_INTXBAR0_G0)

◆ CSL_CONTROLSS_DMAXBAR_STEP

#define CSL_CONTROLSS_DMAXBAR_STEP   (CSL_CONTROLSS_DMAXBAR_DMAXBAR1_GSEL - CSL_CONTROLSS_DMAXBAR_DMAXBAR0_GSEL)

◆ CSL_CONTROLSS_OUTPUTXBAR_STEP

#define CSL_CONTROLSS_OUTPUTXBAR_STEP   (CSL_CONTROLSS_OUTPUTXBAR_OUTPUTXBAR1_G0 - CSL_CONTROLSS_OUTPUTXBAR_OUTPUTXBAR0_G0)

◆ CSL_CONTROLSS_PWMSYNCOUTXBAR_STEP

#define CSL_CONTROLSS_PWMSYNCOUTXBAR_STEP   (CSL_CONTROLSS_PWMSYNCOUTXBAR_PWMSYNCOUTXBAR1_G0 - CSL_CONTROLSS_PWMSYNCOUTXBAR_PWMSYNCOUTXBAR0_G0)

Function Documentation

◆ SOC_xbarSelectInputXBarInputSource()

static void SOC_xbarSelectInputXBarInputSource ( uint32_t  base,
uint8_t  out,
uint8_t  group_select,
uint8_t  group0_muxctl,
uint8_t  group1_muxctl 
)
inlinestatic

Trip & Sync xbar: API to select input source of Input XBar.

Parameters
base[in] Input XBar base address
out[in] Instance of Input XBar
group0_muxctl[in] Mux control to select input from group 0 mux
group1_muxctl[in] Mux control to select input from group 1 mux
group_select[in] Mux control to select group 0 or 1

◆ SOC_xbarGetPWMXBarOutputSignalStatus()

static uint32_t SOC_xbarGetPWMXBarOutputSignalStatus ( uint32_t  base)
inlinestatic

Trip & Sync xbar: API to read raw output signal status of all PWM XBars.

Parameters
base[in] PWM XBar base address
Returns
uint32_t PWM XBar status

◆ SOC_xbarInvertPWMXBarOutputSignalBeforeLatch()

static void SOC_xbarInvertPWMXBarOutputSignalBeforeLatch ( uint32_t  base,
uint32_t  invert_mask 
)
inlinestatic

Trip & Sync xbar: API to configure inversion of output signal status flag (latched) of PWM XBars.

Parameters
base[in] PWM XBar base address
invert_mask[in] Mask defining the PWM XBar output signal flags (latched) to be inverted

◆ SOC_xbarGetPWMXBarOutputSignalLatchedFlag()

static uint32_t SOC_xbarGetPWMXBarOutputSignalLatchedFlag ( uint32_t  base)
inlinestatic

Trip & Sync xbar: API to read latched output signal status of all PWM XBars.

Parameters
base[in] PWM XBar base address
Returns
uint32_t PWM XBar latched status flags

◆ SOC_xbarClearPWMXBarOutputSignalLatchedFlag()

static void SOC_xbarClearPWMXBarOutputSignalLatchedFlag ( uint32_t  base,
uint32_t  clr 
)
inlinestatic

Trip & Sync xbar: API to clear output signal status flag (latched) of PWM XBars.

Parameters
base[in] PWM XBar base address
clr[in] Mask defining the PWM XBar output signal flags (latched) to be cleared

◆ SOC_xbarSelectPWMXBarInputSource()

static void SOC_xbarSelectPWMXBarInputSource ( uint32_t  base,
uint8_t  out,
uint32_t  group0_mask,
uint32_t  group1_mask,
uint32_t  group2_mask,
uint32_t  group3_mask,
uint32_t  group4_mask,
uint32_t  group5_mask,
uint32_t  group6_mask,
uint32_t  group7_mask,
uint32_t  group8_mask 
)
inlinestatic

Trip & Sync xbar: API to select input sources of PWM XBar.

Parameters
base[in] PWM XBar base address
out[in] Instance of PWM XBar
group0_mask[in] Mask to OR inputs from group 0
group1_mask[in] Mask to OR inputs from group 1
group2_mask[in] Mask to OR inputs from group 2
group3_mask[in] Mask to OR inputs from group 3
group4_mask[in] Mask to OR inputs from group 4
group5_mask[in] Mask to OR inputs from group 5
group6_mask[in] Mask to OR inputs from group 6
group7_mask[in] Mask to OR inputs from group 7
group8_mask[in] Mask to OR inputs from group 8

◆ SOC_xbarSelectMinimumDeadBandLogicXBarInputSource()

static void SOC_xbarSelectMinimumDeadBandLogicXBarInputSource ( uint32_t  base,
uint8_t  out,
uint32_t  group0_mask,
uint32_t  group1_mask,
uint32_t  group2_mask 
)
inlinestatic

Trip & Sync xbar: API to select input sources of MDL XBar.

Parameters
base[in] MDL XBar base address
out[in] Instance of MDL XBar
group0_mask[in] Mask to OR inputs from group 0
group1_mask[in] Mask to OR inputs from group 1
group2_mask[in] Mask to OR inputs from group 2

◆ SOC_xbarSelectIllegalComboLogicXBarInputSource()

static void SOC_xbarSelectIllegalComboLogicXBarInputSource ( uint32_t  base,
uint8_t  out,
uint32_t  group0_mask,
uint32_t  group1_mask,
uint32_t  group2_mask 
)
inlinestatic

Trip & Sync xbar: API to select input sources of ICL XBar.

Parameters
base[in] ICL XBar base address
out[in] Instance of ICL XBar
group0_mask[in] Mask to OR inputs from group 0
group1_mask[in] Mask to OR inputs from group 1
group2_mask[in] Mask to OR inputs from group 2

◆ SOC_xbarSelectInterruptXBarInputSource()

static void SOC_xbarSelectInterruptXBarInputSource ( uint32_t  base,
uint8_t  out,
uint32_t  group0_mask,
uint32_t  group1_mask,
uint32_t  group2_mask,
uint32_t  group3_mask,
uint32_t  group4_mask,
uint32_t  group5_mask,
uint32_t  group6_mask 
)
inlinestatic

Trip & Sync xbar: API to select input sources of Interrupt XBar.

Parameters
base[in] Interrupt XBar base address
out[in] Instance of Interrupt XBar
group0_mask[in] Mask to OR inputs from group 0
group1_mask[in] Mask to OR inputs from group 1
group2_mask[in] Mask to OR inputs from group 2
group3_mask[in] Mask to OR inputs from group 3
group4_mask[in] Mask to OR inputs from group 4
group5_mask[in] Mask to OR inputs from group 5
group6_mask[in] Mask to OR inputs from group 6

◆ SOC_xbarSelectDMAXBarInputSource()

static void SOC_xbarSelectDMAXBarInputSource ( uint32_t  base,
uint8_t  out,
uint8_t  group_select,
uint8_t  group0_muxctl,
uint8_t  group1_muxctl,
uint8_t  group2_muxctl,
uint8_t  group3_muxctl,
uint8_t  group4_muxctl,
uint8_t  group5_muxctl 
)
inlinestatic

Trip & Sync xbar: API to select input source of DMA XBar.

Parameters
base[in] DMA XBar base address
out[in] Instance of DMA XBar
group0_muxctl[in] Mux control to select input from group 0 mux
group1_muxctl[in] Mux control to select input from group 1 mux
group2_muxctl[in] Mux control to select input from group 2 mux
group3_muxctl[in] Mux control to select input from group 3 mux
group4_muxctl[in] Mux control to select input from group 4 mux
group5_muxctl[in] Mux control to select input from group 5 mux
group_select[in] Mux control to select group 0/1/2/3/4/5

◆ SOC_xbarGetOutputXBarOutputSignalStatus()

static uint32_t SOC_xbarGetOutputXBarOutputSignalStatus ( uint32_t  base)
inlinestatic

Trip & Sync xbar: API to read raw output signal status of all Output XBars.

Parameters
base[in] Output XBar base address
Returns
uint32_t Output XBar status

◆ SOC_xbarInvertOutputXBarOutputSignalBeforeLatch()

static void SOC_xbarInvertOutputXBarOutputSignalBeforeLatch ( uint32_t  base,
uint32_t  invert 
)
inlinestatic

Trip & Sync xbar: API to configure inversion of output signal status flag (latched) of Output XBars.

Parameters
base[in] Output XBar base address
invert[in] Mask defining the Output XBar output signal flags (latched) to be inverted

◆ SOC_xbarGetOutputXBarOutputSignalLatchedFlag()

static uint32_t SOC_xbarGetOutputXBarOutputSignalLatchedFlag ( uint32_t  base)
inlinestatic

Trip & Sync xbar: API to read latched output signal status of all Output XBars.

Parameters
base[in] Output XBar base address
Returns
uint32_t Output XBar latched status flags

◆ SOC_xbarClearOutputXBarOutputSignalLatchedFlag()

static void SOC_xbarClearOutputXBarOutputSignalLatchedFlag ( uint32_t  base,
uint32_t  clr 
)
inlinestatic

Trip & Sync xbar: API to clear output signal status flag (latched) of Output XBars.

Parameters
base[in] Output XBar base address
clr[in] Mask defining the Output XBar output signal flags (latched) to be cleared

◆ SOC_xbarForceOutputXBarOutputSignalLatchedFlag()

static void SOC_xbarForceOutputXBarOutputSignalLatchedFlag ( uint32_t  base,
uint32_t  force 
)
inlinestatic

Trip & Sync xbar: API to force output signal status flag (latched) of Output XBars.

Parameters
base[in] Output XBar base address
force[in] Mask defining the Output XBar output signal flags (latched) to be forced to set

◆ SOC_xbarSelectLatchOutputXBarOutputSignal()

static void SOC_xbarSelectLatchOutputXBarOutputSignal ( uint32_t  base,
uint32_t  latchselect 
)
inlinestatic

Trip & Sync xbar: API to select output of Output XBars.

Parameters
base[in] Output XBar base address
latchselect[in] Select latched / non-latched output

◆ SOC_xbarSelectStretchedPulseOutputXBarOutputSignal()

static void SOC_xbarSelectStretchedPulseOutputXBarOutputSignal ( uint32_t  base,
uint32_t  stretchselect 
)
inlinestatic

Trip & Sync xbar: API to enable pulse stretching of output of Output XBars.

Parameters
base[in] Output XBar base address
stretchselect[in] Select stretched / non-stretched output

◆ SOC_xbarSelectStretchedPulseLengthOutputXBarOutputSignal()

static void SOC_xbarSelectStretchedPulseLengthOutputXBarOutputSignal ( uint32_t  base,
uint32_t  lengthselect 
)
inlinestatic

Trip & Sync xbar: API to configure pulse streching length of output of Output XBars.

Parameters
base[in] Output XBar base address
lengthselect[in] Configure strech length

◆ SOC_xbarInvertOutputXBarOutputSignal()

static void SOC_xbarInvertOutputXBarOutputSignal ( uint32_t  base,
uint32_t  invertout 
)
inlinestatic

Trip & Sync xbar: API to configure inversion of output signal of Output XBars.

Parameters
base[in] Output XBar base address
invertout[in] Mask defining the Output XBar output signal to be inverted

◆ SOC_xbarSelectOutputXBarInputSource()

static void SOC_xbarSelectOutputXBarInputSource ( uint32_t  base,
uint8_t  out,
uint32_t  group0_mask,
uint32_t  group1_mask,
uint32_t  group2_mask,
uint32_t  group3_mask,
uint32_t  group4_mask,
uint32_t  group5_mask,
uint32_t  group6_mask,
uint32_t  group7_mask,
uint32_t  group8_mask,
uint32_t  group9_mask,
uint32_t  group10_mask 
)
inlinestatic

Trip & Sync xbar: API to select input sources of Output XBar.

Parameters
base[in] Output XBar base address
out[in] Instance of Output XBar
group0_mask[in] Mask to OR inputs from group 0
group1_mask[in] Mask to OR inputs from group 1
group2_mask[in] Mask to OR inputs from group 2
group3_mask[in] Mask to OR inputs from group 3
group4_mask[in] Mask to OR inputs from group 4
group5_mask[in] Mask to OR inputs from group 5
group6_mask[in] Mask to OR inputs from group 6
group7_mask[in] Mask to OR inputs from group 7
group8_mask[in] Mask to OR inputs from group 8
group9_mask[in] Mask to OR inputs from group 9
group10_mask[in] Mask to OR inputs from group 10

◆ SOC_xbarSelectPWMSyncOutXBarInput()

static void SOC_xbarSelectPWMSyncOutXBarInput ( uint32_t  base,
uint8_t  out,
uint32_t  input 
)
inlinestatic

Trip & Sync xbar: API to select input sources of PWM Syncout XBar.

Parameters
base[in] PWM Syncout XBar base address
out[in] Instance of PWM Syncout XBar
input[in] Mask to OR inputs

◆ SOC_xbarSelectEdmaTrigXbarInputSource()

static void SOC_xbarSelectEdmaTrigXbarInputSource ( uint32_t  base,
uint8_t  out,
uint8_t  mux_control 
)
inlinestatic

SoC level xbars: API to select input source of EDMA Trigger XBar.

Parameters
base[in] EDMA Trigger XBar base address
out[in] Instance of EDMA Trigger XBar
mux_control[in] Mux control to select input source

◆ SOC_xbarSelectGpioIntrXbarInputSource()

static void SOC_xbarSelectGpioIntrXbarInputSource ( uint32_t  base,
uint8_t  out,
uint8_t  mux_control 
)
inlinestatic

SoC level xbars: API to select input source of GPIO Interrupt XBar.

Parameters
base[in] GPIO Interrupt XBar base address
out[in] Instance of GPIO Interrupt XBar
mux_control[in] Mux control to select input source

◆ SOC_xbarSelectIcssmIntrXbarInputSource()

static void SOC_xbarSelectIcssmIntrXbarInputSource ( uint32_t  base,
uint8_t  out,
uint8_t  mux_control 
)
inlinestatic

SoC level xbars: API to select input source of ICSSM Interrupt XBar.

Parameters
base[in] ICSSM Interrupt XBar base address
out[in] Instance of ICSSM Interrupt XBar
mux_control[in] Mux control to select input source

◆ SOC_xbarSelectTimesyncXbar0InputSource()

static void SOC_xbarSelectTimesyncXbar0InputSource ( uint32_t  base,
uint8_t  out,
uint8_t  mux_control 
)
inlinestatic

SoC level xbars: API to select input source of TimeSync XBar0.

Parameters
base[in] TimeSync XBar0 base address
out[in] Instance of TimeSync XBar0
mux_control[in] Mux control to select input source

◆ SOC_xbarSelectTimesyncXbar1InputSource()

static void SOC_xbarSelectTimesyncXbar1InputSource ( uint32_t  base,
uint8_t  out,
uint8_t  mux_control 
)
inlinestatic

SoC level xbars: API to select input source of TimeSync XBar1.

Parameters
base[in] TimeSync XBar1 base address
out[in] Instance of TimeSync XBar1
mux_control[in] Mux control to select input source