AM263x MCU+ SDK  10.00.00
ECAP APWM mode

Introduction

This example uses the ECAP in APWM mode to generate a PWM signal.

The example does the below

  • Configures ECAP in APWM mode and configures values in period and compare registers.
  • Waits for the specified time using the ECAP ISR.

External Connections

Connect OUTPUTXBAR1 output to oscilloscope

AM263PX-CC

When using AM263x-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)

  • Connect HSEC Pin 85 to oscilloscope

AM263PX-LP

When using AM263x-LP

  • Connect boosterpack header J6/J8 Pin 50 to oscilloscope

AM263X-CC

When using AM263x-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)

  • Connect HSEC Pin 81 to oscilloscope

AM263X-LP

When using AM263x-LP

  • Connect boosterpack header J6/J8 Pin 58 to oscilloscope

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263x-cc, am263x-lp
Example folder examples/drivers/ecap/ecap_apwm_mode/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run

See Also

ECAP

Sample Output

Shown below is a sample output when the application is run,

ECAP APWM Mode Test Started ...
ECAP APWM Test Passed!!
All tests have passed!!