AM263x Motor Control SDK  10.00.00
APIs for Data Log Library

Introduction

Here is the list of APIs used for Digital Control Library

Data Structures

struct  DATALOG_Obj
 Defines the data logging (DATALOG) object. More...
 

Functions

DATALOG_Handle DATALOG_init (void *pMemory, const size_t numBytes, Trigger_type trigger, float32_t trig_value, int32_t scale)
 Initializes the data logger. More...
 
static void DATALOG_update (DATALOG_Handle handle)
 Updates the data logger. More...
 

Typedefs

typedef struct _DATALOG_Obj_ * DATALOG_Handle
 Defines the DATALOG handle. More...
 

Enumerations

enum  Trigger_type { manual, auto_trigger }
 

Macros

#define DATALOG_DEFAULTS
 Defines the default initialization for the DLOG object. More...
 

Macro Definition Documentation

◆ DATALOG_DEFAULTS

#define DATALOG_DEFAULTS
Value:
{ \
{NULL, \
NULL, \
NULL, \
NULL}, \
true, \
false, \
0, \
DATA_LOG_BUFF_SIZE \
}

Defines the default initialization for the DLOG object.

Typedef Documentation

◆ DATALOG_Handle

typedef struct _DATALOG_Obj_* DATALOG_Handle

Defines the DATALOG handle.

Enumeration Type Documentation

◆ Trigger_type

Enumerator
manual 
auto_trigger 

Function Documentation

◆ DATALOG_init()

DATALOG_Handle DATALOG_init ( void *  pMemory,
const size_t  numBytes,
Trigger_type  trigger,
float32_t  trig_value,
int32_t  scale 
)

Initializes the data logger.

Parameters
[in]pMemoryThe pointer to memory
[in]numBytessize of datalog_obj
[in]triggermanual or auto_triiger
[in]trig_valueTrigger value used for Auto triger type to initiate datalog
[in]scaleHow many datalog update to be skipped

◆ DATALOG_update()

static void DATALOG_update ( DATALOG_Handle  handle)
inlinestatic

Updates the data logger.

Parameters
[in]handleDatalog handle need to be provided

Variable Documentation

◆ datalog

DATALOG_Obj datalog
extern

Defines the DATALOG object.

◆ datalogHandle

DATALOG_Handle datalogHandle
extern

the handle for the Datalog object

NULL
#define NULL
Definition: dcl_macro.h:50