![Logo](ti_logo.svg) |
AM263x MCU+ SDK
09.02.00
|
|
uint32_t edmaRegionId
Definition: qspi_edma_lld.h:64
uint32_t edmaParam
Definition: qspi_edma_lld.h:60
uint32_t edmaTcc
Definition: qspi_edma_lld.h:54
uint32_t edmaBaseAddr
Definition: qspi_edma_lld.h:66
EDMA interrupt configuration object. The object is passed to the EDMA_registerIntr() function....
Definition: edma/v0/edma.h:479
uint32_t edmaChainChId
Definition: qspi_edma_lld.h:58
QSPI EDMA Parameters.
Definition: qspi_edma_lld.h:53
uint32_t edmaChainParam
Definition: qspi_edma_lld.h:62
uint32_t edmaChId
Definition: qspi_edma_lld.h:56
QSPI driver object.
Definition: qspi_lld.h:423
Edma_IntrObject edmaIntrObj
Definition: qspi_edma_lld.h:70
int32_t QSPI_edmaChannelConfig(QSPILLD_Handle qspiHandle)
Function to initialize EDMA before transfers.
int32_t QSPI_edmaChannelFree(QSPILLD_Handle qspiHandle)
Function to free EDMA resources.
This file contains the prototype of EDMA driver APIs.
uint32_t isIntEnabled
Definition: qspi_edma_lld.h:68
QSPI LLD Driver API/interface file.
void QSPI_edmaTransfer(void *dst, void *src, uint32_t length, QSPILLD_Handle qspiHandle, uint32_t timeout)
Function to transfer QSPI data using EDMA.