AM263x MCU+ SDK  09.02.00
qspi/v0/qspi.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2021-2024 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
50 #ifndef QSPI_H_
51 #define QSPI_H_
52 
53 /* ========================================================================== */
54 /* Include Files */
55 /* ========================================================================== */
56 
57 #include <stdint.h>
58 #include <stdbool.h>
59 #include <kernel/dpl/HwiP.h>
60 #include <kernel/dpl/SemaphoreP.h>
61 #include <drivers/hw_include/cslr_qspi.h>
62 #include <drivers/edma.h>
65 
66 #ifdef __cplusplus
67 extern "C" {
68 #endif
69 
70 /* ========================================================================== */
71 /* Macros & Typedefs */
72 /* ========================================================================== */
73 
75 typedef void *QSPI_Handle;
76 
85 #define QSPI_CMD_INVALID_OPCODE (0xFFU)
86 #define QSPI_CMD_INVALID_ADDR (0xFFFFFFFFU)
87 
97 #define QSPI_TRANSFER_COMPLETED (0U)
98 #define QSPI_TRANSFER_STARTED (1U)
99 #define QSPI_TRANSFER_CANCELLED (2U)
100 #define QSPI_TRANSFER_FAILED (3U)
101 #define QSPI_TRANSFER_CSN_DEASSERT (4U)
102 #define QSPI_TRANSFER_TIMEOUT (5U)
103 
105 /* ========================================================================== */
106 /* Structure Definitions */
107 /* ========================================================================== */
108 
116 typedef struct
117 {
118  uint32_t count;
120  void *buf;
122  uint32_t addrOffset;
124  uint32_t status;
126  uint32_t transferTimeout;
129 
130 typedef struct
131 {
132  uint8_t cmd;
134  uint32_t cmdAddr;
137  uint8_t numAddrBytes;
139  void *rxDataBuf;
141  uint32_t rxDataLen;
144 
145 typedef struct
146 {
147  uint8_t cmd;
149  uint32_t cmdAddr;
152  uint8_t numAddrBytes;
154  void *txDataBuf;
156  uint32_t txDataLen;
159 
170 typedef struct
171 {
172  uint32_t edmaInst;
174 } QSPI_Params;
175 
179 typedef struct
180 {
181  /*
182  * User params
183  */
186  uint32_t transferMode;
188  uint32_t rxLines;
190  uint8_t readCmd;
192  uint8_t writeCmd;
194  uint32_t frmLength;
196  uint32_t numAddrBytes;
198  uint32_t numDummyBits;
204  /*
205  * State variables
206  */
207  uint32_t isOpen;
221  /* QSPI LLD Init Object and Handle */
222 
225  /* QSPI LLD Object and Handle */
226 } QSPI_Object;
227 
228 
230 typedef struct
231 {
232  /*
233  * SOC configuration
234  */
235  uintptr_t baseAddr;
237  uintptr_t memMapBaseAddr;
239  uint32_t inputClkFreq;
241  uint32_t baudRateDiv;
243  uint32_t chipSelect;
245  uint32_t csPol;
247  uint32_t frmFmt;
249  uint32_t dataDelay;
251  uint32_t rxLines;
253  uint32_t wrdLen;
255  uint32_t intrNum;
259  bool wordIntr;
261  bool frameIntr;
263  uint8_t intrPriority;
265  bool dmaEnable;
268 } QSPI_Attrs;
269 
270 typedef struct
271 {
276 } QSPI_Config;
277 
279 extern QSPI_Config gQspiConfig[];
281 extern uint32_t gQspiConfigNum;
284 
285 /* ========================================================================== */
286 /* Function Declarations */
287 /* ========================================================================== */
288 
292 void QSPI_init(void);
293 
297 void QSPI_deinit(void);
298 
304 void QSPI_Params_init( QSPI_Params *qspiParams);
305 
320 QSPI_Handle QSPI_open(uint32_t index, const QSPI_Params *openParams);
321 
331 void QSPI_close(QSPI_Handle handle);
332 
345 QSPI_Handle QSPI_getHandle(uint32_t index);
346 
359 uint32_t QSPI_getInputClk(QSPI_Handle handle);
360 
379 
390 int32_t QSPI_writeCmd(QSPI_Handle handle, QSPI_WriteCmdParams *wrParams);
391 
402 int32_t QSPI_writeConfigMode(QSPI_Handle handle, const QSPI_Transaction *trans);
403 
416 
427 int32_t QSPI_readCmd(QSPI_Handle handle, QSPI_ReadCmdParams *rdParams);
428 
441 
452 
461 
470 
488 int32_t QSPI_setPreScaler(QSPI_Handle handle, uint32_t clkDividerVal);
489 
498 int32_t QSPI_setWriteCmd(QSPI_Handle handle, uint8_t command);
499 
508 int32_t QSPI_setReadCmd(QSPI_Handle handle, uint8_t command);
509 
521 int32_t QSPI_setAddressByteCount(QSPI_Handle handle, uint32_t count);
522 
534 int32_t QSPI_setDummyBitCount(QSPI_Handle handle, uint32_t count);
535 
545 int32_t QSPI_setMemAddrSpace(QSPI_Handle handle, uint32_t memMappedPortSwitch);
546 
555 int32_t QSPI_intEnable(QSPI_Handle handle, uint32_t intFlag);
556 
565 int32_t QSPI_intDisable(QSPI_Handle handle, uint32_t intFlag);
566 
575 int32_t QSPI_intClear(QSPI_Handle handle, uint32_t intFlag);
576 
589 int32_t QSPI_setRxLines(QSPI_Handle handle, uint32_t rxLines);
590 
600 uint32_t QSPI_getRxLines(QSPI_Handle handle);
601 
602 void OSPI_phyGetTuningData(uint32_t *phyTuningData, uint32_t *phyTuningDataSize);
603 
604 #ifdef __cplusplus
605 }
606 #endif
607 
608 #endif /* #ifndef QSPI_H_ */
609 
QSPI_writeCmdParams_init
void QSPI_writeCmdParams_init(QSPI_WriteCmdParams *wrParams)
Function to initialize the QSPI_Transaction structure.
gQspiConfig
QSPI_Config gQspiConfig[]
Externally defined driver configuration array.
QSPI_Attrs::frmFmt
uint32_t frmFmt
Definition: qspi/v0/qspi.h:247
QSPI_Object::qspiEdmaHandle
void * qspiEdmaHandle
Definition: qspi/v0/qspi.h:201
QSPI_Object::readCmd
uint8_t readCmd
Definition: qspi/v0/qspi.h:190
QSPI_Object::qspilldHandle
QSPILLD_Handle qspilldHandle
Definition: qspi/v0/qspi.h:224
QSPI_ReadCmdParams::numAddrBytes
uint8_t numAddrBytes
Definition: qspi/v0/qspi.h:137
QSPI_Attrs::dataDelay
uint32_t dataDelay
Definition: qspi/v0/qspi.h:249
QSPI_Params_init
void QSPI_Params_init(QSPI_Params *qspiParams)
Initialize data structure with defaults.
QSPI_writeConfigModeIntr
int32_t QSPI_writeConfigModeIntr(QSPI_Handle handle, QSPI_WriteCmdParams *wrParams)
Function to perform write to the flash in interrupt mode mode.
QSPI_writeCmd
int32_t QSPI_writeCmd(QSPI_Handle handle, QSPI_WriteCmdParams *wrParams)
Function to send specific commands and related data to flash.
QSPI_Config
Definition: qspi/v0/qspi.h:271
QSPI_Transaction::addrOffset
uint32_t addrOffset
Definition: qspi/v0/qspi.h:122
QSPI_intDisable
int32_t QSPI_intDisable(QSPI_Handle handle, uint32_t intFlag)
This function is used to disable word or frame complete interrupt.
QSPI_open
QSPI_Handle QSPI_open(uint32_t index, const QSPI_Params *openParams)
This function opens a given QSPI peripheral.
QSPI_Attrs::baudRateDiv
uint32_t baudRateDiv
Definition: qspi/v0/qspi.h:241
QSPI_setPreScaler
int32_t QSPI_setPreScaler(QSPI_Handle handle, uint32_t clkDividerVal)
Set the QSPI clock register divider value.
QSPI_Attrs::intrNum
uint32_t intrNum
Definition: qspi/v0/qspi.h:255
QSPI_getHandle
QSPI_Handle QSPI_getHandle(uint32_t index)
This function returns the handle of an open QSPI Instance from the instance index.
qspi_edma_lld.h
QSPI_Object::transferMode
uint32_t transferMode
Definition: qspi/v0/qspi.h:186
QSPI_Attrs
QSPI instance attributes - used during init time.
Definition: qspi/v0/qspi.h:231
QSPI_EdmaParams
QSPI EDMA Parameters.
Definition: qspi_edma_lld.h:53
QSPI_Object::lockObj
SemaphoreP_Object lockObj
Definition: qspi/v0/qspi.h:209
QSPI_Transaction::count
uint32_t count
Definition: qspi/v0/qspi.h:118
QSPI_Attrs::intrEnable
bool intrEnable
Definition: qspi/v0/qspi.h:257
QSPI_Params::edmaInst
uint32_t edmaInst
Definition: qspi/v0/qspi.h:172
QSPI_intEnable
int32_t QSPI_intEnable(QSPI_Handle handle, uint32_t intFlag)
This function is used to enable word or frame complete interrupt.
QSPILLD_InitObject
QSPI driver initialization object.
Definition: qspi_lld.h:378
QSPI_Attrs::wrdLen
uint32_t wrdLen
Definition: qspi/v0/qspi.h:253
QSPI_Attrs::wordIntr
bool wordIntr
Definition: qspi/v0/qspi.h:259
QSPI_Object
QSPI driver object.
Definition: qspi/v0/qspi.h:180
SemaphoreP.h
QSPI_getRxLines
uint32_t QSPI_getRxLines(QSPI_Handle handle)
Get QSPI Rx lines in the QSPI object.
QSPI_Object::qspilldObject
QSPILLD_Object qspilldObject
Definition: qspi/v0/qspi.h:223
QSPI_Attrs::inputClkFreq
uint32_t inputClkFreq
Definition: qspi/v0/qspi.h:239
QSPI_Attrs::intrPriority
uint8_t intrPriority
Definition: qspi/v0/qspi.h:263
QSPI_WriteCmdParams::cmdAddr
uint32_t cmdAddr
Definition: qspi/v0/qspi.h:149
QSPI_Attrs::chipSelect
uint32_t chipSelect
Definition: qspi/v0/qspi.h:243
QSPI_Attrs::frameIntr
bool frameIntr
Definition: qspi/v0/qspi.h:261
QSPI_Params
QSPI Parameters.
Definition: qspi/v0/qspi.h:171
edma.h
QSPI_Object::qspilldInitObject
QSPILLD_InitObject qspilldInitObject
Definition: qspi/v0/qspi.h:219
QSPI_setAddressByteCount
int32_t QSPI_setAddressByteCount(QSPI_Handle handle, uint32_t count)
Function to set number of address bytes to be used.
QSPI_Config::object
QSPI_Object * object
Definition: qspi/v0/qspi.h:274
QSPI_Object::handle
QSPI_Handle handle
Definition: qspi/v0/qspi.h:184
QSPILLD_Object
QSPI driver object.
Definition: qspi_lld.h:423
QSPI_Object::transaction
QSPI_Transaction * transaction
Definition: qspi/v0/qspi.h:216
QSPI_ReadCmdParams::rxDataLen
uint32_t rxDataLen
Definition: qspi/v0/qspi.h:141
QSPI_Handle
void * QSPI_Handle
A handle that is returned from a QSPI_open() call.
Definition: qspi/v0/qspi.h:75
QSPI_Object::transferSemObj
SemaphoreP_Object transferSemObj
Definition: qspi/v0/qspi.h:211
QSPI_Object::hwiObj
HwiP_Object hwiObj
Definition: qspi/v0/qspi.h:213
QSPI_WriteCmdParams::txDataBuf
void * txDataBuf
Definition: qspi/v0/qspi.h:154
QSPI_ReadCmdParams
Definition: qspi/v0/qspi.h:131
QSPI_setDummyBitCount
int32_t QSPI_setDummyBitCount(QSPI_Handle handle, uint32_t count)
Function to set number of dummy bits to be used.
HwiP.h
QSPI_init
void QSPI_init(void)
This function initializes the QSPI module.
QSPI_Object::frmLength
uint32_t frmLength
Definition: qspi/v0/qspi.h:194
QSPI_ReadCmdParams::cmd
uint8_t cmd
Definition: qspi/v0/qspi.h:132
QSPI_Object::writeCmd
uint8_t writeCmd
Definition: qspi/v0/qspi.h:192
QSPI_readConfigModeIntr
int32_t QSPI_readConfigModeIntr(QSPI_Handle handle, QSPI_ReadCmdParams *rdParams)
Function to perform read from the flash in interrupt mode.
QSPI_ReadCmdParams::rxDataBuf
void * rxDataBuf
Definition: qspi/v0/qspi.h:139
QSPI_setWriteCmd
int32_t QSPI_setWriteCmd(QSPI_Handle handle, uint8_t command)
Function to set write command to be used.
QSPI_setRxLines
int32_t QSPI_setRxLines(QSPI_Handle handle, uint32_t rxLines)
Set QSPI Rx lines in the QSPI object.
QSPI_ReadCmdParams::cmdAddr
uint32_t cmdAddr
Definition: qspi/v0/qspi.h:134
QSPI_Object::numDummyBits
uint32_t numDummyBits
Definition: qspi/v0/qspi.h:198
QSPI_intClear
int32_t QSPI_intClear(QSPI_Handle handle, uint32_t intFlag)
This function is used to clear word or frame complete interrupt.
QSPI_Attrs::memMapBaseAddr
uintptr_t memMapBaseAddr
Definition: qspi/v0/qspi.h:237
QSPI_transaction_init
void QSPI_transaction_init(QSPI_Transaction *trans)
Function to initialize the QSPI_Transaction structure.
QSPI_WriteCmdParams::cmd
uint8_t cmd
Definition: qspi/v0/qspi.h:147
QSPI_writeConfigMode
int32_t QSPI_writeConfigMode(QSPI_Handle handle, const QSPI_Transaction *trans)
Function to perform writes to the flash in configuration mode.
QSPI_Object::qspilldInitHandle
QSPILLD_InitHandle qspilldInitHandle
Definition: qspi/v0/qspi.h:220
QSPI_readCmd
int32_t QSPI_readCmd(QSPI_Handle handle, QSPI_ReadCmdParams *rdParams)
Function to send specific commands and receive related data from flash.
QSPI_Transaction::status
uint32_t status
Definition: qspi/v0/qspi.h:124
QSPI_readCmdParams_init
void QSPI_readCmdParams_init(QSPI_ReadCmdParams *rdParams)
Function to initialize the QSPI_Transaction structure.
qspi_lld.h
QSPI LLD Driver API/interface file.
QSPI_Object::numAddrBytes
uint32_t numAddrBytes
Definition: qspi/v0/qspi.h:196
QSPI_Attrs::rxLines
uint32_t rxLines
Definition: qspi/v0/qspi.h:251
QSPI_Transaction::transferTimeout
uint32_t transferTimeout
Definition: qspi/v0/qspi.h:126
HwiP_Object
Opaque Hwi object used with the Hwi APIs.
Definition: HwiP.h:93
QSPI_Transaction::buf
void * buf
Definition: qspi/v0/qspi.h:120
QSPI_readMemMapMode
int32_t QSPI_readMemMapMode(QSPI_Handle handle, QSPI_Transaction *trans)
Function to perform reads from the flash in memory mapped mode.
QSPI_setMemAddrSpace
int32_t QSPI_setMemAddrSpace(QSPI_Handle handle, uint32_t memMappedPortSwitch)
This function is used to switch between memory mapped and configuration mode.
QSPI_Attrs::baseAddr
uintptr_t baseAddr
Definition: qspi/v0/qspi.h:235
SemaphoreP_Object
Opaque semaphore object used with the semaphore APIs.
Definition: SemaphoreP.h:59
QSPI_setReadCmd
int32_t QSPI_setReadCmd(QSPI_Handle handle, uint8_t command)
Function to set read command to be used.
QSPI_Attrs::csPol
uint32_t csPol
Definition: qspi/v0/qspi.h:245
QSPI_Config::attrs
const QSPI_Attrs * attrs
Definition: qspi/v0/qspi.h:272
QSPI_Object::isOpen
uint32_t isOpen
Definition: qspi/v0/qspi.h:207
gqspiEdmaParam
QSPI_EdmaParams gqspiEdmaParam
EDMA Paramter for QSPI Transaction.
Definition: qspi/v0/qspi.h:283
QSPI_close
void QSPI_close(QSPI_Handle handle)
Function to close a QSPI peripheral specified by the QSPI handle.
QSPI_deinit
void QSPI_deinit(void)
This function de-initializes the QSPI module.
QSPI_Transaction
Data structure used with QSPI_Transfers - QSPI_writeConfigMode, QSPI_readMemMapMode.
Definition: qspi/v0/qspi.h:117
QSPI_WriteCmdParams::txDataLen
uint32_t txDataLen
Definition: qspi/v0/qspi.h:156
QSPI_WriteCmdParams::numAddrBytes
uint8_t numAddrBytes
Definition: qspi/v0/qspi.h:152
QSPI_Object::rxLines
uint32_t rxLines
Definition: qspi/v0/qspi.h:188
gQspiConfigNum
uint32_t gQspiConfigNum
Externally defined driver configuration array size.
QSPI_getInputClk
uint32_t QSPI_getInputClk(QSPI_Handle handle)
This function returns the input clock at which QSPI was programmed.
QSPI_Attrs::dmaEnable
bool dmaEnable
Definition: qspi/v0/qspi.h:265
OSPI_phyGetTuningData
void OSPI_phyGetTuningData(uint32_t *phyTuningData, uint32_t *phyTuningDataSize)
QSPI_WriteCmdParams
Definition: qspi/v0/qspi.h:146