|
AM263x MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
33 #ifndef MCSPI_DMA_EDMA_H_
34 #define MCSPI_DMA_EDMA_H_
43 typedef struct McspiDma_EdmaArgs_s
49 typedef struct MCSPI_DmaChConfig_s
uint32_t isOpen
Definition: mcspi_dma_edma.h:73
Definition: mcspi_dma_edma.h:50
uint32_t edmaTxParam
Definition: mcspi_dma_edma.h:61
EDMA interrupt configuration object. The object is passed to the EDMA_registerIntr() function....
Definition: edma/v0/edma.h:479
uint32_t edmaDummyParam
Definition: mcspi_dma_edma.h:63
Definition: mcspi_dma_edma.h:44
uint32_t edmaRxParam
Definition: mcspi_dma_edma.h:59
uint32_t edmaTccRx
Definition: mcspi_dma_edma.h:51
uint32_t edmaRegionId
Definition: mcspi_dma_edma.h:65
uint32_t edmaTxChId
Definition: mcspi_dma_edma.h:57
uint32_t edmaRxChId
Definition: mcspi_dma_edma.h:55
uint32_t edmaBaseAddr
Definition: mcspi_dma_edma.h:67
This file contains the prototype of EDMA driver APIs.
uint32_t edmaTccTx
Definition: mcspi_dma_edma.h:53
Edma_IntrObject edmaIntrObjRx
Definition: mcspi_dma_edma.h:69
Edma_IntrObject edmaIntrObjTx
Definition: mcspi_dma_edma.h:71
void * drvHandle
Definition: mcspi_dma_edma.h:45