|
AM263x Motor Control SDK
09.01.00
|
|
Go to the documentation of this file.
33 #ifndef TAMAGAWA_UART_DRV_H_
34 #define TAMAGAWA_UART_DRV_H_
60 #define MAX_EEPROM_ADDRESS (127)
64 #define MAX_EEPROM_WRITE_DATA (255)
@ DATA_ID_C
Definition: tamagawa_soc_uart_interface.h:77
@ DATA_ID_NUM
Definition: tamagawa_soc_uart_interface.h:79
uint8_t sf
Definition: tamagawa_soc_uart_interface.h:101
int32_t tamagawa_command_process(volatile struct tamagawa_uart_interface *tamagawa_interface, UARTLLD_Handle *gUartHandle, int32_t cmd)
Process The Tamagawa Command.
uint8_t data_id
Definition: tamagawa_soc_uart_interface.h:113
@ DATA_ID_1
Definition: tamagawa_soc_uart_interface.h:71
uint8_t enid
Definition: tamagawa_soc_uart_interface.h:102
uint32_t abs
Definition: tamagawa_soc_uart_interface.h:98
Tamagawa Interface.
Definition: tamagawa_soc_uart_interface.h:112
uint8_t rx_crc
Definition: tamagawa_soc_uart_interface.h:116
@ DATA_ID_7
Definition: tamagawa_soc_uart_interface.h:75
uint32_t gpio_pin_number
Definition: tamagawa_soc_uart_interface.h:119
int32_t tamagawa_crc_verify(volatile struct tamagawa_uart_interface *tamagawa_interface)
Compare Received CRC and Calculated CRC.
uint8_t almc
Definition: tamagawa_soc_uart_interface.h:103
uint8_t crc
Definition: tamagawa_soc_uart_interface.h:106
uint8_t edf
Definition: tamagawa_soc_uart_interface.h:90
uint8_t edf
Definition: tamagawa_soc_uart_interface.h:105
@ DATA_ID_2
Definition: tamagawa_soc_uart_interface.h:72
data_id
Data ID codes.
Definition: tamagawa_soc_uart_interface.h:69
@ DATA_ID_6
Definition: tamagawa_soc_uart_interface.h:74
Tamagawa Interface Received data.
Definition: tamagawa_soc_uart_interface.h:97
@ DATA_ID_8
Definition: tamagawa_soc_uart_interface.h:76
@ DATA_ID_3
Definition: tamagawa_soc_uart_interface.h:73
void tamagawa_init(volatile struct tamagawa_uart_interface *tamagawa_interface, uint32_t instance, uint32_t base_address, uint32_t pin_number, uint32_t pin_direction)
Configure GOPIO pin for RTSn(sw flow control)
uint8_t adf
Definition: tamagawa_soc_uart_interface.h:104
struct tamagawa_tx tx
Definition: tamagawa_soc_uart_interface.h:114
Tamagawa Interface Transmit data.
Definition: tamagawa_soc_uart_interface.h:88
uint32_t abm
Definition: tamagawa_soc_uart_interface.h:99
uint8_t cf
Definition: tamagawa_soc_uart_interface.h:100
uint8_t adf
Definition: tamagawa_soc_uart_interface.h:89
uint32_t uart_instance
Definition: tamagawa_soc_uart_interface.h:117
struct tamagawa_rx rx
Definition: tamagawa_soc_uart_interface.h:115
@ DATA_ID_D
Definition: tamagawa_soc_uart_interface.h:78
uint32_t gpio_base_address
Definition: tamagawa_soc_uart_interface.h:118
@ DATA_ID_0
Definition: tamagawa_soc_uart_interface.h:70