AM263x MCU+ SDK  09.00.00
sipc_notify_cfg.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2022-23 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
21  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 #ifndef SIPC_NOTIFY_CFG_H_
33 #define SIPC_NOTIFY_CFG_H_
34 
35 #ifdef __cplusplus
36 extern "C"
37 {
38 #endif
39 
40 #include <drivers/hw_include/am263x/cslr_soc.h>
41 #include <kernel/dpl/CpuIdP.h>
42 
46 #define SIPC_MSG_SIZE (13u)
47 
48 /* Max number of interrupt configs possible for AM263x */
49 #define INTR_CFG_NUM_MAX (1u)
50 
51 /* If SIPC is compiled for R5 core then Max client ID = 32
52  * Else for HSM its 2 */
53 
54 
55 
56 /* HSM specific register addresses defined here to remove the dependency on CSL files */
57 #define HSM_SOC_CTRL_U_BASE (0x40000000U)
58 #define HSM_SOC_CTRL_HSM_MBOX_READ_DONE_ACK (0x00000048U)
59 #define HSM_SOC_CTRL_HSM_MBOX_READ_DONE (0x0000004CU)
60 
61 /* R5 Register for sending and receiving IPC interrutps
62  * As write DONE interrupt line is being used by regular IPC communication we will use READ_DONE_ACK
63  * register to post the interrupt to receiving core and it will read READ_DONE register to process
64  * that interrupt */
65 #define R5FSS0_0_MBOX_READ_DONE_ACK (CSL_MSS_CTRL_U_BASE + CSL_MSS_CTRL_R5SS0_CORE0_MBOX_READ_DONE_ACK)
66 #define R5FSS0_0_MBOX_READ_DONE (CSL_MSS_CTRL_U_BASE + CSL_MSS_CTRL_R5SS0_CORE0_MBOX_READ_DONE)
67 #define R5FSS0_1_MBOX_READ_DONE_ACK (CSL_MSS_CTRL_U_BASE + CSL_MSS_CTRL_R5SS0_CORE1_MBOX_READ_DONE_ACK)
68 #define R5FSS0_1_MBOX_READ_DONE (CSL_MSS_CTRL_U_BASE + CSL_MSS_CTRL_R5SS0_CORE1_MBOX_READ_DONE)
69 #define R5FSS1_0_MBOX_READ_DONE_ACK (CSL_MSS_CTRL_U_BASE + CSL_MSS_CTRL_R5SS1_CORE0_MBOX_READ_DONE_ACK)
70 #define R5FSS1_0_MBOX_READ_DONE (CSL_MSS_CTRL_U_BASE + CSL_MSS_CTRL_R5SS1_CORE0_MBOX_READ_DONE)
71 #define R5FSS1_1_MBOX_READ_DONE_ACK (CSL_MSS_CTRL_U_BASE + CSL_MSS_CTRL_R5SS1_CORE1_MBOX_READ_DONE_ACK)
72 #define R5FSS1_1_MBOX_READ_DONE (CSL_MSS_CTRL_U_BASE + CSL_MSS_CTRL_R5SS1_CORE1_MBOX_READ_DONE)
73 
74 /* HSM registers for sending and receiving IPC interrupts */
75 #define HSM0_0_MBOX_READ_DONE_ACK (HSM_SOC_CTRL_U_BASE + HSM_SOC_CTRL_HSM_MBOX_READ_DONE_ACK)
76 #define HSM0_0_MBOX_READ_DONE (HSM_SOC_CTRL_U_BASE + HSM_SOC_CTRL_HSM_MBOX_READ_DONE)
77 
78 /* CPU bit positions within the HSM mailbox registers for sending interrupt
79  * HSM will write the READ_DONE_ACK register to raise an interrupt to R5 core */
80 #define R5FSS0_0_MBOX_WRITE_PROC_BIT_POS ( 0U)
81 #define R5FSS0_1_MBOX_WRITE_PROC_BIT_POS ( 4U)
82 #define R5FSS1_0_MBOX_WRITE_PROC_BIT_POS ( 8U)
83 #define R5FSS1_1_MBOX_WRITE_PROC_BIT_POS ( 12U)
84 
85 /* Bitshift to raise an interrupt from R5 core to HSM */
86 #define HSM0_0_MBOX_WRITE_PROC_BIT_POS ( 6U)
87 
88 /* CPU bit positions within the mailbox registers for receiving interrupts */
89 #define R5FSS0_0_MBOX_READ_PROC_BIT_POS ( 0U)
90 #define R5FSS0_1_MBOX_READ_PROC_BIT_POS ( 4U)
91 #define R5FSS1_0_MBOX_READ_PROC_BIT_POS ( 8U)
92 #define R5FSS1_1_MBOX_READ_PROC_BIT_POS (12U)
93 #define HSM0_0_MBOX_READ_PROC_BIT_POS (24U)
94 
95 /* Mailbox interrupts numbers */
96 #define R5FSS0_0_MBOX_READ_ACK_INTR ( 137U)
97 #define R5FSS0_1_MBOX_READ_ACK_INTR ( 137U)
98 #define R5FSS1_0_MBOX_READ_ACK_INTR ( 137U)
99 #define R5FSS1_1_MBOX_READ_ACK_INTR ( 137U)
100 #define HSM0_0_MBOX_READ_ACK_INTR ( 56U )
101 
107 typedef enum SIPC_CoreId_
108 {
116 
123 typedef enum SIPC_SecCoreId_
124 {
130 
131 #if defined(__ARM_ARCH_7R__)
132 
133 /* If building for R5 then read selfcore ID from the Core Cluster register */
134 static uint32_t SIPC_readSelfCoreID(void)
135 {
136  uint32_t coreId ;
137  CSL_ArmR5CPUInfo cpuId = {0, 0};
138  CSL_armR5GetCpuID(&cpuId);
139  /* both cpuId and greId fields can be either 0 or 1
140  * ex for R5FSS1-0 core grpId = 1 and cpu id = 0 */
141  coreId = cpuId.cpuID | (cpuId.grpId) << 1 ;
142  return coreId;
143 }
144 #define SELF_CORE_ID (SIPC_readSelfCoreID())
145 
152 #define SIPC_CLIENT_ID_MAX (5U)
153 
154 #else
155 #define SIPC_CLIENT_ID_MAX (2U)
156 #define SELF_CORE_ID (CORE_ID_HSM0_0)
157 #endif
158 
159 /*
160  * Client ID used by HSM server's boot notify message
161  */
162 #define SIPC_BOOT_NOTIFY_CLIENT_ID (0U)
163 
164 #ifdef __cplusplus
165 }
166 #endif
167 
168 #endif
SIPC_SecCoreId
SIPC_SecCoreId
Secure host Id to identify different secure hosts. Max number of secure host on AM263x is 2.
Definition: sipc_notify_cfg.h:124
CORE_INDEX_SEC_MASTER_1
@ CORE_INDEX_SEC_MASTER_1
Definition: sipc_notify_cfg.h:126
CORE_ID_R5FSS1_1
@ CORE_ID_R5FSS1_1
Definition: sipc_notify_cfg.h:112
CORE_INDEX_HSM
@ CORE_INDEX_HSM
Definition: sipc_notify_cfg.h:127
CSL_ArmR5CPUInfo::grpId
uint32_t grpId
Definition: CpuIdP.h:62
CORE_ID_MAX
@ CORE_ID_MAX
Definition: sipc_notify_cfg.h:114
CORE_ID_R5FSS1_0
@ CORE_ID_R5FSS1_0
Definition: sipc_notify_cfg.h:111
CSL_ArmR5CPUInfo
Structure containing the CPU Info such as CPU ID and Cluster Group ID.
Definition: CpuIdP.h:57
CORE_ID_R5FSS0_0
@ CORE_ID_R5FSS0_0
Definition: sipc_notify_cfg.h:109
CORE_ID_HSM0_0
@ CORE_ID_HSM0_0
Definition: sipc_notify_cfg.h:113
SIPC_coreId
SIPC_coreId
Core Ids to identify different cores.
Definition: sipc_notify_cfg.h:108
MAX_SEC_CORES_WITH_HSM
@ MAX_SEC_CORES_WITH_HSM
Definition: sipc_notify_cfg.h:128
CORE_INDEX_SEC_MASTER_0
@ CORE_INDEX_SEC_MASTER_0
Definition: sipc_notify_cfg.h:125
CpuIdP.h
CSL_ArmR5CPUInfo::cpuID
uint32_t cpuID
Definition: CpuIdP.h:58
CSL_armR5GetCpuID
void CSL_armR5GetCpuID(CSL_ArmR5CPUInfo *cpuInfo)
Get the cluster group and CPU ID for current R5 Core.
CORE_ID_R5FSS0_1
@ CORE_ID_R5FSS0_1
Definition: sipc_notify_cfg.h:110