![Logo](ti_logo.svg) |
AM263x MCU+ SDK
09.00.00
|
|
Go to the documentation of this file.
33 #ifndef BOOTLOADER_SOC_AM263X_H_
34 #define BOOTLOADER_SOC_AM263X_H_
42 #include <drivers/hw_include/cslr_soc.h>
54 #define BOOTLOADER_DEVTYPE_HSSE (0x0AU)
56 #define BOOTLOADER_DEVTYPE_HSFS (0xAAU)
58 #define BOOTLOADER_DEVTYPE_GP (0x03U)
60 #define BOOTLOADER_CLIENT_ID (0x02)
82 typedef struct Bootloader_socCoreOpModeConfig_s
int32_t Bootloader_socCpuSetClock(uint32_t cpuId, uint32_t cpuHz)
Set the clock of a particular CPU in the AM64x SOC.
char * Bootloader_socGetCoreName(uint32_t cpuId)
Get the name of a core.
int32_t Bootloader_socCpuRequest(uint32_t cpuId)
Request for a particular CPU in the AM64x SOC.
void Bootloader_socConfigurePll(void)
API to configure Core and Per PLLS.
void Bootloader_socLoadHsmRtFw(const uint8_t *HsmRtFw, uint32_t hsmRTSize)
API to load hsm runtime firmware.
int32_t Bootloader_socCpuSetEntryPoint(uint32_t cpuId, uintptr_t entryPoint)
Set entry point for self CPU in the AM64x SOC from reset.
uint32_t Bootloader_socIsAuthRequired(void)
API to check if authentication is required for the device. Checks the SYS_STATUS register to see if d...
int32_t Bootloader_socCpuPowerOnReset(uint32_t cpuId, void *socCoreOpMode)
Do power-on-reset of a particular CPU in the AM64x SOC.
Data structure containing information about the operating mode specific to the SOC.
Definition: bootloader_soc.h:83
uint32_t defaultClockHz
Definition: bootloader_soc.h:71
int32_t Bootloader_socCpuResetRelease(uint32_t cpuId, uintptr_t entryPoint)
Release a particular CPU in the AM64x SOC from reset.
Data structure containing information about a core specific to the SOC.
Definition: bootloader_soc.h:70
uint32_t Bootloader_socRprcToCslCoreId(uint32_t rprcCoreId)
Obtain the CSL core ID of a CPU from its RPRC core ID.
uint64_t Bootloader_socCpuGetClock(uint32_t cpuId)
Get the clock of a particular CPU in the AM64x SOC.
void Bootloader_socGetBootSeqOid(uint8_t *boot_seq_oid)
API to get boot sequence oid.
int32_t Bootloader_socCpuRelease(uint32_t cpuId)
Release a particular CPU in the AM64x SOC.
uint32_t r5fss1_opMode
Definition: bootloader_soc.h:87
void Bootloader_socInitL2MailBoxMemory(void)
API to Init L2,L3 Banks and Mailbox Memory.
int32_t Bootloader_socCpuResetReleaseSelf(void)
Release self CPU in the AM64x SOC from reset.
int32_t Bootloader_socAuthImage(uint32_t certLoadAddr)
API to authenticate (and decrypt if needed) an appimage using SYSFW.
uint32_t Bootloader_socTranslateSectionAddr(uint32_t cslCoreId, uint32_t addr)
Translate a CPU address to the SOC address wherever applicable.
uint32_t * Bootloader_socGetSelfCpuList(void)
Get the list of self cpus in the SOC.
void Bootloader_socSetAutoClock()
API to set CPU clock to 200 MHz or 400 MHz on the basis of eFUSE bits configuration.
uint32_t Bootloader_socCpuGetClkDefault(uint32_t cpuId)
Get the default clock of a particular CPU in the AM64x SOC.
int32_t Bootloader_socSecHandover(void)
API to trigger the security handover from SYSFW.
uint32_t r5fss0_opMode
Definition: bootloader_soc.h:84
int32_t Bootloader_socMemInitCpu(uint32_t cpuId)
Initialize the core memories of a specific core.