AM263x MCU+ SDK  09.00.00
ADC SOC EPWM

Introduction

This examples demonstrates periodical triggering of conversion on ADC1 by EPWM0

Example Block diagram

SOC Configurations

  • SOC 0 trigger is set by EPWM0SOCA
  • Samples on ADC1 Channel 0

Interrupt Configurations

  • ADC1INT1 source is set to EOC/SOC0
  • INTXBAR0 is set to ADC1INT1.

ISR App_adcISR

  • Reads the SOC0 result.
  • Clears ADC1INT1 flag

External Connections

AM263x-CC E2

  • feed analog input on ADC 1 Channel 0 - HSEC connecter pin - 12

AM263x-CC E1

  • feed analog input on ADC 1 Channel 0 - HSEC connecter pin - 18

AM263x-LP

  • feed analog input on ADC 1 Channel 0 - J1/J3 Pin - 24

Watch Variables

  • gAdc1Result0 : the array holds the sampled values of the ADC 1 Channel 0

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263x-cc, am263x-lp
Example folder examples/drivers/adc/adc_soc_epwm/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • Using watch variables, view the ADC conversion results.
  • View the ADC conversion results in UART console logs

See Also

ADC

Sample Output

Shown below is a sample output when the application is run,

ADC Soc EPWM Test Started
ADC 1 channel 1 output:
128
128
128
128
128
128
128
128
128
128
128
ADC Soc EPWM Test Passed
All tests have passed!!