Introduction
This example is a EtherCAT SubDevice application based on EtherCAT SubDevice Stack Code (SSC) version 5.13 from Beckhoff.
The example does the below
- Initializes the EtherCAT SubDevice stack
- Initializes the FWHAL, which kicks off the ESC
- SubDevice is taken to INIT state. It can be move to OP (operational) state by connecting it to a EtherCAT MainDevice, and process data communication is possible after that.
- Note
- Following features are not tested or implemented in this release :
- Use of flash (Online Application Upgrade) is not verified
- Run and Error LEDs are not implemented
- LEDs linked to Process Data are not implemented
- Use of I2C based EEPROM memory for TIESC EEPROM is not implemented
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 freertos |
Toolchain | ti-arm-clang |
Boards | am263x-cc, am263x-lp |
Example folder | examples/industrial_comms/ethercat_SubDevice_beckhoff_ssc_demo |
Steps to Run the Example
- To build this example, it is necessary to get the EtherCAT SubDevice Stack Code (SSC). Download EtherCAT stack version 5.13 from ETG website and extract it to a local folder. Please refer to "Application Note ET9300 (EtherCAT SubDevice Stack Code)" for more details on SSC.
- Generate the patched EtherCAT SubDevice stack code source files using any one of the below mentioned methods:
- Using the patch file
- Copy the EtherCAT SubDevice Stack files to
{SDK_INSTALL_PATH}/source/industrial_comms/ethercat_SubDevice/beckhoff_stack/stack_sources/
folder.
- Download Windows Patch Utility from gnuwin32 sourceforge. (Note that this is not a TI tool. See licensing information page for more details)
- Download Dos2Unix/Unix2Dos-Text file format converters from gnuwin32 sourceforge. (Note that this is not a TI tool. See licensing information page for more details)
- Patch file utility(Patch.exe) and unix2dos.exe utility can be found in their bin folders.
- Launch DOS Command prompt
- CD to the folder
${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_SubDevice/beckhoff_stack/patch
which contains TI_ECAT.patch.
- Execute unix2dos.exe as given below:
$(Dos2Unix/Unix2Dos-DIR)/bin/unix2dos.exe TI_ECAT.patch
- CD to patch file utility bin folder.
- Execute patch.exe as given below:
patch.exe -i ${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_SubDevice/beckhoff_stack/patch/TI_ECAT.patch -d ${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_SubDevice/beckhoff_stack/stack_sources/
Using Beckhoff SSC Tool
- Install SSC tool version 1.5.3.0. This configuration tool facilitates working with the EtherCAT SubDevice Stack Code (SSC), as it allows reducing the size of the EtherCAT SubDevice stack code by removing unused code parts depending on the desired configuration. Objects should be defined in a .xlsx file. Please refer to EtherCAT SubDevice Design - Quick Guide for details.
- Click on "Import" button and select TI_ESC_[SDK_VERSION].xml present in SoC specific folder inside
${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_SubDevice/beckhoff_stack/patch
folder.
- Make sure "Custom" is selected in the dialog box and "TI [SOC] Sample \<Texas Instruments Incorporated\>" is selected from the list.
- Set DC_SUPPORTED to 1 if not set.
- Save the project.
- Click "Project->Create new SubDevice Files". This will generate the EtherCAT Source files specific to the the selected TI device.
- Copy all the generated files except tiescappl.c, tiescappl.h and tiescapplObjects.h to
${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_SubDevice/beckhoff_stack/stack_sources/
.
- Note
- For the SDK example, tiescappl.c and tiescappl.h files are used from "${SDK_INSTALL_PATH}/examples/industrial_comms/ethercat_SubDevice_beckhoff_ssc_demo/" folder, and not from the SSC Tool generated files.
- If you want to modify the object dictionary, you can update the "${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_SubDevice/beckhoff_stack/patch/am64x_am243x_am263x/tiescappl.xlsx" file and then the SSC tool will generate the application code accordingly.
- Change macro defintions in
{SDK_INSTALL_PATH}/source/industrial_comms/ethercat_SubDevice/beckhoff_stack/stack_sources/ecat_def.h
, if required for your application. Please ensure that TIESC_HW is set to 1, and TIESC_APPLICATION is set to 1.
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- To test the application, one can use TwinCAT or any other compatible EtherCAT MainDevice. The steps to test the SubDevice with TwinCAT are present in EtherCAT SubDevice Setup with TwinCAT.
- Attention
- If you need to reload and run the example again, EVM power-cycle is MUST.
Sample Output
Shown below is a sample output when the application is run:
EtherCAT Device
EtherCAT Sample application
Revision/Type : x0590 Build : x04FD
Firmware Version : 5.4.253
SYNC0 task started
SYNC1 task started
See Also
EtherCAT SubDevice FWHAL