This page lists all the examples related to position sense.
- BISS-C Diagnostic
- EnDat Diagnostic
- EnDAT3 Diagnostic
- NIKON Diagnostic
- Tamagawa Diagnostic
- Tamagawa over UART Example
Encoder Examples Debug Guide
This section provides a debugging guide for troubleshooting issues that may arise during testing or development.
Encoder Register Configuration
The ICSSM_PR1_CFG_SLV registers from offset 0xE0 to 0x11C are allocated for encoder configuration. To review and verify the encoder settings:
- Halt the Arm® Cortex®-R5F core
- Open the memory browser window
- Enter the address of the ICSSM_PR1_CFG_SLV register and view the configured values
Note: Ensure you are entering the correct base address for encoder registers. Each ICSS instance has a different address for the CFG register.
For detailed register descriptions, refer to: Table 4-415 of the AM263x Sitara Processors Technical Reference Manual Register Addendum
Key registers and their configurations:
- ICSS_PRU0_ED_RX_CFG_REG
- Division factor for Rx clock
- RX clock source
- Polarity of the RX Start Bit
- RX Over Sample size
- ICSS_PRU0_ED_TX_CFG_REG
- Division factor for Tx clock
- Load share mode configuration
- TX clock source
- ICSS_PRU0_ED_CH0_CFG0_REG
- RX frame size
- TX frame size
- TX wire delay configuration
- ICSS_PRU0_ED_CH0_CFG1_REG
- Rx arm counter value if Rx auto arm is enabled
- TST delay
- ICSS_GPCFG0_REG
- Controls the ICSS wrap mux select (should be in EnDAT mode)
PRU-ICSS 3 channel register view
Hardware Setup and Pin Configuration
The RS485 interface card, control card, and encoder should be connected to the correct PRU GPIO pins mapped for the Encoder interface Peripheral IF mode. All associated pins must be selected in SysConfig.
LP-AM263P + BP-AM2BLDCSERVO Booster Pack Pin Multiplexing for SDK example
| Pin name | Jumper number | Function |
| PR0_PRU0_GPIO3 | J2.19 | Channel 1 clock |
| PR0_PRU0_GPO4 | J2.17 | Channel 1 transmit |
| PR0_PRU0_GPO5 | J2.13 | Channel 1 transmit enable |
| PR0_PRU0_GPI10 | J1.8 | Channel 1 receive |
| GPIO Pin (SDFM0_D1/D13) | J8.73 | Enable encoder voltage in Axis 1 of BP (Fix this pin to high with SoC GPIO mode) |
PRU Firmware Debug
For PRU-related issues, verify that the application is loading the PRU firmware into the correct PRU core. If firmware loading fails:
- Check the PRU core selection
- Verify the PRU slice selection
- Review application-level configuration
Debugging Steps for PRU Core with Loaded Firmware:
- Import the PRU firmware for the target core
- Build the firmware
- Open the debug window and connect to the PRU core
- Load symbols into the connected core:
- Click the Load button
- Select
Load Symbols
- Load the firmware .out file from the firmware project
- After symbols are loaded, use the step-into button to execute debug commands
Load EnDAT RTU firmware symbols
Multi-channel modes
Multi-channel with single PRU mode
- Note
- This subsection is applicable for BiSS-C, EnDat, Nikon A-format, and Tamagawa only.
- Data transmission and reception must happen simultaneously on all channels.
- The encoder configuration and cable length should be the same on all channels.
- If encoders across channels don't respond at the same time, this mode will not work. Load share configuration should be used instead.
Multi-channel with load share mode
- Note
- This subsection is not applicable for EnDAT3.
- Data transmission and reception can happen independently on all channels.
- After a command is sent, all channels wait for a response and process the response independently. However, all channels must finish processing before the next command can be triggered. (This restriction does not apply to HDSL. HDSL channels can continue operating independently.)
Periodic Trigger Mode
- Note
- This subsection is not applicable for HDSL.
SDK examples uses IEP compare/capture event(s) to trigger commands in periodic mode. Firmware triggers a R5F interrupt after getting a response from the encoder. The application code uses a callback function to clear the PRU interrupt, which can be modified as per the use case. CMP/CAP event number can be configured using SysConfig module of encoder. Refer the example specific page for details (see Periodic Trigger Modes).
When programming the values for periodic trigger CMP/CAP mode, ensure that the command send and receive can complete within the cycle time. In multi-channel, ensure that command completion for timings for all channels are considered. Incorrect values may send PRU FW in bad state. Also, refer to encoder specifications to ensure that requirement for mimimum interval between two commands is met.
IEP Registers Configuration
The Industrial Ethernet Peripheral (IEP) is used for periodic trigger mode. If the IEP is not configured correctly, periodic trigger mode will not work.
To verify IEP configuration:
- Check if the IEP is running by examining
IEP_COUNT_REG0/1 registers
- Verify counter increment by monitoring count values
- Review
IEP_CMP_CFG_REG to ensure all compare events are properly configured for trigger mode
- Check
IEP_CMP_STATUS_REG to verify that corresponding compare events are setting status flags correctly
- Validate that Compare Registers are configured with correct trigger point values
Note: Ensure you are entering the correct address for IEP registers. Each ICSS instance has a different base address for the IEP registers.
PRU-ICSS IEP register view
PRU-ICSS IEP CMP events register view
For detailed register descriptions, refer to: Table 4-417 of the AM263x Sitara Processors Technical Reference Manual Register Addendum
Interrupt Controller Internal Signals Mapping
If you experience missing PRU interrupts or incorrect IRQ mapping, verify the interrupt mapping between PRU and R5F.
- The host interrupt numbers defined in "*_periodic_trigger.c" file(s) in SDK examples (e.g., ICSS_PRU_ENDAT_INT_NUM) must match the interrupt channel assignments in SysConfig PRU(ICSS) module -> INTC section -> INTC Host Interrupt
- Host interrupt channels route PRU events to the R5F core
- Mapping: Host Interrupt 2-9 in SysConfig = HOST_INTR_PEND_0-7 registers
- If the host interrupt assignments are changed in SysConfig, macros in "*_periodic_trigger.c" file(s) need to be updated accordingly to maintain proper interrupt delivery from PRU to R5F.
- The INTC event numbers defined "*_periodic_trigger.c" file(s) must match the corresponding definitions in the PRU firmware header file (e.g., "source/position_sense/endat/firmware/endat_icss_reg_defs.h")
- These event numbers are used for communication between the R5F and PRU firmware. Any changes to these values must be synchronized between both files (firmware and application) to ensure proper interrupt handling.
For example, the EnDAT single channel example uses:
- PRU Event:
18: pr0_pru_mst_intr[2]_intr_req
- Channel: 2
- Host Interrupt: 2
PRU-ICSS INTC view
The interrupt service routine (ISR) configuration is implemented in endat_periodic_trigger.c. Here's a key code snippet showing the configuration:
HwiP_Params_init(&hwi_params);
hwi_params.intNum = ICSS_PRU_ENDAT_INT_NUM;
hwi_params.callback = &endat_pru_irq_handler;
hwi_params.args = pruicss_handle;
hwi_params.isPulse = FALSE;
hwi_params.isFIQ = FALSE;
status = HwiP_construct(&gEndatHwiObject[CONFIG_ENDAT0][0], &hwi_params);
DebugP_assert(status == SystemP_SUCCESS);
void endat_pru_irq_handler(void *pruicss_handle)
{
if(pruicss_handle ==
NULL)
{
return;
}
#if(CONFIG_ENDAT0_MODE == ENDAT_MODE_MULTI_CHANNEL_MULTI_PRU)
gPruEndatIrqCnt[CONFIG_ENDAT0][1]++;
#else
gPruEndatIrqCnt[CONFIG_ENDAT0][0]++;
#endif
PRUICSS_clearEvent((PRUICSS_Handle)pruicss_handle, PRU_TRIGGER_HOST_ENDAT_EVT);
}
The R5F interrupt number "ICSS_PRU_ENDAT_INT_NUM" and PRU event number "PRU_TRIGGER_HOST_ENDAT_EVT" and is defined in endat_periodic_trigger.h.
- Note
- Arm is a registered trademark of Arm Limited (or its subsidiaries or affiliates) in the US and/or elsewhere.