BISS-C diagnostic application does the following:
This application is controlled with a terminal interface using a serial over USB connection between the PC host and the EVM. Please connect a USB cable between the PC and the EVM/LP. A serial terminal application (like teraterm/ hyperterminal/ minicom) is then run on the host. To configure, select the serial port corresponding to the port emulated over USB by the EVM. The host serial port should be configured to 115200 baud, no parity, 1 stop bit and no flow control.
The BISS-C receiver firmware running on ICSS0-PRU1 provides a defined interface. The BISS-C diagnostic application interacts with the BISS-C receiver firmware interface. It then presents the user with menu options to select Data ID code. The application collects the data entered by the user and configures the relevant interface. Then via the BISS-C receiver interface, the command is triggered. Once the command completion is indicated by the interface, the status of the transaction is checked. If the Status indicates success, the result is presented to the user.
Folder/Files | Description |
---|---|
${SDK_INSTALL_PATH}/examples/position_sense/bissc_diagnostic | |
bissc_diagnostic.c | BISS-C diagnostic application |
${SDK_INSTALL_PATH}/source/position_sense/bissc | |
firmware/ | Folder containing BISS-C PRU firmware sources. |
driver/ | BISS-C diagnostic driver. |
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 freertos |
ICSSM | ICSSM |
PRU | PRU0 |
Toolchain | ti-arm-clang |
Board | am263px-lp (Single channel example) |
Example folder | examples/position_sense/bissc_diagnostic |
Designator | ON/OFF | Description |
---|---|---|
J13 | ON | 3V3 Supply to Booster Pack |
J14 | ON | 5V0 Supply to Booster Pack |
Designator | ON/OFF | Description |
---|---|---|
J11 | OFF | VSENSE/ISENSE select |
J13 | OFF | VSENSE/ISENSE select |
J17 | Pin 1-2 Connected | SDFM Clock Feedback Select |
J18/J19 | J19 installed: sets VSENSOR1 to 5.0V | Axis 1: Encoder/Resolver Voltage Select |
J20/J21 | J21 installed: sets VSENSOR2 to 5.0V | Axis 2: Encoder/Resolver Voltage Select |
J22 | OFF | Axis 1: Manchester Encoding Select |
J23 | OFF | Axis 2: Manchester Encoding Select |
J24 | OFF | Axis 1: RS485/DSL MUX |
J25 | OFF | Axis 2: RS485/DSL MUX |
J26 | OFF | VSENSE/ISENSE Select |
J27 | OFF | Encoder and SDFM Paths Select |
J28 | ON | AM243/AM263 Mode |
Shown below is a sample output when the application is run:
Shown below is a sample output to enable safety and the safety encoder results:
# | Name | Description | Pass/fail Criteria |
---|---|---|---|
1 | Data readout (absolute position data) | In this command we will receive: Absolute rotor position value, errors, and warnings | CRC success with ABS, E, W and CRC values printed in the terminal. |
2 | Control Communication | In this command we will receive: Absolute rotor position value, errors, and warnings, along with the result of the control communication command. | CRC success with ABS position value, E, W and CRC values of position data along with the control communication result printed in the terminal. |
3 | Start periodic continuous mode | In this command we will receive: Absolute rotor position value, errors, and warnings periodically. Rotate the rotor of motor and see the changes in Position value on UART. | 0 CRC errors with ABS position value, E, W and CRC values printed in the terminal. |
4 | Enable safety mode | In this command we will enable Safety mode by using control communication: | Safety should be enabled and CRC and Sign of Life counters will displayed from next position data request |