AM263Px Motor Control SDK  10.00.00
BISS-C Protocol Design

Introduction

This design implements BISS-C Receiver (a.k.a subsequent electronics) using the 3 channel peripheral interface available on the TI Sitara™ AM64x/AM243x/AM26x SoCs. The 3 channel peripheral interface is a digital bidirectional serial interface for position encoders, also suited for safety related applications. Only four signal lines are required, differential pair each for clock and data. In BISS-C, clock is provided by receiver and data is provided by the encoder. Data is transmitted in synchronism with clock. Transfer between receiver and encoder at the physical layer is in accordance with RS485, with transceiver at both ends.

System Overview

Position feedback system consists of a position encoder attached to a motor, up to 100 meter of cable which provides power and serial communication and the receiver interface for position encoder. In case of Sitara™ processor the receiver interface for position encoder is just one function of a connected drive controller. The Sitara™ processor provides in addition to the resources for Industrial Ethernet and motor control application including on-chip ADCs, Delta Sigma demodulator for current measurement. BISS-C Receiver on processor uses one ICSSx Slice. Clock, data transmit, data receive and receive enable signals from PRU of ICSS is available in Sitara™ processor.

Implementation

The BISS-C receiver function is implemented on TI Sitara™ Devices. Design is split into three parts – 3 channel peripheral interface support in PRU, firmware running in PRU and driver running in ARM. Application is supposed to use the BISS-C driver APIs to leverage 3 channel peripheral interface functionality.

SDK examples used the BISS-C hardware capability in PRU0 of PRU-ICSSM.

Remaining PRUs are available for Industrial Ethernet communication and/or motor control interfaces.

Specifications

Parameter Value Details
Maximum Cable Length 100m Supports up-to 10MHz with delay compensation
Maximum Frequency 10 MHz Supports up-to 100m cable.
Startup/Initialization Frequency 1 MHz After power on or reset
Frequencies supported Upto 10 MHz Changeable at run-time
CRC 6/4 bits Position-data/control-data verification
Receive oversample ratio 1x to 8x Tested with 4x,6x & 8x(Frequency specific)

3 Channel Peripheral Interface PRU hardware interface

Refer TRM for details

BISS-C Firmware Implementation

Following section describes the firmware implementation of BISS-C receiver on PRU-ICSS. Deterministic behavior of the 32 bit RISC core running upto 200 MHz provides resolution on sampling external signals and generating external signals. It makes uses of 3 channel peripheral interface support in PRU for data transmission.

The PRU-ICSS firmware supports following configuration.

  1. Single Channel

Implementation for Single Channel

Single core of PRU-ICSS slice is used in this configuration.

ARM, PRU, BISS-C module Integration for Single Channel

Firmware Architecture

Overall Block Diagram

Firmware first detects and estimates the processing delay of the encoder as part of the initialization. Then it waits for the user to provide command (user after setting up the command, user sets command trigger bit), upon detecting trigger, first it checks whether the clock frequency has changed and if yes, it re-estimates the processing delay for the new clock frequency.

Then it reads the position data and check if a control communication is in process. It verifies the position data CRC by comparing it with the on-the-fly computation of CRC. In case of control communication mode, it backs up the CDS bit and transmits the CDM bit by overriding the clock pulse during the BISS-C cycle timeout phase. If the control communication is in progress it goes back to read the position data for the next cycle. If the control communication is completed, it updates the control command status, position data status and returns to wait for the next trigger command from ARM.

In case of Safety mode enabled, firmware will be executed as explained below:

RX flow when Safety is enabled

Firmware will perform configuration as usually and then before entering into RX it checks whether safety is enabled for that particular encoder or not. If enabled, firmware will perform receive and downsample and CRC computation is excluded, after all the encoders data bits are read successfully, before going into timeout firmware will perform post processing to compute the 16 bit CRC for safety enabled encoders. Please note that Post processing will be applicable only for the encoders which we have enabled safety using control communication. Please find below is the image explains CPW and SPW as per BiSSC safety specifications.

BiSS Frame according to the BiSS Safety profile

Above image is taken from BiSS Safety Concept Document.

Note
BiSS safety is implemented by assuming 2 encoders connected in Daisy chain, one will send CPW and another one will send SPW. CRC errors are expected while enabling Safety using control communication. Because control communication will need multiple BiSS cycles to confirm and the safety may be enabled in the encoder before control communication is completed and encoder may send 16-bit CRC in some of the BiSS cycles.
Firmware running on PRU-ICSS will be remain HALTED if encoder is not detected and application will wait for 5 seconds and exit with error code.

Initialization

Initialization for All Modes

Initialization is performed both on the ARM and PRU as shown in the figure above. During the initialization, based on the clock frequency selected the PRU detects the Encoder and estimates its processing delay in terms of clock cycles. The processing delay is measured 8 times and an average value is used for compensation. Note that whenever the user changes the clock frequency, the initialization routine on the PRU is executed to estimate the processing delay.

If using "Multi Channel with Encoders of Different Make" configuration where load share mode is enabled, one of the cores among enabled cores will be set as the primary core for performing global configurations of PRU-ICSS's BISS-C interface. These global configurations include clock frequency configuration and TX global re-initialization.

There needs to be a synchronization between PRUs before changing any global configuration. For this purpose, each active PRU core sets synchronization bit before any operation needing synchronization and clears the synchronization bit when it is ready. The assigned primary core will wait for all active channel's synchronization bits to be cleared and then perform the global configuration.

Receive Position Data

BISS-C main loop for Position Data

Once the firmware receives the trigger from ARM, it will first calculate the RX frame size and check if there is a change in the clock frequency from the previous run. If yes, it will recalculate the processing delay of the encoder for the given clock frequency.

Next, it will start the clock signal to wait for the acknowledgement bit followed by the start bit. If the program is in control mode, it will back up the CDS bit for subsequent processing. Next it will read the position data bits, error and warning bits while computing the CRC on the fly. Finally, it will read the 6-bit CRC. If the program is in control mode, it will override the clock signal to transmit the CDM bit to the encoder.

The program will then wait for the timeout period and verify CRC of the position data bits. If the program is in control mode, it will check if the control command cycle is completed. If yes, it will update the results and the status bits before returning to the starting point.

Control Communication

BISS-C control communication loop

BISS-c control communication is performed over multiple cycles. Refer to the standard for more details on control communication. The firmware expects a control command as a 16-bit hex value. Once a control communication is started, the program will first transmit 14 0's as CDM bit during the timeout period at the end of the BISS-C cycle. This is then followed by a start bit to indicate to the encoder that control communication is in progress. The figure shown above explains the flow for a register read access. The register write access and control commands follows similar steps. Example commands for the register read access is given in the table below.

BISS-C hex commands

Post Processing for 16-bit Safety CRC

BISS-C Safety Post Processing for 16-bit Safety CRC

In case if safety is enabled we will only perform receive and downsample for the RX bits and CRC computation will be performed during timeout in the Postprocessing section. We will loop for all encoders across channels and perform 16-bit CRC computation using XOR based approach with the provided polynomial from the BiSS specifications. The 16 bit CRC is computed and compared with the received CRC and the error statistics are updated.

Continuous mode
Continuous Mode

BiSS-C receiver application has the support for continuous mode in which periodically clock is supplied to encoder and its position data is read and computed the CRC. User can stop continuous mode by hitting any key in UART console. Input cycle time should be greater than or equal to the BiSS cycle time considering position data bits, E, W, CRC and timeout.

3 Channel Peripheral Interface

The physical data transmission in 3 channel peripheral interface is done using RS-485 standard. The data is transmitted as differential signals using the RS485 between the 3 channel peripheral interface Receiver and the Encoder.

The Receiver sends the clock to the BISS-C encoder, data transmission in either direction (one at a time) occurs in synchronism with the clock. The design uses two differential signals for each of the lines (clock and data).

BISS-C Receiver and the encoder is connected using the RS-485 transceiver. Data is transmitted differentially over RS-485. It has the advantages of high noise immunity and long distance transmission capabilities.

Pin Multiplexing

Note
  • k = 0,1 (PRU-ICSS Instance) for AM243x/AM261x/AM64x and k = 0 for AM263x/AM263Px
  • n = 0,1 (PRU-ICSS Slice)
Pin name Signal name Function
PR<k>_PRU<n>_GPO0 pru<n>_bissc0_clk Channel 0 clock
PR<k>_PRU<n>_GPO1 pru<n>_bissc0_out Channel 0 transmit
PR<k>_PRU<n>_GPO2 pru<n>_bissc0_outen Channel 0 transmit disable
PR<k>_PRU<n>_GPI9 pru<n>_bissc0_in Channel 0 receive
PR<k>_PRU<n>_GPO3 pru<n>_bissc1_clk Channel 1 clock
PR<k>_PRU<n>_GPO4 pru<n>_bissc1_out Channel 1 transmit
PR<k>_PRU<n>_GPO5 pru<n>_bissc1_outen Channel 1 transmit disable
PR<k>_PRU<n>_GPI10 pru<n>_bissc1_in Channel 1 receive
PR<k>_PRU<n>_GPO6 pru<n>_bissc2_clk Channel 2 clock
PR<k>_PRU<n>_GPO7 pru<n>_bissc2_out Channel 2 transmit
PR<k>_PRU<n>_GPO8 pru<n>_bissc2_outen Channel 2 transmit disable
PR<k>_PRU<n>_GPI11 pru<n>_bissc2_in Channel 2 receive

LP-AM263P Booster Pack Pin Multiplexing

Pin name Signal name Function
PR0_PRU0_GPIO3 pru1_endat1_clk Channel 1 clock
PR0_PRU0_GPO4 pru1_endat1_out Channel 1 transmit
PR0_PRU0_GPO5 pru1_endat1_outen Channel 1 transmit enable
PR0_PRU0_GPI10 pru1_endat1_in Channel 1 receive
SDFM0_D1 Pin (J8.73) ENC1_EN Enable 3 channel peripheral interface in Axis 1 of BP (D13 GPIO pin)