|
AM261x INDUSTRIAL COMMUNICATIONS SDK
10.02.00
|
|
Go to the documentation of this file.
50 #include <kernel/dpl/HwiP.h>
60 typedef struct PN_IntAttrs_s
83 typedef struct PN_IntConfig_s
uint32_t intPrio
Definition: PN_Handle.h:70
Definition: PN_Handle.h:84
void * callBackPtr
Definition: PN_Handle.h:76
void * isrFnPtr
Definition: PN_Handle.h:74
struct PN_Config_s * PN_Handle
Alias for Profinet Handle containing base addresses and modules.
Definition: PN_Handle.h:98
uint32_t coreIntNum
Definition: PN_Handle.h:66
uint32_t pruIntNum
Definition: PN_Handle.h:64
uint32_t socEvId
Definition: PN_Handle.h:68
void * args
Definition: PN_Handle.h:72
PN_IntAttrs ptcpIntConfig
Definition: PN_Handle.h:92
Definition: PN_Handle.h:61
PN_IntAttrs dhtIntConfig
Definition: PN_Handle.h:90
PN_IntAttrs cpmIntConfig
Definition: PN_Handle.h:88
PN_IntAttrs ppmIntConfig
Definition: PN_Handle.h:86
HwiP_Object interruptObject
Definition: PN_Handle.h:62