|
AM261x Motor Control SDK
10.02.00
|
|
Go to the documentation of this file.
53 #include "math_types.h"
74 typedef struct _USER_Params_
77 int_least16_t numIsrTicksPerCtrlTick;
99 uint_least8_t numVoltageSensors;
120 uint16_t motor_numEncSlots;
257 bool flag_bypassMotorId;
301 #endif // end of USERPARAMS_H definition
float32_t RoverLPole_rps
Definition: userParams.h:268
float32_t Dir_fe_max_Hz
Definition: userParams.h:278
int_least16_t numCtrlTicksPerCurrentTick
Definition: userParams.h:90
float32_t oneOverFlux_min_sf
Definition: userParams.h:275
float32_t Dir_fe_min_Hz
Definition: userParams.h:277
int_least16_t numIsrTicksPerEstTick
Definition: userParams.h:82
float32_t freqNearZeroSpeedLimit_Hz
Definition: userParams.h:264
float32_t estKappa
Definition: userParams.h:269
Defines a structure for the user parameters.
Definition: userParams.h:75
uint16_t motor_numPolePairs
for the motor
Definition: userParams.h:119
int_least16_t numCtrlTicksPerSpeedTick
Definition: userParams.h:94
MotorNum_e
Enumeration for the Motor numbers.
Definition: userParams.h:63
float32_t flux_max_Wb
Definition: userParams.h:273
int_least16_t numIsrTicksPerTrajTick
Definition: userParams.h:86
MOTOR_Type_e
Enumeration for the motor types.
Definition: motor.h:67
Contains motor-specific enum and structs.
uint_least8_t numCurrentSensors
Definition: userParams.h:98
@ MTR_1
Definition: userParams.h:64
float32_t oneOverFlux_max_sf
Definition: userParams.h:276
@ MTR_3
Definition: userParams.h:66
@ MTR_2
Definition: userParams.h:65
float32_t directionPole_2_rps
Definition: userParams.h:266
float32_t flux_Wb
Definition: userParams.h:271
float32_t flux_min_Wb
Definition: userParams.h:272
float32_t fluxPole_rps
Definition: userParams.h:267
float32_t indEst_speedMaxFraction
Definition: userParams.h:181
float32_t directionPole_rps
Definition: userParams.h:265
float float32_t
Definition: dcl_common.h:58
float32_t dcBus_nominal_V
voltage, V
Definition: userParams.h:76
float32_t maxFrequency_Hz
Definition: userParams.h:281