AM261x Motor Control SDK  10.02.00
Introduction

Welcome to Motor Control SDK for AM261X. This SDK contains examples, libraries and tools to develop RTOS and no-RTOS based applications enabling real-time communication for position sense from motors for ARM R5F CPU and related peripherals.

Attention
This SDK also includes AM261X Industrial Communications SDK and AM261X MCU+ SDK.

Getting Started

To get started, see GETTING STARTED page.

Note
  • Motor Control SDK version 10.02.00 supports LP-AM261 Rev. E2 only. The upcoming LP-AM261 board revision will feature integrated DP83869 Ethernet PHYs onboard, replacing the DP83826E daughter card approach used in LP-AM261 Rev. E2.
  • To build examples from Industrial Communications SDK and MCU+ SDK using CCS projects, user has to add ${SDK_INSTALL_PATH}/ind_comms_sdk path and ${SDK_INSTALL_PATH}/mcu_plus_sdk path to "Product discovery path" respectively in CCS (from Window->Preferences->Code Composer Studio->Products)
  • In order to build the Networking examples from MCU+ SDK using CCS projects, the user needs to change the file action of the source files from "link" to "copy" in the example.projectspec and then import their project in CCS.

Block Diagram

Given below is a block diagram of the SW modules in this SDK

Software Block Diagram

The main software components in the block diagram specific to motor control are described below

Software Components Documentation Page Description
Position Sense Encoders
BISS-C BISS-C Driver and PRU-ICSS firmware for BISS-C encoder interface
EnDat EnDat Driver and PRU-ICSS firmware for EnDat encoder interface
HDSL HDSL Driver and PRU-ICSS firmware for Hiperface DSL encoder interface
Nikon A-format Nikon A-format Driver and PRU-ICSS firmware for Nikon A-format encoder interface
Tamagawa Tamagawa Driver and PRU-ICSS firmware for Tamagawa encoder interface
Real Time Libraries
Control algorithms Control algorithms Library for control algorithms and techniques used in motors such as PMSM and BLDC
Datalog Datalog Library for storing the real time values of user selectable variables
Digital Control Library (DCL) Digital Control Library (DCL) Header-only library for digital control applications
Observer algorithms Observer algorithms Header-only library for encoder/observer algorithms used in both sensored/sensorless field oriented control (FOC)
Software Frequency Response Analyzer Software Frequency Response Analyzer Library that enables developers to quickly measure the frequency response of their digital power converter.
Transforms Transformation Algorithm Transformation including Clarke, Park, Space Vector Generation used in motor control applications.
Examples and Demos
Examples and Demos Examples and Demos Examples and demos showing usage of different SW libraries and APIs for motor control

For details on software components of Industrial Communications SDK and MCU+ SDK, please refer to AM261X Industrial Communications SDK and AM261X MCU+ SDK respectively.

Directory Structure

Given below is a overview of the directory structure to help you navigate the SDK and related tools.

Folder/Files Description
${SDK_INSTALL_PATH}/
README_FIRST_AM261X.html Open this file in a web browser to reach this user guide
makefile Top level makefile to build the whole SDK using "make"
imports.mak Top level makefile to list paths to dependent tools
docs/ Offline browseable HTML documentation
examples/ Example applications for AM261X, across multiple boards
source/ Device drivers, middleware libraries and APIs
ind_comms_sdk/ Industrial Communications SDK
mcu_plus_sdk/ MCU+ SDK

Given below are the paths where the different tools needed outside the SDK, like CCS, SysConfig are installed by default in Windows. In Linux, the tools are installed by default in ${HOME}/ti.

Folder/Files Description
C:/ti/ccs1281 Code Composer Studio
C:/ti/sysconfig_1.23.0 SysConfig. NOTE, SysConfig is also installed as part of CCS at ${CCS_INSTALL_PATH}/ccs/utils/sysconfig_x.x.x
C:/ti/ti-cgt-armllvm_4.0.1.LTS TI ARM CLANG compiler tool chain

Licenses

The licensing information of this SDK, as well as any third-party components included which are made available under a number of other open-source licenses are enumerated as part of the manifest. A complete manifest along with export control information is detailed here [LINK] and the SDK Software License Agreement (SLA) is here [LINK]

Help and Support

For additional help and support, see https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum

Documentation Credits

This user guide is generated using doxygen, v1.8.20. See https://www.doxygen.nl/index.html