AM243x Motor Control SDK  11.00.00
DCL PI Test

Simple DCL PI controller demonstration

This example leverages a PI controller from the digital control library (DCL). It demonstrates how to set up and run the PI controller. The example first initializes the datalog DCL_FDLOG to the test vector, runs the controller based on the test input and compares the output with the expected value.

Files and directory structure

Folder/Files Description
${SDK_INSTALL_PATH}/examples/rtlibs/dcl/dcl_pi/
pi_test.c Main function for PI testing
pi_test.h Contains all initialization of needed structures
data/ Contains pre-generated data files result compares with
${SDK_INSTALL_PATH}/source/rtlibs/dcl
dcl/ Folder containing DCL library source

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss0-0 freertos
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp
Example folder examples/rtlibs/dcl/dcl_pi

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run:

PI test produced 0 error