AM243x Motor Control SDK  2025.00.00
PRU-ICSSG Input/Output Modes

PRU-ICSSG overview

One PRU-ICSSG is divided into two slices (Slice 0 and Slice 1), each having 2 programmable real-time unit (PRU) cores; namely Programmable Real-time Units (PRU0/PRU1), Real-Time Units (RTU_PRU0/RTU_PRU1), and Transmit Programmable Real-Time Units (TX_PRU0/TX_PRU1). In total, there are 6 cores.

PRU-ICSSG Block Diagram

For more details on PRU-ICSSG, please see section "6.4 Programmable Real-Time Unit and Industrial Communication Subsystem - Gigabit (PRU_ICSSG)" of AM243x Technical Reference Manual.

Input/Output modes

Each PRU-ICSSG slice has 20 PRU GPIO pins, which are multiplexed with other functional signals at the device level. There is also an internal wrapper multiplexing that expands the device top-level multiplexing. This wrapper multiplexing is controlled by the GPCFGx_REG register (where x = 0 or 1 for slice) in the PRU-ICSSG CFG register space and allows direct GPIO, MII_RT, 3-channel Peripheral Interface, and Sigma Delta functionality to be muxed with the PRU GPIO device signals, as shown in the figure below. Note that the device top-level muxing has higher priority over the internal muxing. For more details, please see section "6.4.2.1 PRU_ICSSG Internal Pinmux" of AM243x Technical Reference Manual.

PRU-ICSSG Pin Modes

The following are different input/output modes based on different values of the GPCFGx_REG register:

  1. GPIO mode (0)
    • PRU EGPIs Direct Input
    • PRU EGPIs 16-Bit Parallel Capture
    • PRU EGPIs 28-Bit Shift In
    • PRU EGPOs Direct Output
    • PRU EGPO Shift Out
  2. Peripheral IF mode (1)
    • Three-Channel Peripheral Interface used for absolute encoder interfaces like BiSS-C, EnDat, Hiperface DSL, Nikon A-format, Tamagawa, custom UART, etc.
  3. MII mode (2)
    • MII/RGMII mode used for industrial communication protocol and standard ethernet
  4. SD mode (3)
    • Sigma Delta (SD) Decimation Filtering used for current sense interface
Attention
Pin mode selection is done per PRU-ICSSG slice. If Peripheral IF mode is selected for a slice, all pins from that slice are selected for Peripheral IF mode and cannot be used for other modes like GPIO or SD or MII.
Note
  • Some devices may not pin out all 29 bits of R31 and all 32 bits of R30. For which pins are available on a specific device, see the device-specific datasheet for device pin mapping.
  • PRUs have full input and output control in all modes
  • RTU_PRUs and TX_PRUs see R31 input and can process received pin data in parallel
  • A special PRU/RTU_PRU/TX_PRU load sharing option for Peripheral IF mode and SD mode is available

For more details, please see section "6.4.5.2.2.3 General-Purpose Inputs (R31): Enhanced PRU GP Module" of AM243x Technical Reference Manual.

Load Share Mode

In load share mode, PRU GPIO pins are divided among PRU/RTU_PRU/TX_PRU cores. This is available for Peripheral IF mode and SD mode only.

PRU-ICSSG Load Share Mode

The following sections contain a brief overview of different modes.

GPIO mode

Note
  • Some devices may not pin out all 29 bits of R31 and all 32 bits of R30. For which pins are available on a specific device, see the device-specific datasheet for device pin mapping.

PRU EGPIs Direct Input

PRU R31 (EGPI) Direct Input Mode
  • PRU GPI[19:0] pin data feeds directly into the PRU R31[19:0] bits.

PRU EGPIs 16-Bit Parallel Capture

PRU R31 (EGPI) 16-Bit Parallel Capture Mode
  • DATAIN[0:15] is captured by the positive edge or negative edge of CLOCKIN.
  • CLOCKIN edge is selected by the ICSSG_GPCFGx_REG register.

PRU EGPIs 28-Bit Shift In

PRU R31 (EGPI) 28-Bit Shift Mode
  • DATAIN is sampled and shifted into a 28-bit shift register.
  • Shift Counter (Cnt_16) feature is mapped to pru<n>_r31_status[28]. Cnt_16 is self-clearing and is connected to the PRU Interrupt Controller (INTC).
  • SB (Start Bit detection) feature is mapped to pru<n>_r31_status[29]. Start Bit (SB) is cleared by the ICSSG_GPECFGx_REG register. Start Bit value (0h or 1h) is selected by the ICSSG_GPECFGx_REG register.

PRU EGPOs Direct Output

PRU R30 (EGPO) Direct Output Mode
  • PRU R30[19:0] bits feed directly to GPO[19:0].

PRU EGPO Shift Out

PRU R30 (GPO) Shift Out Mode
  • pru<n>_r30[0] is shifted out on DATAOUT on every rising edge of pru<n>_r30[1] (CLOCKOUT).
  • Free Running Clock or Fixed Clock Count Mode is selected by the ICSSG_GPECFGx_REG register.
  • This mode uses two 16-bit shadow registers (GPO_SH0 and GPO_SH1) to support ping-pong buffers.
  • LOAD_GPO_SH0 (Load Shadow Register 0) is mapped to pru<n>_r30[29]. LOAD_GPO_SH1 (Load Shadow Register 1) is mapped to pru<n>_r30[30].
  • ENABLE_SHIFT is mapped to pru<n>_r30[31].

Peripheral IF mode

Peripheral IF Mode
  • The Three-Channel Peripheral Interface is used for absolute encoder interfaces, custom UART, etc.
  • 3 channels per PRU-ICSSG slice with baud range from 100 kHz to 32 MHz (based on SoC PLL) per slice
    • Optional load sharing mode across PRU/RTU_PRU/TX_PRU cores per slice of PRU-ICSSG which enables each core to control 1 channel each
  • ICSS_UART_CLK (default) or ICSS_CORE_CLK clock is an input to independent clock dividers to produce a normal clock and an oversampling clock
  • Half-duplex (TX and RX are not supported concurrently)
  • TX/RX FIFO size of 32 bits
  • Configurable oversampling on RX
  • Optional RX frame size auto start/shut off
  • Individual TX channel start trigger or simultaneous TX start trigger for all channels
  • Optional SW direct snoop of data input
  • RX Start Bit of '1' or '0'
  • Flexible HW-assisted clock output generation to allow free running, stop high and stop low (after last RX data), or stop high (after last TX data) operation with optional software clock override feature

Signal Configuration

Pad Names at Device Level Peripheral IF Mode Example usage for 4-wire interface like EnDat 2.2 Example usage for 2-wire interface like Hiperface DSL
PRG<k>_PRU<n>_GPO0 PERIF0_CLK Channel 0 Clock -
PRG<k>_PRU<n>_GPO1 PERIF0_OUT Channel 0 Data Out Channel 0 Data Out
PRG<k>_PRU<n>_GPO2 PERIF0_OUT_EN Channel 0 Output Enable Channel 0 Output Enable
PRG<k>_PRU<n>_GPO3 PERIF1_CLK Channel 1 Clock -
PRG<k>_PRU<n>_GPO4 PERIF1_OUT Channel 1 Data Out Channel 1 Data Out
PRG<k>_PRU<n>_GPO5 PERIF1_OUT_EN Channel 1 Output Enable Channel 1 Output Enable
PRG<k>_PRU<n>_GPO6 PERIF2_CLK Channel 2 Clock -
PRG<k>_PRU<n>_GPO7 (*note 4) PERIF2_OUT Channel 2 Data Out Channel 2 Data Out
PRG<k>_PRU<n>_GPO8 PERIF2_OUT_EN Channel 2 Output Enable Channel 2 Output Enable
PRG<k>_PRU<n>_GPI9 (*note 4) PERIF0_IN Channel 0 Data In Channel 0 Data In
PRG<k>_PRU<n>_GPI10 (*note 4) PERIF1_IN Channel 1 Data In Channel 1 Data In
PRG<k>_PRU<n>_GPI11 PERIF2_IN Channel 2 Data In Channel 2 Data In
PRG<k>_PRU<n>_GPO12 (*note 3) PERIF2_OUT Channel 2 Data Out Channel 2 Data Out
PRG<k>_PRU<n>_GPI13 (*note 3) PERIF0_IN Channel 0 Data In Channel 0 Data In
PRG<k>_PRU<n>_GPI14 (*note 3) PERIF1_IN Channel 1 Data In Channel 1 Data In
Note
  1. These signals are shared with the GPIO, MII, and SD modes. To configure for Peripheral IF, PRU_ICSS_GPCFGx[29-26] PR1_PRUy_GP_MUX_SEL needs to be set to 1h.
  2. Some devices may not pin out all 29 bits of R31 and all 32 bits of R30. For which pins are available on a specific device, see the device-specific datasheet for device pin mapping.
  3. This alternate pinmux is enabled when SA mux selection register is configured (ICSSG_SA_MX_REG[7] G_MUX_EN = 1)
  4. This is the default pinmux when SA mux selection is not enabled (ICSSG_SA_MX_REG[7] G_MUX_EN = 0)

SD mode

Sigma Delta Mode
  • Sigma Delta (SD) Decimation Filtering mode is used for current sense interface.
  • Sigma Delta Filter Module (SDFM) is achieved by a combination of PRU hardware and firmware.
  • Hardware integrators perform the accumulation part of Sinc filtering and the differentiation part is done in firmware (Sinc2/Sinc3)
  • Up to 9 channels of concurrent counting per PRU slice
    • Optional load sharing mode across PRU/RTU_PRU/TX_PRU cores per slice of PRU-ICSSG which enables each core to control 3 channels each
  • Software can read all 3 stages of accumulators
  • Clock source option of per channel or one per 3 channels or one per 9 channels
  • Fast detection for overcurrent detection (via sliding window size max: 28 clocks)
  • sinc1 snoop for overcurrent detection
  • Manchester decode mode per channel removes the need for CLK
  • Synchronized conversion is possible using IEP comparator registers

The following images show the block diagram of the Sigma Delta hardware integrators and integration with the PRU R30 / R31 interface for a single channel. The three accumulators (acc1-acc3) for each channel are simple 28-bit adders. The input for acc1 is 1-bit, while the inputs for acc2 and acc3 are 28-bits. On each positive edge of CLK_OUT, all three 28-bit counters (acc1-acc3) increment.

Sigma Delta Hardware Integrators Block Diagram (snoop = 0)
Sigma Delta Hardware Integrators Block Diagram (snoop = 1)

Signal Configuration

Pad Names at Device Level Sigma Delta (SD) Mode Function
PRG<k>_PRU<n>_GPI0 SD0_CLK SD demodulator clock channel 0 or
SD demodulator clock for channels 0, 1 and 2
PRG<k>_PRU<n>_GPI1 SD0_D SD demodulator data channel 0 or
generate SD_CLKOUT clock (*note 4)
PRG<k>_PRU<n>_GPI2 SD1_CLK SD demodulator clock channel 1
PRG<k>_PRU<n>_GPI3 SD1_D SD demodulator data channel 1
PRG<k>_PRU<n>_GPI4 SD2_CLK SD demodulator clock channel 2
PRG<k>_PRU<n>_GPI5 SD2_D SD demodulator data channel 2
PRG<k>_PRU<n>_GPI6 SD3_CLK SD demodulator clock channel 3 or
SD demodulator clock for channels 3, 4 and 5
PRG<k>_PRU<n>_GPI7 SD3_D SD demodulator data channel 3
PRG<k>_PRU<n>_GPI8 SD4_CLK SD demodulator clock channel 4
PRG<k>_PRU<n>_GPI9 (*note 5) SD4_D SD demodulator data channel 4
PRG<k>_PRU<n>_GPI10 (*note 5) SD5_CLK SD demodulator clock channel 5
PRG<k>_PRU<n>_GPI11 SD5_D SD demodulator data channel 5
PRG<k>_PRU<n>_GPI12 SD6_CLK SD demodulator clock channel 6 or
SD demodulator clock for channels 6, 7 and 8
PRG<k>_PRU<n>_GPI13 SD6_D SD demodulator data channel 6
PRG<k>_PRU<n>_GPI14 SD7_CLK SD demodulator clock channel 7
PRG<k>_PRU<n>_GPI15 SD7_D SD demodulator data channel 7
PRG<k>_PRU<n>_GPI16 SD8_CLK SD demodulator clock channel 8 or
SD demodulator clock for channels 0 to 8
PRG<k>_PRU<n>_GPI17 SD8_D SD demodulator data channel 8
PRG<k>_PRU<n>_GPI18 (*note 3) SD4_D SD demodulator data channel 4
PRG<k>_PRU<n>_GPI19 (*note 3) SD5_CLK SD demodulator clock channel 5
Note
  1. These signals are shared with the GPIO, MII, and Peripheral IF modes. To configure for SD, ICSSG_GPCFGx_REG[29-26] PR1_PRUy_GP_MUX_SEL needs to be set to 3h.
  2. Some devices may not pin out all 29 bits of R31 and all 32 bits of R30. For which pins are available on a specific device, see the device-specific datasheet for device pin mapping.
  3. This alternate pinmux is only available when SA mux selection register is configured (ICSSG_SA_MX_REG[7] G_MUX_EN = 1)
  4. The PRG<k>_PRU0_GPI1 signal (muxed with SD0_D) can be used as SD_CLKOUT when PRU_ICSSG generates the clock. This is a trade-off as the PRU application will lose one SD channel. SD_CLKOUT needs to go through a clock generator chip if driving multiple sigma delta modulators and also be looped back into PRU_ICSSG as SD_CLKIN, typically pru_gpi16. For more details, please see section "6.4.5.2.2.3.5.1 Sigma Delta Block Diagram and Signals" of AM243x Technical Reference Manual.
  5. This is the default pinmux when SA mux selection is not enabled (ICSSG_SA_MX_REG[7] G_MUX_EN = 0)