EtherCAT Slave
 
Loading...
Searching...
No Matches
CiA 402 Example

Scope

This example covers how to enable the CiA 402 device profile.

Related Files

ecSlvCiA402.c
ecSlvCiA402.h
ESL_cia402Demo.c
ESL_cia402Demo.h
ESL_cia402Obd.c
ESL_cia402Obd.h
EtherCAT_Slave_CiA402.c

CiA 402 Example

This example configures a 3 axis motor control application. If the device or the ESI file (EtherCAT Slave Information) does not support the CiA 402 device profile, the subsequent registration calls should be disabled. The following functions are implemented in ESL_cia402Demo.c.

EC_SLV_APP_motionControl

Motion control is done in this function. The control of modes CSP, CSV or CST is shown.

EC_SLV_APP_cia402Application

The function contains an implementation of the CiA 402 State Machine (although an external one can be registered). This state machine works alongside the CiA 402 application. The application reads the control object (0x6040) and writes the status object (0x6041). The application activates the axis and checks if there is any error pending. If an error is pending then it calls to transition actions to resolve the error and clears the error status if required.

EC_SLV_APP_cia402LocalError

If the CiA 402 State machine changes to an error state this function is called. It is used to notify the error, not to take any action.

Basic Setup

The example starts by initializing operating system (OSAL) and hardware abstraction layers (HWAL). The EtherCAT functionality itself is implemented within the EC_SLV_APP_loopTask that is started from the main application entry point, both are implemented in EtherCAT_Slave_CiA402.c.

Hardware Setup

EC_SLV_APP_loopTask starts with the initialization of the GPIO driver and the configuration of the PHY and LED pins in the function EC_SLV_APP_initBoardFunctions in ecSlvCiA402.c.

Next PHY parameters, such as address, polarity and RX link are configured in EC_SLV_APP_registerStacklessBoardFunctions.

Program flow of the EtherCAT Slave CiA402 Example Application

Initialization of Stack, PRU, and Device Identification

Before entering the main stack loop, the example application itself is initialized in EC_SLV_APP_CIA_applicationInit. This function creates a new EtherCAT Slave device instance, registers a board status LED callback, sets vendor ID, product code and name, revision number, etc.

Program flow of the EtherCAT Slave CiA402 Example Application

After the basic initialization, EC_SLV_APP_CIA_applicationInit continues with the setup of the CiA 402 example drives and motion control example.

CiA 402 Basics

CiA402 State Machine

CiA402 State Machine or Finite State Automation (FSA) is independent to the EtherCAT State Machine (ESM) and defines internal and external behaviour for each state. The state of the drive determines which commands are accepted and whether high power is applied. States are changed when a control-word from the host-controller is received. They can also be changed due to internal events. The current state is indicated by the status-word. The control-word and different command values (e.g. velocity) are mapped into default RxPDOs (receive process data objects). The status-word and different actual values (e.g. position) are mapped into TxPDOs.

For a detailed description of the state machine transition please refer to the chapter 5.1 of the ETG6010 CiA402 implementation directive.

CiA402 State Machine

Control Word

The control object 0x6040 is used to request state changes on the CiA402 state machine. The control commands are coded by bits.

Bit Description
0 Switch on
1 Enable voltage
2 Quick Stop
3 Enable Operation
4-6 Operation mode specific
7 Fault reset

These defines are available to transition between different states.

Define Value Description
CONTROLWORD_COMMAND_SHUTDOWN 0x0006 Shutdown command
CONTROLWORD_COMMAND_SWITCHON 0x0007 Switch on command
CONTROLWORD_COMMAND_SWITCHON_ENABLEOPERATION 0x000F Switch on and enable command
CONTROLWORD_COMMAND_DISABLEVOLTAGE 0x0000 Disable voltage command
CONTROLWORD_COMMAND_QUICKSTOP 0x0002 Quickstop command
CONTROLWORD_COMMAND_DISABLEOPERATION 0x0007 Disable operation command
CONTROLWORD_COMMAND_ENABLEOPERATION 0x000F Enable operation command
CONTROLWORD_COMMAND_FAULTRESET 0x0080 Fault reset command

Status Word

The status object 0x6041 is used to get the state of the CiA402 state machine.

Bit Description
0 Ready to switch on
1 Switched on
2 Operation enabled
3 Fault
4 Voltage enabled
5 Quick Stop
6 Switch on disabled

These defines are available to interpret the FSA states.

Define Value Description
STATUSWORD_STATE_NOTREADYTOSWITCHON 0x0000 Not ready to switch on
STATUSWORD_STATE_SWITCHEDONDISABLED 0x0040 Switched on but disabled
STATUSWORD_STATE_READYTOSWITCHON 0x0021 Ready to switch on
STATUSWORD_STATE_SWITCHEDON 0x0023 Switched on
STATUSWORD_STATE_OPERATIONENABLED 0x0027 Operation enabled
STATUSWORD_STATE_QUICKSTOPACTIVE 0x0007 Quickstop active
STATUSWORD_STATE_FAULTREACTIONACTIVE 0x000F Fault reaction active
STATUSWORD_STATE_FAULT 0x0008 Fault state

Operation modes

These modes are recommended to be supported by the drives:

Operation mode Code
Profile position mode 1
Velocity mode 2
Profile velocity mode 3
Torque profile mode 4
Homing mode 6
Interpolated position mode 7
Cyclic synchronous position mode 8
Cyclic synchronous velocity mode 9
Cyclic synchronous torque mode 10
Cyclic synchronous torque mode with commutation angle 11

The operation mode object 0x6060 is used to request an operation mode.

The operation mode display object 0x6061 is used to get the current operation mode.

Position control

The target position object 0x607A is used to request the target position.

The position actual value object 0x6064 gets the drive's current position.

Velocity control

The target velocity object 0x60FF is used to request the target velocity.

The velocity actual value object 0x606C gets the drive's current velocity.

Torque control

The target torque object 0x6071 is used to request the target torque.

The torque actual value object 0x6077 gets the drive's current torque.

Request object summary

These are the objects that must be written to the drive to command a specific operation.

Index Description
0x6040 Control Word
0x6060 Operation mode
0x607A Target position
0x60FF Target velocity
0x6071 Target torque

Feedback object summary

These are the objects that must be read to get the current status of the drive.

Index Description
0x6041 Status Word
0x6061 Operation mode display
0x6064 Position actual value
0x606C Velocity actual value
0x6077 Torque actual value

Using CiA 402 Example on TwinCAT

  • The CiA402 demo simulates a three axis application. For each axis the objects described above are mapped as process data. Therefore, the first step is to scan the device and bring it to Operational state.
CiA402 runs in OP
  • Open the Drive 1, the CiA402 mapped objects can be accessed there:
CiA402 example process data
  • Go to the Modes of operation object and set the cyclic synchronous position mode (8):
Set value dialog
Online view
  • Go to the Modes of operation display object. It will show that the cyclic synchronous position mode has been set:
Online view
  • Go to the Target position object and set a desired position for the axis:
Set value dialog
  • Go to the Position actual value object. As we did not enable the operation, the axis did not move:
Online view
  • Go to the Controlword object and set the switch on and enable operation commands (0x000F):
Set Value Dialog
Online view
  • Go to the Statusword object. It will show that drive has been switched on and the operation has been enabled:
Online view
  • Finally, go to the Position actual value object again. As the operation has been enabled, the axis reached the target position (65536):
Online view
  • The written values as well as the values provided by the drive simulation can be seen in the object dictionary.
Object Dictionary

The rest of the axis and other operation modes can be configured following the same steps described above. Furthermore, there are more objects used for the drive application but this example covers only the basic configuration. Please refer to the ETG6010 document for a detailed description of the CiA402 directive.

Extend to 6 Axis Motor Control Application

Below are the steps to be followed to extend the CiA402 example to 6-axis motor contol application.

  • Increase the number of axis to 6 in ecSlvCiA402.h file
#define AXES_NUMBER (6u)
  • Create additional pointers to TxPDOs and RxPDOs in EC_SLV_APP_CIA_Application_t in ecSlvCiA402.h file.
// RxPDOs
EC_API_SLV_Pdo_t* ptRxPdo1600;
EC_API_SLV_Pdo_t* ptRxPdo1601;
EC_API_SLV_Pdo_t* ptRxPdo1602;
// To extend to 6-axis
EC_API_SLV_Pdo_t* ptRxPdo1603;
EC_API_SLV_Pdo_t* ptRxPdo1604;
EC_API_SLV_Pdo_t* ptRxPdo1605;
// TxPDOs
EC_API_SLV_Pdo_t* ptTxPdo1A00;
EC_API_SLV_Pdo_t* ptTxPdo1A01;
EC_API_SLV_Pdo_t* ptTxPdo1A02;
// To extend to 6-axis
EC_API_SLV_Pdo_t* ptTxPdo1A03;
EC_API_SLV_Pdo_t* ptTxPdo1A04;
EC_API_SLV_Pdo_t* ptTxPdo1A05;
Definition ecSlvApiInternal.h:172
  • Adapt the additional axis indexes in ecSlvCiA402.c file
#define AXIS_ONE 0
#define AXIS_TWO 1
#define AXIS_THREE 2
#define AXIS_FOUR 3
#define AXIS_FIVE 4
#define AXIS_SIX 5
error = EC_SLV_APP_populateRxPDO(pAppInstance_p, pAppInstance_p->ptRxPdo1603, AXIS_FOUR);
if (error != EC_API_eERR_NONE)
{
OSAL_printf("Create RxPDO error code: 0x%08x\r\n", error);
goto Exit;
}
error = EC_SLV_APP_populateRxPDO(pAppInstance_p, pAppInstance_p->ptRxPdo1604, AXIS_FIVE);
if (error != EC_API_eERR_NONE)
{
OSAL_printf("Create RxPDO error code: 0x%08x\r\n", error);
goto Exit;
}
error = EC_SLV_APP_populateRxPDO(pAppInstance_p, pAppInstance_p->ptRxPdo1605, AXIS_SIX);
if (error != EC_API_eERR_NONE)
{
OSAL_printf("Create RxPDO error code: 0x%08x\r\n", error);
goto Exit;
}
@ EC_API_eERR_NONE
Definition ecSlvApiDef_error.h:41
error = EC_SLV_APP_populateTxPDO(pAppInstance_p, pAppInstance_p->ptTxPdo1A03, AXIS_FOUR);
if (error != EC_API_eERR_NONE)
{
OSAL_printf("Create TxPDO error code: 0x%08x\r\n", error);
goto Exit;
}
error = EC_SLV_APP_populateTxPDO(pAppInstance_p, pAppInstance_p->ptTxPdo1A04, AXIS_FIVE);
if (error != EC_API_eERR_NONE)
{
OSAL_printf("Create TxPDO error code: 0x%08x\r\n", error);
goto Exit;
}
error = EC_SLV_APP_populateTxPDO(pAppInstance_p, pAppInstance_p->ptTxPdo1A05, AXIS_SIX);
if (error != EC_API_eERR_NONE)
{
OSAL_printf("Create TxPDO error code: 0x%08x\r\n", error);
goto Exit;
}
  • Increase the heap size in sysconfig file.

Each additional axis needs 27952 bytes of heap memory for creating the objects such as control word, status word, quick stop, shutdown, mode of operation, position actual value, velocity actual value and more. Also, RxPDOs/TxPDOs, CoE object dictionary consumes some memory. Hence it is required to increase the heap memory size. For 6-axis control, the minimum heap size required would be 229376 bytes.

Increase Heap Memory
Allocate System Memory from MSRAM

Similarly, the CiA402 example can be extended to 9-axis motor contol application. For 9-axis control, the minimum heap size required would be 327680 bytes. Make sure that the size of MSRAM memory region is increased.

References