This page lists all the examples of ICSSG SDFM available in this SDK. Following sections describe the features available in each of the examples.
The ICSS SDFM driver provides a well defined set of APIs to expose sigma delta interface.
The ICSS SDFM examples invoke these APIs to
Once these steps are executed
SDFM has SysConfig support to initialize SDFM parameters and configure SDFM pins.
SysConfig is used to configure things mentioned below:
ICSSG SDFM driver supports three methods to generate clock which can be fed externally to modulator and SD_CLK pins. All SDFM sdk examples are using SDFM clock generated from eCAP, other two options has some trade-off as you will lose SD channel due to pin conflict.
Note: SysConfig only provides the clock selection option. Dividers have to be configured via API calls.
The PRG<k>_PRU1/0_GPI1 signal (muxed with SD0_D) can be used as SD_CLKOUT when PRU ICSSG generates clock. This is a trade-off as PRU application will lose one SD channel. Based on dividers value API SDFM_configClockFromGPO1 does configuration of PRU registers and enables pru to generate clock.
| SD clock (MHz) | PRU core clock (MHz) | First divider(div0) | Second divider(div1) | Description |
|---|---|---|---|---|
| 20 | 300 | 15 (0x1C) | 1 (0x00) | 20 = 300/(15*1) |
| 20 | 300 | 7.5 (0x0E) | 2 (0x01) | 20 = 300/(7.5*1) |
| 10 | 300 | 15 (0x1C) | 2 (0x01) | 10 = 300/(15*2) |
| 5 | 200 | 10 (0x) | 4 (0x01) | 5 = 200/(10*4) |
ICSSG eCAP can be used for SDFM clock generation. Based on divider value API SDFM_configEcap does configuration of eCAP registers and enables eCAP to generate output clock on PRGx_ECAP0_IN_APWM_OUT pin.
| SD clock (MHz) | PRU core clock (MHz) | divider |
|---|---|---|
| 20 | 300 | 15 |
| 15 | 300 | 20 |
| 10 | 200 | 20 |
ICSSG IEP has Sync0/Sync1 cyclic generation mode to generate clock which can be used for SDFM clock. The generated clock comes out on two pin corresponding SYNC0 and SYNC1. IEP also has SYNC1 delay feature which can be used to define delay between SYNC1 and SYNC0 output.
| API | Description | Parameters |
|---|---|---|
| SDFM_configIepSyncMode | Configures IEP SYNC0 and SYNC1 registers to generate free running clock | highPulseWidth: Number of clock cycles SYNC0/1 will be high, periodTime: Period between the rising edges of output clock, syncStartTime: starting time of free running clock |
| SDFM_enableIep | Enables IEP timer | 20 |
| SDFM_configSync1Delay | Defines clock cycles from the start of SYNC0 to the start of SYNC1 | delay: Delay before the start of SYNC1 |
| SD clock (MHz) | IEP clock (MHz) | highPulseWidth | periodTime | syncStartTime | Description |
|---|---|---|---|---|---|
| 20 | 300 | 6 (7-1) | 14 (15-1) | Any unsigned integer value | IEP clock 300MHz, SD clk = 20Mhz, Div = 300/20 = 15, one period time = 15 IEP cycles, high plus time = 7 IEP cycles |
| 10 | 200 | 9 (10-1) | 19 (20-1) | Any unsigned integer value | IEP clock 300MHz, SD clk = 10Mhz, Div = 200/10 = 20, one period time = 20 IEP cycles, high plus time = 10 IEP cycles (50% duty cycle) |
It is a better clock option to handle phase compensation. SDK has an example icss_sdfm_three_channel_with_phase_compensation for showing phase compensation.
Note : There is pin conflict between SDFM channel 8 data PIN and IEP0 SYNC_OUT1
Three parameters needs to configure for each SDFM channel.
PRU ICSSG SDFM interface supports three SINC filters to filter SD bit streams.
Normal current is used for SDFM data filter. It has features mentioned below
Note:
Over current is used for comparator filter to detect low threshold, high threshold and zero cross and generate PWM trips. It has features mentioned below
The Fast Detect is used for fast over current detection and trip generation. It has features mentioned below
Following section describes the flow of the examples.
| Folder/Files | Description |
|---|---|
| ${SDK_INSTALL_PATH}/examples/current_sense/icss_sdfm_nine_channel_with_continuous_mode | Application specific sources for ICSS SDFM for continuous normal current sampling for nine channels |
| ${SDK_INSTALL_PATH}/examples/current_sense/icss_sdfm_nine_channel_load_share_mode | Application specific sources for ICSS SDFM for trigger based normal current sampling for nine channels |
| ${SDK_INSTALL_PATH}/examples/current_sense/icss_sdfm_three_channel_single_pru_mode | Application specific sources for ICSS SDFM for trigger based normal current sampling for three channels |
| ${SDK_INSTALL_PATH}/examples/current_sense/icss_sdfm_three_channel_with_continuous_mode | Application specific sources for ICSS SDFM for continuous normal current sampling for three channels |
| ${SDK_INSTALL_PATH}/examples/current_sense/icss_sdfm_three_channel_with_phase_compensation | Application specific sources for ICSS SDFM with phase compensation |
| ${SDK_INSTALL_PATH}/examples/current_sense | Common source for ICSS SDFM applications |
| ${SDK_INSTALL_PATH}/source/current_sense/sdfm | |
| firmware/ | Folder containing ICSS SDFM firmware sources |
| driver/ | ICSS SDFM driver source |
| include/ | Folder containing ICSS SDFM structures and APIs declarations |
| Parameter | Value |
|---|---|
| CPU + OS | r5fss0-0 freertos |
| ICSSG | ICSSG0 |
| PRU | PRU0 (single channel) |
| PRU0, RTU-PRU0, TXPRU0 (multi channel using three PRUs - load share mode) | |
| Toolchain | ti-arm-clang |
| Board | am243x-evm, am243x-lp |
| Examples folder | examples/current_sense |
Following are different examples for ICSS SDFM:
| Example | Enabled Features | Tested/Supported Features |
|---|---|---|
| Basic ICSS SDFM Examples | Trigger based Normal current, Over current detection | Zero cross detection, Fast detect, Double Update |
| SDFM Examples with Continuous Normal Current Sampling | Continuous normal current sampling | Fast detect |
| SDFM Example With Phase Compensation | Trigger based Normal current, Phase compensation, Over current detection | Fast detect, Double Update, Zero cross detection |