AM243x MCU+ SDK  09.02.00
sdl_pok.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) Texas Instruments Incorporated 2023
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  *
32  */
33 
42 #ifndef SDL_POK_H_
43 #define SDL_POK_H_
44 
45 #include <sdl/pok/v1/sdl_ip_pok.h>
46 #include <sdl/pok/v1/sdl_pok_def.h>
47 #include <sdl/esm/v0/v0_0/sdl_ip_esm.h>
48 #include <sdl/dpl/sdl_dpl.h>
49 #include <sdl/pok/v1/sdl_pok.h>
50 
51 
52 
53 #if defined (SOC_AM64X)
54 #include <sdl/pok/v1/soc/am64x/sdl_soc_pok.h>
55 #endif
56 
57 
58 #if defined (SOC_AM243X)
59 #if defined (R5F_CORE)
61 #endif
62 #endif
63 
64 #ifdef __cplusplus
65 extern "C" {
66 #endif
67 
68 #include <sdl/include/soc_config.h>
69 
70 #if defined (IP_VERSION_POK_V1)
71 #include <sdl/pok/v1/sdl_pok.h>
72 #include <sdl/pok/v1/sdl_ip_pok.h>
73 #include <sdl/pok/v1/soc/sdl_soc_pok.h>
74 #endif
75 
76 #ifdef __cplusplus
77 }
78 #endif
79 #endif /* SDL_POK_H_ */
80 
sdl_pok_def.h
Header file containing various enumerations, structure definitions and function declarations for the ...
sdl_pok.h
This file contains the prototypes of the APIs present in the device abstraction layer file of POK....
sdl_dpl.h
This file contains the SDL DPL API's.
sdl_soc_pok.h
This file contains the prototypes of the APIs present in the device abstraction layer file of POK....