AM243x MCU+ SDK  09.02.00
I2C Temperature Read

Introduction

This example demonstrates probing of sensor via I2C and read data from it. The application reads data from the temperature sensor in the EVM. Application reads 20 samples from the sensor and exits.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am243x-evm
Example folder examples/drivers/i2c/i2c_temperature

Steps to Run the Example

See Also

I2C

Sample Output

Shown below is a sample output when the application is run,

[I2C] Temperature sensor found at device address 0x48
[I2C] Sample 0: 39.000000 (celcius)
[I2C] Sample 1: 39.000000 (celcius)
[I2C] Sample 2: 39.000000 (celcius)
[I2C] Sample 3: 39.000000 (celcius)
[I2C] Sample 4: 39.000000 (celcius)
[I2C] Sample 5: 39.000000 (celcius)
[I2C] Sample 6: 39.000000 (celcius)
[I2C] Sample 7: 39.000000 (celcius)
[I2C] Sample 8: 39.000000 (celcius)
[I2C] Sample 9: 39.000000 (celcius)
[I2C] Sample 10: 39.000000 (celcius)
[I2C] Sample 11: 39.000000 (celcius)
[I2C] Sample 12: 39.000000 (celcius)
[I2C] Sample 13: 39.000000 (celcius)
[I2C] Sample 14: 39.000000 (celcius)
[I2C] Sample 15: 39.000000 (celcius)
[I2C] Sample 16: 39.000000 (celcius)
[I2C] Sample 17: 39.000000 (celcius)
[I2C] Sample 18: 39.000000 (celcius)
[I2C] Sample 19: 39.000000 (celcius)
All tests have passed!!