![Logo](ti_logo.svg) |
AM243x INDUSTRIAL COMMUNICATIONS SDK
09.02.00
|
|
Go to the documentation of this file.
65 #define PNISO_MAX_NUM_EVENTS 2
72 #define PNISO_MODE_NONE 0
81 #define PNISO_MODE_INTERRUPT 1
86 #define PNISO_MODE_GPIO 2
91 #define PNISO_MODE_DISABLE 0
96 #define PNISO_MODE_ENABLE 1
void PN_ISO_deInitGPIOEvent(PN_Handle pnHandle, PNISOM_Handle isoHandle)
API to De init the ISOM event/signal.
struct PN_Config_s * PN_Handle
Alias for Profinet Handle containing base addresses and modules.
Definition: PN_Handle.h:102
void PN_ISO_enableGPIOEvent(PN_Handle pnHandle, PNISOM_Handle isoHandle)
API to enable the ISOM event/signal generation.
PNISOM_Handle PN_ISO_initGPIOEvent(PN_Handle pnHandle, uint8_t isoMode, uint32_t timeval, uint32_t duration)
API to initialize the ISOM event/signal. Returns the ISOM handle. The Event/signal will be disabled b...
void PN_ISO_disableGPIOEvent(PN_Handle pnHandle, PNISOM_Handle isoHandle)
API to disable the ISOM event/signal generation.
uint32_t * PNISOM_Handle
ISOM handle.
Definition: iPNIsoMDrv.h:101