AM243x Motor Control SDK  09.02.00
Transformation Algorithm

Introduction

The Transformation module consists of transformation commonly found in motor-control applications.

Features Supported

Transformation module includes:

  • Clarke transformation
  • Park transformation
  • Inverse Park transformation
  • Space Vector Generation (SVGEN)
    • Common-mode subtraction approach
  • DPWM Generation (Part of SVGEN)
    • Maximum Modulation
    • Minimum Modulation
  • SVGEN current reconstruction for single-shunt (SVGENCURRENT)
  • Phase voltage reconstruction in overmodulation (VOLTS_RECON)

Features Not Supported

N/A

Benchmark Results

A benchmark on R5F core has been conducted to observe the following results when running the following functions:

Transform Function Cpu Cycles
Clarke Transform
CLARKE_run_twoInput 16
CLARKE_run_threeInput 18
Park Transform
PARK_run 19*
Inverse Park Transform
IPARK_run 19*
Space Vector Generation
SVGEN_runCom 41
DPWM Generation
SVGEN_runMax 36
SVGEN_runMin 36
Phase voltage reconstruction
VOLREC_calcVolSF 30
VOLREC_run 90
Note
both PARK and IPARK does not include trigonometric calculations of phasor. For R5F core, it's recommened to leverage the fast ti_arm_sincos/FastRTS_sincos function found in mathlib of MCU+ SDK.
  • Ran with TI Clang Compiler v3.2.0.LTS, with -Os flag and the benchmarking function placed in TCM memory. Obtained the average result from 600 consecutive loops of running transform functions with DPL CycleCountP, mimicking the usage of a control loop.
  • Actual result may vary depending on provided datasets and memory configuration. For R5F, it is recommended for users to map control loops to TCM for the best performance.

Provided Examples

The following examples has been provided to demonstrate transformation module:

Additional References

N/A

API

APIs for Transformation Algorithms