Real-time communication with encoders and current sensing is typically handled by the Programmable Real-Time Unit Industrial Communication Subsystem (PRU-ICSS). The PRU-ICSS is a co-processor subsystem containing Programmable Real-Time (PRU) cores which implement the low level firmware. The PRU-ICSS frees up the main ARM cores in the device for other functions, such as control and data processing.
Applications and PRU-ICSS firmwares for following position sense encoders are provided in the SDK.