AM243x MCU+ SDK  09.01.00
UART Echo DMA LLD

Introduction

This example demonstrates the UART RX and TX operation in blocking, DMA mode of operation from LLD driver. This example receives 8 characters and echos back the same. The application ends when the user types 8 characters.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp
Example folder examples/drivers/uart/uart_echo_dma_lld

Steps to Run the Example

See Also

UART

Sample Output

Shown below is a sample output when the application is run, Please note that application prints in both CCS and UART console. In UART console you need to enter 8 characters.

CCS Console:

[UART] Echo example DMA mode started ...
All tests have passed!!

UART Console:

This is uart echo test DMA blocking mode
Receives 8 characters then echo's back. Please input..
12345678
All tests have passed!!