Simple DCL PI controller demonstration
This example leverages a PI controller from the digital control library(DCL). It demonstrates how to setup and run the PI controller. The example first initializes the datalog DCL_FDLOG to the test vector, run the controller based on the test input and compare the output with the expected value.
Folder/Files | Description |
---|---|
${SDK_INSTALL_PATH}/examples/dcl/dcl_pi/ | |
pi_test.c | Main function for PI testing |
pi_test.h | Contains all initialization of needed strctures |
data/ | Contains pre-generated data files result compares with |
${SDK_INSTALL_PATH}/source/dcl | |
dcl/ | Folder containing DCL library source |
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 nortos |
r5fss0-0 freertos | |
Toolchain | ti-arm-clang |
Boards | am243x-evm, am243x-lp |
Example folder | examples/dcl/dcl_pi |
Shown below is a sample output when the application is run: