ASM Test Application
All the register read are complete.
The MIDR register value is 0x411fc153
The CTR register value is 0x8003c003
The TCMTR register value is 0x10001
The MPUIR register value is 0x1000
The MPIDR register value is 0xc0000000
The PFR0 register value is 0x131
The PFR1 register value is 0x1
The ID_DFR0 register value is 0x10400
The ID_AFR0 register value is 0x0
The ID_MMFR0 register value is 0x210030
The ID_MMFR1 register value is 0x0
The ID_MMFR2 register value is 0x1200000
The ID_MMFR3 register value is 0x211
The ID_ISAR0 register value is 0x2101111
The ID_ISAR1 register value is 0x13112111
The ID_ISAR2 register value is 0x21232141
The ID_ISAR3 register value is 0x1112131
The ID_ISAR4 register value is 0x10142
The ID_ISAR5 register value is 0x0
The CCSIDR register value is 0xf00fe019
The CLIDR register value is 0x9200003
The AIDR register value is 0x0
The CSSELR register value is 0x1
The SCTLR register value is 0x1e5187d
The ACTLR register value is 0x27
The SecondaryACTLR register value is 0x400000
The CPACR register value is 0xc0f00000
The MPURegionBaseADDR register value is 0x70000000
The MPURegionEnableR register value is 0x29
The MPURegionAccessControlR register value is 0x20b
The RGNR register value is 0x3
The BTCMRegionR register value is 0x80019
The ATCMRegionR register value is 0x25
The SlavePortControlR register value is 0x0
The CONTEXTIDR register value is 0x0
The ThreadProcessIDR1 register value is 0x0
The ThreadProcessIDR2 register value is 0x0
The ThreadProcessIDR3 register value is 0x0
The nVALIRQSET register value is 0x0
The nVALFIQSET register value is 0x0
The nVALRESETSET register value is 0x0
The nVALDEBUGSET register value is 0x0
The nVALIRQCLEAR register value is 0x0
The nVALFIQCLEAR register value is 0x0
The nVALRESETCLEAR register value is 0x0
The nVALDEBUGCLEAR register value is 0x0
The BuildOption1R register value is 0x80000
The BuildOption2R register value is 0x8abfc5c7
The PinOptionR register value is 0xc
The LLPPnormalAXIRR register value is 0x0
The LLPPvirtualAXIRR register value is 0x0
The AHBRR register value is 0x5000004d
The CFLR register value is 0x0
The PMOVSR register value is 0x0
The DFSR register value is 0x0
The ADFSR register value is 0x0
The DFAR register value is 0x0
The IFSR register value is 0x0
The IFAR register value is 0x0
The AIFSR register value is 0x0
Test Name: ASM API TEST PASSED
All tests have passed