Functions | |
| void | PN_event1IsrHandler (void *arg) |
| Event1 ISR handler. Used to call the application ISR Handler in case a Ti ISOM event/signal is triggered. More... | |
| void | PN_event2IsrHandler (void *arg) |
| Event2 ISR handler. Used to call the application ISR Handler in case a To ISOM event/signal is triggered. More... | |
| int8_t | PN_ISO_initGPIOEvent (PN_Handle pnHandle, uint8_t isoMode, uint8_t isoEvent, uint32_t timeval, uint32_t duration) |
| API to initialize the ISOM event/signal. Returns the ISOM handle. The Event/signal will be disabled by default. More... | |
| void | PN_ISO_enableGPIOEvent (PN_Handle pnHandle) |
| API to enable the ISOM event/signal generation. More... | |
| void | PN_ISO_disableGPIOEvent (PN_Handle pnHandle) |
| API to disable the ISOM event/signal generation. More... | |
| void | PN_ISO_deInitGPIOEvent (PN_Handle pnHandle) |
| API to De init the ISOM event/signal. More... | |
Macros | |
| #define | PNISO_MAX_NUM_EVENTS 2 |
| #define | PNISO_MODE_NONE 0 |
| #define | PNISO_MODE_INTERRUPT 1 |
| #define | PNISO_MODE_GPIO 2 |
| #define | PNISO_MODE_DISABLE 0 |
| #define | PNISO_MODE_ENABLE 1 |
| #define | PNISO_TI_EVENT 1 |
| #define | PNISO_TI_EVENT_REG_SHIFT 0 |
| #define | PNISO_TO_EVENT 2 |
| #define | PNISO_TO_EVENT_REG_SHIFT 1 |
| #define | PNISO_ERR_SUCCESS 0 |
| #define | PNISO_ERR_INVALID_EVENT -1 |
| #define | PNISO_ERR_EVENTS_EXHAUSTED -2 |
| #define PNISO_MAX_NUM_EVENTS 2 |
Maximum number of ISOM events supported in a network cycle by firmware
| #define PNISO_MODE_NONE 0 |
Used to Disable ISOM mode
| #define PNISO_MODE_INTERRUPT 1 |
ISOM Interrupt Mode
| #define PNISO_MODE_GPIO 2 |
ISOM GPIO Mode
| #define PNISO_MODE_DISABLE 0 |
Disable ISOM mode
| #define PNISO_MODE_ENABLE 1 |
Enable ISOM mode
| #define PNISO_TI_EVENT 1 |
Input ISOM event
| #define PNISO_TI_EVENT_REG_SHIFT 0 |
Bit shift value for TI event
| #define PNISO_TO_EVENT 2 |
Output ISOM event
| #define PNISO_TO_EVENT_REG_SHIFT 1 |
Bit shift value for TO event
| #define PNISO_ERR_SUCCESS 0 |
| #define PNISO_ERR_INVALID_EVENT -1 |
| #define PNISO_ERR_EVENTS_EXHAUSTED -2 |
| void PN_event1IsrHandler | ( | void * | arg | ) |
Event1 ISR handler. Used to call the application ISR Handler in case a Ti ISOM event/signal is triggered.
| [in] | arg |
| void PN_event2IsrHandler | ( | void * | arg | ) |
Event2 ISR handler. Used to call the application ISR Handler in case a To ISOM event/signal is triggered.
| [in] | arg |
| int8_t PN_ISO_initGPIOEvent | ( | PN_Handle | pnHandle, |
| uint8_t | isoMode, | ||
| uint8_t | isoEvent, | ||
| uint32_t | timeval, | ||
| uint32_t | duration | ||
| ) |
API to initialize the ISOM event/signal. Returns the ISOM handle. The Event/signal will be disabled by default.
| pnHandle | Profinet Handle | |
| [in] | isoMode | ISOM Mode - PNISO_MODE_GPIO/PNISO_MODE_INTERRUPT |
| [in] | isoEvent | ISOM Event - PNISO_TI_EVENT/PNISO_TO_EVENT |
| [in] | timeval | time in nanosecond to trigger the event/signal (Reference is Start of Cycle) |
| [in] | duration | Duration of signal in nanoseconds |
| 0 | on success |
| -1 | if max number of events reached |
| -2 | if invalid event type passed |
| void PN_ISO_enableGPIOEvent | ( | PN_Handle | pnHandle | ) |
API to enable the ISOM event/signal generation.
| pnHandle | Profinet Handle |
| void PN_ISO_disableGPIOEvent | ( | PN_Handle | pnHandle | ) |
API to disable the ISOM event/signal generation.
| pnHandle | Profinet Handles |
| void PN_ISO_deInitGPIOEvent | ( | PN_Handle | pnHandle | ) |
API to De init the ISOM event/signal.
| pnHandle | Profinet Handle |